ltib is latest downloaded from freescale : L3.0.35_1.1.0_121218_source.tar.gz
Applied all the necessary patches for the build to work on ubuntu 12.04 and ltib builds well past the blue configuration screen.
However when trying to build the busybox it fails with a linker problem.
It appears the build script is not finding necessary libraries:
the linker error script is as follows:
==========
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find /lib/libc.so.6
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find /usr/lib/libc_nonshared.a
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find /lib/ld-linux.so.3
collect2: ld returned 1 exit status
RPM build errors:
Build time for busybox: 5 seconds
Started: Sat Mar 16 20:00:41 2013
Ended: Sat Mar 16 20:00:47 2013
Elapsed: 6 seconds
These packages failed to build:
busybox
========================
Any advice will be appreciated