Failed to flash system.img

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to flash system.img

747 Views
Raana
Contributor III

Dear all,

 

Currently, I'm using i.Mx6 SabreSD based custom board. There I'm trying to flash the Android (Android Nougat 7.1.1) binaries into eMMC. We have 4 kind of boards (i.Mx6Q/D/DL/S). All the cores are working fine except i.Mx6Solo (512MB RAM).

 

Before I have kept two u-boot.imx only. One is for Quad/Dual and another one is for DL/Solo (common DCD settings). The same configurations are working fine with latest Linux release and the earlier Android release too.

 

But here, it was giving error when i tried with DL and solo. So, after that I have kept difference cfg file for DL (because my DL is 1GB). After that DL was working without any error.

 

But solo is always giving error. Whether it's related to RAM size ?

 

MFG tool from, android_N7.1.1_1.0.0_tools.tar.gz.

It's giving error, exactly when flashing the system.img file (error log attached).

 

What may be the issue? Please guide me to move further.

 

Thank You.

Best Regards,

J.P.Raja

Original Attachment has been moved to: MFG-solo-error-log.txt.zip

Labels (3)
0 Kudos
Reply
1 Reply

605 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raja

from log "out_of_memory" yes, this may be caused by memory size.

One can try to decrease CMA size and rerun ddr test for Solo,
after finding new ddr coefficients, rebuild mfg tools firmware (files in mfg tools /firmare folder)
with new ones. Please refer to attached Yocto Guide sect.6.2 Manufacturing Tool.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply