Ethernet bandwidth on iMX6 dual lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet bandwidth on iMX6 dual lite

1,084 Views
richardbuchmann
Contributor I

Hi,

We have several problems with ethernet bandwidth of our board based on a iMX6 dual lite.

A dual lite should work at 340 Mbps using TCP but it does not. This is what we get on a similar board based on a quad not-lite.

Please read below the tests we did to find out the root cause.

Test NC

  • On the dual lite board
    dd if=/dev/zero bs=1M | nc 192.168.1.24 5001
  • On a PC (192.168.1.24)
    nc -l -p 5001 > /dev/null
    and in another shell :
    sudo iftop -i eth0

Results : only 100 Mbps instead of expected 340 (or more)

Test TCP

  1. On the dual lite board
    gst-launch-1.0 videotestsrc ! video/x-raw, width=1280, height=2048, framerate=25/1, format=GRAY8 ! imagefreeze ! queue max-size-buffers=1 ! tcpclientsink port=5000 host=192.168.1.24 sync=false
  2. On a PC (192.168.1.24)
    gst-launch-1.0 tcpserversrc port=5000 host=0.0.0.0 ! queue ! videoparse format=25 width=1280 height=2048 framerate=50/1 ! queue ! videoconvert ! queue ! fpsdisplaysink sync=false
  3. Reboot and try again

Results : the FPS is varying a lot. At every boot, the FPS max is like random.

Question

Is there anything wrong ?

Is it possible to increase the bandwidth ?

Labels (3)
0 Kudos
Reply
3 Replies

852 Views
richardbuchmann
Contributor I

How many should be the expected bandwidth for a dual lite @800 MHz ?

0 Kudos
Reply

852 Views
Yuri
NXP Employee
NXP Employee

Hello,

    Perhaps the following general considerations help to improve

network performance. Also, it makes sense to use the recent

BSP (L3.14.38).

How To: Network / TCP / UDP Tuning

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

852 Views
richardbuchmann
Contributor I

Hi,

We followed the steps described in the link. (How To: Network / TCP / UDP Tuning)

Unfortunately, the performances are still the same (the new values are properly applied) :

- about 100 Mb/s on our dual lite.

- about 340 Mb/s on our quad.

Info: CPU usage is 0% before running tests.

0 Kudos
Reply