Hi,
We have several problems with ethernet bandwidth of our board based on a iMX6 dual lite.
A dual lite should work at 340 Mbps using TCP but it does not. This is what we get on a similar board based on a quad not-lite.
Please read below the tests we did to find out the root cause.
Test NC
Results : only 100 Mbps instead of expected 340 (or more)
Test TCP
Results : the FPS is varying a lot. At every boot, the FPS max is like random.
Question
Is there anything wrong ?
Is it possible to increase the bandwidth ?
Hello,
Perhaps the following general considerations help to improve
network performance. Also, it makes sense to use the recent
BSP (L3.14.38).
How To: Network / TCP / UDP Tuning
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
We followed the steps described in the link. (How To: Network / TCP / UDP Tuning)
Unfortunately, the performances are still the same (the new values are properly applied) :
- about 100 Mb/s on our dual lite.
- about 340 Mb/s on our quad.
Info: CPU usage is 0% before running tests.