Dear support,
Based on the i.MX6 EVK schematic, ETH_VDDIO should be 1.8V or 2.5V. Unfortunately we accidentally wired 3.3V to ETH_VDDIO to NVCC_RGMII on our board. Luckily we don't use any Ethernet components on our board. I would like to ask your opinion whether this voltage will cause problem of the operation of the board and the CPU?
Vincent
Hi Vincent
i.MX6Q max. NVCC_RGMII is 2.625V according to Table 6. Operating Ranges
Table 6. Operating Ranges i.MX6DQ Datasheet, so 3.3V may cause problems to processor.
http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------