Dear Experts, Could you please help me to resolve this issue. ERROR: m4-native-1.4.18-r0 do_compile: oe_runmake failed Tried the following DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland bitbake core-image-minimal
Ubuntu version 16.4 LTS
Thank you
The following is the Build log console log
-------------------------------------------------
valeo-cic@bbr:~/imx-yocto-bsp/build-wayland$ bitbake core-image-minimal
NOTE: Your conf/bblayers.conf has been automatically updated.
WARNING: You have included the meta-gnome layer, but 'x11' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-gnome README for details on enabling meta-gnome support.
Parsing recipes: 100% |######################################################################################################################################################################| Time: 0:01:29
Parsing of 2562 .bb files complete (0 cached, 2562 parsed). 3483 targets, 454 skipped, 8 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mqevk"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "4.14-sumo"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-poky = "HEAD:c9bd4984f8f471ca2c43052714f4413ba99cf171"
meta-oe
meta-multimedia = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-freescale = "HEAD:27ca94f8a4336790ba117b4298566f6820e7e74c"
meta-freescale-3rdparty = "HEAD:82037216280a39957fb4272581637abec734ad50"
meta-freescale-distro = "HEAD:f7e2216e93aff14ac32728a13637a48df436b7f4"
meta-bsp
meta-sdk = "HEAD:8eeb420fad668b733ab95b460895e1c337c66b25"
meta-browser = "HEAD:75640e14e325479c076b6272b646be7a239c18aa"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-qt5 = "HEAD:d4e7f73d04e8448d326b6f89908701e304e37d65"
Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:02
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: m4-native-1.4.18-r0 do_compile: oe_runmake failed
ERROR: m4-native-1.4.18-r0 do_compile: Function failed: do_compile (log file is located at /home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/temp/log.do_compile.29555)
ERROR: Logfile of failure stored in: /home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/temp/log.do_compile.29555
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 8 infodir=/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/info
| make all-recursive
| make[1]: Entering directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build'
| Making all in .
| make[2]: Entering directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build'
| make[2]: Nothing to be done for 'all-am'.
| make[2]: Leaving directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build'
| Making all in examples
| make[2]: Entering directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build/examples'
| make[2]: Nothing to be done for 'all'.
| make[2]: Leaving directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build/examples'
| Making all in lib
| make[2]: Entering directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build/lib'
| rm -f alloca.h-t alloca.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| cat ../../m4-1.4.18/lib/alloca.in.h; \
| } > alloca.h-t && \
| mv -f alloca.h-t alloca.h
| rm -f configmake.h-t && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| echo '#define PREFIX "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr"'; \
| echo '#define EXEC_PREFIX "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr"'; \
| echo '#define BINDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/bin"'; \
| echo '#define SBINDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/sbin"'; \
| echo '#define LIBEXECDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/libexec"'; \
| echo '#define DATAROOTDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share"'; \
| echo '#define DATADIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share"'; \
| echo '#define SYSCONFDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/etc"'; \
| echo '#define SHAREDSTATEDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/com"'; \
| echo '#define LOCALSTATEDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/var"'; \
| echo '#define RUNSTATEDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/var/run"'; \
| echo '#define INCLUDEDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include"'; \
| echo '#define OLDINCLUDEDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include"'; \
| echo '#define DOCDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/doc/m4"'; \
| echo '#define INFODIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/info"'; \
| echo '#define HTMLDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/doc/m4"'; \
| echo '#define DVIDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/doc/m4"'; \
| echo '#define PDFDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/doc/m4"'; \
| echo '#define PSDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/doc/m4"'; \
| echo '#define LIBDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/lib"'; \
| echo '#define LISPDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/emacs/site-lisp"'; \
| echo '#define LOCALEDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/locale"'; \
| echo '#define MANDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/man"'; \
| echo '#define MANEXT ""'; \
| echo '#define PKGDATADIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/share/m4"'; \
| echo '#define PKGINCLUDEDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include/m4"'; \
| echo '#define PKGLIBDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/lib/m4"'; \
| echo '#define PKGLIBEXECDIR "/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/libexec/m4"'; \
| } | sed '/""/d' > configmake.h-t && \
| mv -f configmake.h-t configmake.h
| rm -f c++defs.h-t c++defs.h && \
| sed -n -e '/_GL_CXXDEFS/,$p' \
| < ../../m4-1.4.18/build-aux/snippet/c++defs.h \
| > c++defs.h-t && \
| mv c++defs.h-t c++defs.h
| rm -f arg-nonnull.h-t arg-nonnull.h && \
| sed -n -e '/GL_ARG_NONNULL/,$p' \
| < ../../m4-1.4.18/build-aux/snippet/arg-nonnull.h \
| > arg-nonnull.h-t && \
| mv arg-nonnull.h-t arg-nonnull.h
| rm -f warn-on-use.h-t warn-on-use.h && \
| sed -n -e '/^.ifndef/,$p' \
| < ../../m4-1.4.18/build-aux/snippet/warn-on-use.h \
| > warn-on-use.h-t && \
| mv warn-on-use.h-t warn-on-use.h
| rm -f limits.h-t limits.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */' && \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_LIMITS_H''@|<limits.h>|g' \
| < ../../m4-1.4.18/lib/limits.in.h; \
| } > limits.h-t && \
| mv limits.h-t limits.h
| rm -f unused-parameter.h-t unused-parameter.h && \
| sed -n -e '/GL_UNUSED_PARAMETER/,$p' \
| < ../../m4-1.4.18/build-aux/snippet/unused-parameter.h \
| > unused-parameter.h-t && \
| mv unused-parameter.h-t unused-parameter.h
| rm -f stdint.h-t stdint.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's/@''HAVE_STDINT_H''@/1/g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_STDINT_H''@|<stdint.h>|g' \
| -e 's/@''HAVE_C99_STDINT_H''@/1/g' \
| -e 's/@''HAVE_SYS_TYPES_H''@/1/g' \
| -e 's/@''HAVE_INTTYPES_H''@/1/g' \
| -e 's/@''HAVE_SYS_INTTYPES_H''@/0/g' \
| -e 's/@''HAVE_SYS_BITYPES_H''@/0/g' \
| -e 's/@''HAVE_WCHAR_H''@/1/g' \
| -e 's/@''HAVE_LONG_LONG_INT''@/1/g' \
| -e 's/@''HAVE_UNSIGNED_LONG_LONG_INT''@/1/g' \
| -e 's/@''APPLE_UNIVERSAL_BUILD''@/0/g' \
| -e 's/@''BITSIZEOF_PTRDIFF_T''@//g' \
| -e 's/@''PTRDIFF_T_SUFFIX''@//g' \
| -e 's/@''BITSIZEOF_SIG_ATOMIC_T''@//g' \
| -e 's/@''HAVE_SIGNED_SIG_ATOMIC_T''@//g' \
| -e 's/@''SIG_ATOMIC_T_SUFFIX''@//g' \
| -e 's/@''BITSIZEOF_SIZE_T''@//g' \
| -e 's/@''SIZE_T_SUFFIX''@//g' \
| -e 's/@''BITSIZEOF_WCHAR_T''@//g' \
| -e 's/@''HAVE_SIGNED_WCHAR_T''@//g' \
| -e 's/@''WCHAR_T_SUFFIX''@//g' \
| -e 's/@''BITSIZEOF_WINT_T''@//g' \
| -e 's/@''HAVE_SIGNED_WINT_T''@//g' \
| -e 's/@''WINT_T_SUFFIX''@//g' \
| -e 's/@''GNULIB_OVERRIDES_WINT_T''@/0/g' \
| < ../../m4-1.4.18/lib/stdint.in.h; \
| } > stdint.h-t && \
| mv stdint.h-t stdint.h
| /home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/hosttools/mkdir -p sys
| rm -f sys/types.h-t sys/types.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_SYS_TYPES_H''@|<sys/types.h>|g' \
| -e 's|@''WINDOWS_64_BIT_OFF_T''@|0|g' \
| < ../../m4-1.4.18/lib/sys_types.in.h; \
| } > sys/types.h-t && \
| mv sys/types.h-t sys/types.h
| rm -f fcntl.h-t fcntl.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_FCNTL_H''@|<fcntl.h>|g' \
| -e 's/@''GNULIB_FCNTL''@/1/g' \
| -e 's/@''GNULIB_NONBLOCKING''@/0/g' \
| -e 's/@''GNULIB_OPEN''@/1/g' \
| -e 's/@''GNULIB_OPENAT''@/0/g' \
| -e 's|@''HAVE_FCNTL''@|1|g' \
| -e 's|@''HAVE_OPENAT''@|1|g' \
| -e 's|@''REPLACE_FCNTL''@|1|g' \
| -e 's|@''REPLACE_OPEN''@|0|g' \
| -e 's|@''REPLACE_OPENAT''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/fcntl.in.h; \
| } > fcntl.h-t && \
| mv fcntl.h-t fcntl.h
| rm -f langinfo.h-t langinfo.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''HAVE_LANGINFO_H''@|1|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_LANGINFO_H''@|<langinfo.h>|g' \
| -e 's/@''GNULIB_NL_LANGINFO''@/1/g' \
| -e 's|@''HAVE_LANGINFO_CODESET''@|1|g' \
| -e 's|@''HAVE_LANGINFO_T_FMT_AMPM''@|1|g' \
| -e 's|@''HAVE_LANGINFO_ERA''@|1|g' \
| -e 's|@''HAVE_LANGINFO_YESEXPR''@|1|g' \
| -e 's|@''HAVE_NL_LANGINFO''@|1|g' \
| -e 's|@''REPLACE_NL_LANGINFO''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/langinfo.in.h; \
| } > langinfo.h-t && \
| mv langinfo.h-t langinfo.h
| rm -f locale.h-t locale.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */' && \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_LOCALE_H''@|<locale.h>|g' \
| -e 's/@''GNULIB_LOCALECONV''@/1/g' \
| -e 's/@''GNULIB_SETLOCALE''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_DUPLOCALE''@/0/g' \
| -e 's|@''HAVE_DUPLOCALE''@|1|g' \
| -e 's|@''HAVE_XLOCALE_H''@|1|g' \
| -e 's|@''REPLACE_LOCALECONV''@|0|g' \
| -e 's|@''REPLACE_SETLOCALE''@|0|g' \
| -e 's|@''REPLACE_DUPLOCALE''@|0|g' \
| -e 's|@''REPLACE_STRUCT_LCONV''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/locale.in.h; \
| } > locale.h-t && \
| mv locale.h-t locale.h
| rm -f math.h-t math.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */' && \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT_AS_FIRST_DIRECTIVE''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_AS_FIRST_DIRECTIVE_MATH_H''@|<math.h>|g' \
| -e 's/@''GNULIB_ACOSF''@/0/g' \
| -e 's/@''GNULIB_ACOSL''@/0/g' \
| -e 's/@''GNULIB_ASINF''@/0/g' \
| -e 's/@''GNULIB_ASINL''@/0/g' \
| -e 's/@''GNULIB_ATANF''@/0/g' \
| -e 's/@''GNULIB_ATANL''@/0/g' \
| -e 's/@''GNULIB_ATAN2F''@/0/g' \
| -e 's/@''GNULIB_CBRT''@/0/g' \
| -e 's/@''GNULIB_CBRTF''@/0/g' \
| -e 's/@''GNULIB_CBRTL''@/0/g' \
| -e 's/@''GNULIB_CEIL''@/0/g' \
| -e 's/@''GNULIB_CEILF''@/0/g' \
| -e 's/@''GNULIB_CEILL''@/0/g' \
| -e 's/@''GNULIB_COPYSIGN''@/0/g' \
| -e 's/@''GNULIB_COPYSIGNF''@/0/g' \
| -e 's/@''GNULIB_COPYSIGNL''@/0/g' \
| -e 's/@''GNULIB_COSF''@/0/g' \
| -e 's/@''GNULIB_COSL''@/0/g' \
| -e 's/@''GNULIB_COSHF''@/0/g' \
| -e 's/@''GNULIB_EXPF''@/0/g' \
| -e 's/@''GNULIB_EXPL''@/0/g' \
| -e 's/@''GNULIB_EXP2''@/0/g' \
| -e 's/@''GNULIB_EXP2F''@/0/g' \
| -e 's/@''GNULIB_EXP2L''@/0/g' \
| -e 's/@''GNULIB_EXPM1''@/0/g' \
| -e 's/@''GNULIB_EXPM1F''@/0/g' \
| -e 's/@''GNULIB_EXPM1L''@/0/g' \
| -e 's/@''GNULIB_FABSF''@/0/g' \
| -e 's/@''GNULIB_FABSL''@/0/g' \
| -e 's/@''GNULIB_FLOOR''@/0/g' \
| -e 's/@''GNULIB_FLOORF''@/0/g' \
| -e 's/@''GNULIB_FLOORL''@/0/g' \
| -e 's/@''GNULIB_FMA''@/0/g' \
| -e 's/@''GNULIB_FMAF''@/0/g' \
| -e 's/@''GNULIB_FMAL''@/0/g' \
| -e 's/@''GNULIB_FMOD''@/0/g' \
| -e 's/@''GNULIB_FMODF''@/0/g' \
| -e 's/@''GNULIB_FMODL''@/0/g' \
| -e 's/@''GNULIB_FREXPF''@/0/g' \
| -e 's/@''GNULIB_FREXP''@/1/g' \
| -e 's/@''GNULIB_FREXPL''@/1/g' \
| -e 's/@''GNULIB_HYPOT''@/0/g' \
| -e 's/@''GNULIB_HYPOTF''@/0/g' \
| -e 's/@''GNULIB_HYPOTL''@/0/g' \
| < ../../m4-1.4.18/lib/math.in.h | \
| sed -e 's/@''GNULIB_ILOGB''@/0/g' \
| -e 's/@''GNULIB_ILOGBF''@/0/g' \
| -e 's/@''GNULIB_ILOGBL''@/0/g' \
| -e 's/@''GNULIB_ISFINITE''@/0/g' \
| -e 's/@''GNULIB_ISINF''@/0/g' \
| -e 's/@''GNULIB_ISNAN''@/0/g' \
| -e 's/@''GNULIB_ISNANF''@/0/g' \
| -e 's/@''GNULIB_ISNAND''@/0/g' \
| -e 's/@''GNULIB_ISNANL''@/0/g' \
| -e 's/@''GNULIB_LDEXPF''@/0/g' \
| -e 's/@''GNULIB_LDEXPL''@/0/g' \
| -e 's/@''GNULIB_LOG''@/0/g' \
| -e 's/@''GNULIB_LOGF''@/0/g' \
| -e 's/@''GNULIB_LOGL''@/0/g' \
| -e 's/@''GNULIB_LOG10''@/0/g' \
| -e 's/@''GNULIB_LOG10F''@/0/g' \
| -e 's/@''GNULIB_LOG10L''@/0/g' \
| -e 's/@''GNULIB_LOG1P''@/0/g' \
| -e 's/@''GNULIB_LOG1PF''@/0/g' \
| -e 's/@''GNULIB_LOG1PL''@/0/g' \
| -e 's/@''GNULIB_LOG2''@/0/g' \
| -e 's/@''GNULIB_LOG2F''@/0/g' \
| -e 's/@''GNULIB_LOG2L''@/0/g' \
| -e 's/@''GNULIB_LOGB''@/0/g' \
| -e 's/@''GNULIB_LOGBF''@/0/g' \
| -e 's/@''GNULIB_LOGBL''@/0/g' \
| -e 's/@''GNULIB_MODF''@/0/g' \
| -e 's/@''GNULIB_MODFF''@/0/g' \
| -e 's/@''GNULIB_MODFL''@/0/g' \
| -e 's/@''GNULIB_POWF''@/0/g' \
| -e 's/@''GNULIB_REMAINDER''@/0/g' \
| -e 's/@''GNULIB_REMAINDERF''@/0/g' \
| -e 's/@''GNULIB_REMAINDERL''@/0/g' \
| -e 's/@''GNULIB_RINT''@/0/g' \
| -e 's/@''GNULIB_RINTF''@/0/g' \
| -e 's/@''GNULIB_RINTL''@/0/g' \
| -e 's/@''GNULIB_ROUND''@/0/g' \
| -e 's/@''GNULIB_ROUNDF''@/0/g' \
| -e 's/@''GNULIB_ROUNDL''@/0/g' \
| -e 's/@''GNULIB_SIGNBIT''@/1/g' \
| -e 's/@''GNULIB_SINF''@/0/g' \
| -e 's/@''GNULIB_SINL''@/0/g' \
| -e 's/@''GNULIB_SINHF''@/0/g' \
| -e 's/@''GNULIB_SQRTF''@/0/g' \
| -e 's/@''GNULIB_SQRTL''@/0/g' \
| -e 's/@''GNULIB_TANF''@/0/g' \
| -e 's/@''GNULIB_TANL''@/0/g' \
| -e 's/@''GNULIB_TANHF''@/0/g' \
| -e 's/@''GNULIB_TRUNC''@/0/g' \
| -e 's/@''GNULIB_TRUNCF''@/0/g' \
| -e 's/@''GNULIB_TRUNCL''@/0/g' \
| | \
| sed -e 's|@''HAVE_ACOSF''@|1|g' \
| -e 's|@''HAVE_ACOSL''@|1|g' \
| -e 's|@''HAVE_ASINF''@|1|g' \
| -e 's|@''HAVE_ASINL''@|1|g' \
| -e 's|@''HAVE_ATANF''@|1|g' \
| -e 's|@''HAVE_ATANL''@|1|g' \
| -e 's|@''HAVE_ATAN2F''@|1|g' \
| -e 's|@''HAVE_CBRT''@|1|g' \
| -e 's|@''HAVE_CBRTF''@|1|g' \
| -e 's|@''HAVE_CBRTL''@|1|g' \
| -e 's|@''HAVE_COPYSIGN''@|1|g' \
| -e 's|@''HAVE_COPYSIGNL''@|1|g' \
| -e 's|@''HAVE_COSF''@|1|g' \
| -e 's|@''HAVE_COSL''@|1|g' \
| -e 's|@''HAVE_COSHF''@|1|g' \
| -e 's|@''HAVE_EXPF''@|1|g' \
| -e 's|@''HAVE_EXPL''@|1|g' \
| -e 's|@''HAVE_EXPM1''@|1|g' \
| -e 's|@''HAVE_EXPM1F''@|1|g' \
| -e 's|@''HAVE_FABSF''@|1|g' \
| -e 's|@''HAVE_FABSL''@|1|g' \
| -e 's|@''HAVE_FMA''@|1|g' \
| -e 's|@''HAVE_FMAF''@|1|g' \
| -e 's|@''HAVE_FMAL''@|1|g' \
| -e 's|@''HAVE_FMODF''@|1|g' \
| -e 's|@''HAVE_FMODL''@|1|g' \
| -e 's|@''HAVE_FREXPF''@|1|g' \
| -e 's|@''HAVE_HYPOTF''@|1|g' \
| -e 's|@''HAVE_HYPOTL''@|1|g' \
| -e 's|@''HAVE_ILOGB''@|1|g' \
| -e 's|@''HAVE_ILOGBF''@|1|g' \
| -e 's|@''HAVE_ILOGBL''@|1|g' \
| -e 's|@''HAVE_ISNANF''@|1|g' \
| -e 's|@''HAVE_ISNAND''@|1|g' \
| -e 's|@''HAVE_ISNANL''@|1|g' \
| -e 's|@''HAVE_LDEXPF''@|1|g' \
| -e 's|@''HAVE_LOGF''@|1|g' \
| -e 's|@''HAVE_LOGL''@|1|g' \
| -e 's|@''HAVE_LOG10F''@|1|g' \
| -e 's|@''HAVE_LOG10L''@|1|g' \
| -e 's|@''HAVE_LOG1P''@|1|g' \
| -e 's|@''HAVE_LOG1PF''@|1|g' \
| -e 's|@''HAVE_LOG1PL''@|1|g' \
| -e 's|@''HAVE_LOGBF''@|1|g' \
| -e 's|@''HAVE_LOGBL''@|1|g' \
| -e 's|@''HAVE_MODFF''@|1|g' \
| -e 's|@''HAVE_MODFL''@|1|g' \
| -e 's|@''HAVE_POWF''@|1|g' \
| -e 's|@''HAVE_REMAINDER''@|1|g' \
| -e 's|@''HAVE_REMAINDERF''@|1|g' \
| -e 's|@''HAVE_RINT''@|1|g' \
| -e 's|@''HAVE_RINTL''@|1|g' \
| -e 's|@''HAVE_SINF''@|1|g' \
| -e 's|@''HAVE_SINL''@|1|g' \
| -e 's|@''HAVE_SINHF''@|1|g' \
| -e 's|@''HAVE_SQRTF''@|1|g' \
| -e 's|@''HAVE_SQRTL''@|1|g' \
| -e 's|@''HAVE_TANF''@|1|g' \
| -e 's|@''HAVE_TANL''@|1|g' \
| -e 's|@''HAVE_TANHF''@|1|g' \
| -e 's|@''HAVE_DECL_ACOSL''@|1|g' \
| -e 's|@''HAVE_DECL_ASINL''@|1|g' \
| -e 's|@''HAVE_DECL_ATANL''@|1|g' \
| -e 's|@''HAVE_DECL_CBRTF''@|1|g' \
| -e 's|@''HAVE_DECL_CBRTL''@|1|g' \
| -e 's|@''HAVE_DECL_CEILF''@|1|g' \
| -e 's|@''HAVE_DECL_CEILL''@|1|g' \
| -e 's|@''HAVE_DECL_COPYSIGNF''@|1|g' \
| -e 's|@''HAVE_DECL_COSL''@|1|g' \
| -e 's|@''HAVE_DECL_EXPL''@|1|g' \
| -e 's|@''HAVE_DECL_EXP2''@|1|g' \
| -e 's|@''HAVE_DECL_EXP2F''@|1|g' \
| -e 's|@''HAVE_DECL_EXP2L''@|1|g' \
| -e 's|@''HAVE_DECL_EXPM1L''@|1|g' \
| -e 's|@''HAVE_DECL_FLOORF''@|1|g' \
| -e 's|@''HAVE_DECL_FLOORL''@|1|g' \
| -e 's|@''HAVE_DECL_FREXPL''@|1|g' \
| -e 's|@''HAVE_DECL_LDEXPL''@|1|g' \
| -e 's|@''HAVE_DECL_LOGL''@|1|g' \
| -e 's|@''HAVE_DECL_LOG10L''@|1|g' \
| -e 's|@''HAVE_DECL_LOG2''@|1|g' \
| -e 's|@''HAVE_DECL_LOG2F''@|1|g' \
| -e 's|@''HAVE_DECL_LOG2L''@|1|g' \
| -e 's|@''HAVE_DECL_LOGB''@|1|g' \
| -e 's|@''HAVE_DECL_REMAINDER''@|1|g' \
| -e 's|@''HAVE_DECL_REMAINDERL''@|1|g' \
| -e 's|@''HAVE_DECL_RINTF''@|1|g' \
| -e 's|@''HAVE_DECL_ROUND''@|1|g' \
| -e 's|@''HAVE_DECL_ROUNDF''@|1|g' \
| -e 's|@''HAVE_DECL_ROUNDL''@|1|g' \
| -e 's|@''HAVE_DECL_SINL''@|1|g' \
| -e 's|@''HAVE_DECL_SQRTL''@|1|g' \
| -e 's|@''HAVE_DECL_TANL''@|1|g' \
| -e 's|@''HAVE_DECL_TRUNC''@|1|g' \
| -e 's|@''HAVE_DECL_TRUNCF''@|1|g' \
| -e 's|@''HAVE_DECL_TRUNCL''@|1|g' \
| | \
| sed -e 's|@''REPLACE_ACOSF''@|0|g' \
| -e 's|@''REPLACE_ASINF''@|0|g' \
| -e 's|@''REPLACE_ATANF''@|0|g' \
| -e 's|@''REPLACE_ATAN2F''@|0|g' \
| -e 's|@''REPLACE_CBRTF''@|0|g' \
| -e 's|@''REPLACE_CBRTL''@|0|g' \
| -e 's|@''REPLACE_CEIL''@|0|g' \
| -e 's|@''REPLACE_CEILF''@|0|g' \
| -e 's|@''REPLACE_CEILL''@|0|g' \
| -e 's|@''REPLACE_COSF''@|0|g' \
| -e 's|@''REPLACE_COSHF''@|0|g' \
| -e 's|@''REPLACE_EXPF''@|0|g' \
| -e 's|@''REPLACE_EXPM1''@|0|g' \
| -e 's|@''REPLACE_EXPM1F''@|0|g' \
| -e 's|@''REPLACE_EXP2''@|0|g' \
| -e 's|@''REPLACE_EXP2L''@|0|g' \
| -e 's|@''REPLACE_FABSL''@|0|g' \
| -e 's|@''REPLACE_FLOOR''@|0|g' \
| -e 's|@''REPLACE_FLOORF''@|0|g' \
| -e 's|@''REPLACE_FLOORL''@|0|g' \
| -e 's|@''REPLACE_FMA''@|0|g' \
| -e 's|@''REPLACE_FMAF''@|0|g' \
| -e 's|@''REPLACE_FMAL''@|0|g' \
| -e 's|@''REPLACE_FMOD''@|0|g' \
| -e 's|@''REPLACE_FMODF''@|0|g' \
| -e 's|@''REPLACE_FMODL''@|0|g' \
| -e 's|@''REPLACE_FREXPF''@|0|g' \
| -e 's|@''REPLACE_FREXP''@|0|g' \
| -e 's|@''REPLACE_FREXPL''@|0|g' \
| -e 's|@''REPLACE_HUGE_VAL''@|0|g' \
| -e 's|@''REPLACE_HYPOT''@|0|g' \
| -e 's|@''REPLACE_HYPOTF''@|0|g' \
| -e 's|@''REPLACE_HYPOTL''@|0|g' \
| -e 's|@''REPLACE_ILOGB''@|0|g' \
| -e 's|@''REPLACE_ILOGBF''@|0|g' \
| -e 's|@''REPLACE_ISFINITE''@|0|g' \
| -e 's|@''REPLACE_ISINF''@|0|g' \
| -e 's|@''REPLACE_ISNAN''@|0|g' \
| -e 's|@''REPLACE_ITOLD''@|0|g' \
| -e 's|@''REPLACE_LDEXPL''@|0|g' \
| -e 's|@''REPLACE_LOG''@|0|g' \
| -e 's|@''REPLACE_LOGF''@|0|g' \
| -e 's|@''REPLACE_LOGL''@|0|g' \
| -e 's|@''REPLACE_LOG10''@|0|g' \
| -e 's|@''REPLACE_LOG10F''@|0|g' \
| -e 's|@''REPLACE_LOG10L''@|0|g' \
| -e 's|@''REPLACE_LOG1P''@|0|g' \
| -e 's|@''REPLACE_LOG1PF''@|0|g' \
| -e 's|@''REPLACE_LOG1PL''@|0|g' \
| -e 's|@''REPLACE_LOG2''@|0|g' \
| -e 's|@''REPLACE_LOG2F''@|0|g' \
| -e 's|@''REPLACE_LOG2L''@|0|g' \
| -e 's|@''REPLACE_LOGB''@|0|g' \
| -e 's|@''REPLACE_LOGBF''@|0|g' \
| -e 's|@''REPLACE_LOGBL''@|0|g' \
| -e 's|@''REPLACE_MODF''@|0|g' \
| -e 's|@''REPLACE_MODFF''@|0|g' \
| -e 's|@''REPLACE_MODFL''@|0|g' \
| -e 's|@''REPLACE_NAN''@|0|g' \
| -e 's|@''REPLACE_REMAINDER''@|0|g' \
| -e 's|@''REPLACE_REMAINDERF''@|0|g' \
| -e 's|@''REPLACE_REMAINDERL''@|0|g' \
| -e 's|@''REPLACE_ROUND''@|0|g' \
| -e 's|@''REPLACE_ROUNDF''@|0|g' \
| -e 's|@''REPLACE_ROUNDL''@|0|g' \
| -e 's|@''REPLACE_SIGNBIT''@|0|g' \
| -e 's|@''REPLACE_SIGNBIT_USING_GCC''@|1|g' \
| -e 's|@''REPLACE_SINF''@|0|g' \
| -e 's|@''REPLACE_SINHF''@|0|g' \
| -e 's|@''REPLACE_SQRTF''@|0|g' \
| -e 's|@''REPLACE_SQRTL''@|0|g' \
| -e 's|@''REPLACE_TANF''@|0|g' \
| -e 's|@''REPLACE_TANHF''@|0|g' \
| -e 's|@''REPLACE_TRUNC''@|0|g' \
| -e 's|@''REPLACE_TRUNCF''@|0|g' \
| -e 's|@''REPLACE_TRUNCL''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h'; \
| } > math.h-t && \
| mv math.h-t math.h
| rm -f signal.h-t signal.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */' && \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_SIGNAL_H''@|<signal.h>|g' \
| -e 's|@''GNULIB_PTHREAD_SIGMASK''@|0|g' \
| -e 's|@''GNULIB_RAISE''@|1|g' \
| -e 's/@''GNULIB_SIGNAL_H_SIGPIPE''@/1/g' \
| -e 's/@''GNULIB_SIGPROCMASK''@/1/g' \
| -e 's/@''GNULIB_SIGACTION''@/1/g' \
| -e 's|@''HAVE_POSIX_SIGNALBLOCKING''@|1|g' \
| -e 's|@''HAVE_PTHREAD_SIGMASK''@|1|g' \
| -e 's|@''HAVE_RAISE''@|1|g' \
| -e 's|@''HAVE_SIGSET_T''@|1|g' \
| -e 's|@''HAVE_SIGINFO_T''@|1|g' \
| -e 's|@''HAVE_SIGACTION''@|1|g' \
| -e 's|@''HAVE_STRUCT_SIGACTION_SA_SIGACTION''@|1|g' \
| -e 's|@''HAVE_TYPE_VOLATILE_SIG_ATOMIC_T''@|1|g' \
| -e 's|@''HAVE_SIGHANDLER_T''@|1|g' \
| -e 's|@''REPLACE_PTHREAD_SIGMASK''@|0|g' \
| -e 's|@''REPLACE_RAISE''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/signal.in.h; \
| } > signal.h-t && \
| mv signal.h-t signal.h
| rm -f spawn.h-t spawn.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''HAVE_SPAWN_H''@|1|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_SPAWN_H''@|<spawn.h>|g' \
| -e 's/@''GNULIB_POSIX_SPAWN''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNP''@/1/g' \
| -e 's/@''GNULIB_POSIX_SPAWN_FILE_ACTIONS_INIT''@/1/g' \
| -e 's/@''GNULIB_POSIX_SPAWN_FILE_ACTIONS_ADDCLOSE''@/1/g' \
| -e 's/@''GNULIB_POSIX_SPAWN_FILE_ACTIONS_ADDDUP2''@/1/g' \
| -e 's/@''GNULIB_POSIX_SPAWN_FILE_ACTIONS_ADDOPEN''@/1/g' \
| -e 's/@''GNULIB_POSIX_SPAWN_FILE_ACTIONS_DESTROY''@/1/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_INIT''@/1/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_GETFLAGS''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_SETFLAGS''@/1/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_GETPGROUP''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_SETPGROUP''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_GETSCHEDPARAM''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_SETSCHEDPARAM''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_GETSCHEDPOLICY''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_SETSCHEDPOLICY''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_GETSIGDEFAULT''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_SETSIGDEFAULT''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_GETSIGMASK''@/0/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_SETSIGMASK''@/1/g' \
| -e 's/@''GNULIB_POSIX_SPAWNATTR_DESTROY''@/1/g' \
| -e 's|@''HAVE_POSIX_SPAWN''@|1|g' \
| -e 's|@''HAVE_POSIX_SPAWNATTR_T''@|1|g' \
| -e 's|@''HAVE_POSIX_SPAWN_FILE_ACTIONS_T''@|1|g' \
| -e 's|@''REPLACE_POSIX_SPAWN''@|0|g' \
| -e 's|@''REPLACE_POSIX_SPAWN_FILE_ACTIONS_ADDCLOSE''@|0|g' \
| -e 's|@''REPLACE_POSIX_SPAWN_FILE_ACTIONS_ADDDUP2''@|0|g' \
| -e 's|@''REPLACE_POSIX_SPAWN_FILE_ACTIONS_ADDOPEN''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/spawn.in.h; \
| } > spawn.h-t && \
| mv spawn.h-t spawn.h
| rm -f stdio.h-t stdio.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */' && \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_STDIO_H''@|<stdio.h>|g' \
| -e 's/@''GNULIB_DPRINTF''@/0/g' \
| -e 's/@''GNULIB_FCLOSE''@/1/g' \
| -e 's/@''GNULIB_FDOPEN''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_FFLUSH''@/1/g' \
| -e 's/@''GNULIB_FGETC''@/1/g' \
| -e 's/@''GNULIB_FGETS''@/1/g' \
| -e 's/@''GNULIB_FOPEN''@/1/g' \
| -e 's/@''GNULIB_FPRINTF''@/1/g' \
| -e 's/@''GNULIB_FPRINTF_POSIX''@/0/g' \
| -e 's/@''GNULIB_FPURGE''@/1/g' \
| -e 's/@''GNULIB_FPUTC''@/1/g' \
| -e 's/@''GNULIB_FPUTS''@/1/g' \
| -e 's/@''GNULIB_FREAD''@/1/g' \
| -e 's/@''GNULIB_FREOPEN''@/0/g' \
| -e 's/@''GNULIB_FSCANF''@/1/g' \
| -e 's/@''GNULIB_FSEEK''@/1/g' \
| -e 's/@''GNULIB_FSEEKO''@/1/g' \
| -e 's/@''GNULIB_FTELL''@/1/g' \
| -e 's/@''GNULIB_FTELLO''@/1/g' \
| -e 's/@''GNULIB_FWRITE''@/1/g' \
| -e 's/@''GNULIB_GETC''@/1/g' \
| -e 's/@''GNULIB_GETCHAR''@/1/g' \
| -e 's/@''GNULIB_GETDELIM''@/0/g' \
| -e 's/@''GNULIB_GETLINE''@/0/g' \
| -e 's/@''GNULIB_OBSTACK_PRINTF''@/0/g' \
| -e 's/@''GNULIB_OBSTACK_PRINTF_POSIX''@/0/g' \
| -e 's/@''GNULIB_PCLOSE''@/0/g' \
| -e 's/@''GNULIB_PERROR''@/0/g' \
| -e 's/@''GNULIB_POPEN''@/0/g' \
| -e 's/@''GNULIB_PRINTF''@/1/g' \
| -e 's/@''GNULIB_PRINTF_POSIX''@/0/g' \
| -e 's/@''GNULIB_PUTC''@/1/g' \
| -e 's/@''GNULIB_PUTCHAR''@/1/g' \
| -e 's/@''GNULIB_PUTS''@/1/g' \
| -e 's/@''GNULIB_REMOVE''@/0/g' \
| -e 's/@''GNULIB_RENAME''@/1/g' \
| -e 's/@''GNULIB_RENAMEAT''@/0/g' \
| -e 's/@''GNULIB_SCANF''@/1/g' \
| -e 's/@''GNULIB_SNPRINTF''@/1/g' \
| -e 's/@''GNULIB_SPRINTF_POSIX''@/0/g' \
| -e 's/@''GNULIB_STDIO_H_NONBLOCKING''@/0/g' \
| -e 's/@''GNULIB_STDIO_H_SIGPIPE''@/1/g' \
| -e 's/@''GNULIB_TMPFILE''@/0/g' \
| -e 's/@''GNULIB_VASPRINTF''@/1/g' \
| -e 's/@''GNULIB_VDPRINTF''@/0/g' \
| -e 's/@''GNULIB_VFPRINTF''@/1/g' \
| -e 's/@''GNULIB_VFPRINTF_POSIX''@/0/g' \
| -e 's/@''GNULIB_VFSCANF''@/0/g' \
| -e 's/@''GNULIB_VSCANF''@/0/g' \
| -e 's/@''GNULIB_VPRINTF''@/1/g' \
| -e 's/@''GNULIB_VPRINTF_POSIX''@/0/g' \
| -e 's/@''GNULIB_VSNPRINTF''@/0/g' \
| -e 's/@''GNULIB_VSPRINTF_POSIX''@/0/g' \
| < ../../m4-1.4.18/lib/stdio.in.h | \
| sed -e 's|@''HAVE_DECL_FPURGE''@|0|g' \
| -e 's|@''HAVE_DECL_FSEEKO''@|1|g' \
| -e 's|@''HAVE_DECL_FTELLO''@|1|g' \
| -e 's|@''HAVE_DECL_GETDELIM''@|1|g' \
| -e 's|@''HAVE_DECL_GETLINE''@|1|g' \
| -e 's|@''HAVE_DECL_OBSTACK_PRINTF''@|1|g' \
| -e 's|@''HAVE_DECL_SNPRINTF''@|1|g' \
| -e 's|@''HAVE_DECL_VSNPRINTF''@|1|g' \
| -e 's|@''HAVE_DPRINTF''@|1|g' \
| -e 's|@''HAVE_FSEEKO''@|1|g' \
| -e 's|@''HAVE_FTELLO''@|1|g' \
| -e 's|@''HAVE_PCLOSE''@|1|g' \
| -e 's|@''HAVE_POPEN''@|1|g' \
| -e 's|@''HAVE_RENAMEAT''@|1|g' \
| -e 's|@''HAVE_VASPRINTF''@|1|g' \
| -e 's|@''HAVE_VDPRINTF''@|1|g' \
| -e 's|@''REPLACE_DPRINTF''@|0|g' \
| -e 's|@''REPLACE_FCLOSE''@|1|g' \
| -e 's|@''REPLACE_FDOPEN''@|0|g' \
| -e 's|@''REPLACE_FFLUSH''@|1|g' \
| -e 's|@''REPLACE_FOPEN''@|0|g' \
| -e 's|@''REPLACE_FPRINTF''@|0|g' \
| -e 's|@''REPLACE_FPURGE''@|0|g' \
| -e 's|@''REPLACE_FREOPEN''@|0|g' \
| -e 's|@''REPLACE_FSEEK''@|1|g' \
| -e 's|@''REPLACE_FSEEKO''@|1|g' \
| -e 's|@''REPLACE_FTELL''@|0|g' \
| -e 's|@''REPLACE_FTELLO''@|0|g' \
| -e 's|@''REPLACE_GETDELIM''@|0|g' \
| -e 's|@''REPLACE_GETLINE''@|0|g' \
| -e 's|@''REPLACE_OBSTACK_PRINTF''@|0|g' \
| -e 's|@''REPLACE_PERROR''@|0|g' \
| -e 's|@''REPLACE_POPEN''@|0|g' \
| -e 's|@''REPLACE_PRINTF''@|0|g' \
| -e 's|@''REPLACE_REMOVE''@|0|g' \
| -e 's|@''REPLACE_RENAME''@|0|g' \
| -e 's|@''REPLACE_RENAMEAT''@|0|g' \
| -e 's|@''REPLACE_SNPRINTF''@|0|g' \
| -e 's|@''REPLACE_SPRINTF''@|0|g' \
| -e 's|@''REPLACE_STDIO_READ_FUNCS''@|0|g' \
| -e 's|@''REPLACE_STDIO_WRITE_FUNCS''@|0|g' \
| -e 's|@''REPLACE_TMPFILE''@|0|g' \
| -e 's|@''REPLACE_VASPRINTF''@|1|g' \
| -e 's|@''REPLACE_VDPRINTF''@|0|g' \
| -e 's|@''REPLACE_VFPRINTF''@|0|g' \
| -e 's|@''REPLACE_VPRINTF''@|0|g' \
| -e 's|@''REPLACE_VSNPRINTF''@|0|g' \
| -e 's|@''REPLACE_VSPRINTF''@|0|g' \
| -e 's|@''ASM_SYMBOL_PREFIX''@|""|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h'; \
| } > stdio.h-t && \
| mv stdio.h-t stdio.h
| rm -f stdlib.h-t stdlib.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */' && \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_STDLIB_H''@|<stdlib.h>|g' \
| -e 's/@''GNULIB__EXIT''@/0/g' \
| -e 's/@''GNULIB_ATOLL''@/0/g' \
| -e 's/@''GNULIB_CALLOC_POSIX''@/0/g' \
| -e 's/@''GNULIB_CANONICALIZE_FILE_NAME''@/1/g' \
| -e 's/@''GNULIB_GETLOADAVG''@/0/g' \
| -e 's/@''GNULIB_GETSUBOPT''@/0/g' \
| -e 's/@''GNULIB_GRANTPT''@/0/g' \
| -e 's/@''GNULIB_MALLOC_POSIX''@/1/g' \
| -e 's/@''GNULIB_MBTOWC''@/1/g' \
| -e 's/@''GNULIB_MKDTEMP''@/1/g' \
| -e 's/@''GNULIB_MKOSTEMP''@/0/g' \
| -e 's/@''GNULIB_MKOSTEMPS''@/0/g' \
| -e 's/@''GNULIB_MKSTEMP''@/1/g' \
| -e 's/@''GNULIB_MKSTEMPS''@/0/g' \
| -e 's/@''GNULIB_POSIX_OPENPT''@/0/g' \
| -e 's/@''GNULIB_PTSNAME''@/0/g' \
| -e 's/@''GNULIB_PTSNAME_R''@/0/g' \
| -e 's/@''GNULIB_PUTENV''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_QSORT_R''@/0/g' \
| -e 's/@''GNULIB_RANDOM''@/0/g' \
| -e 's/@''GNULIB_RANDOM_R''@/0/g' \
| -e 's/@''GNULIB_REALLOC_POSIX''@/0/g' \
| -e 's/@''GNULIB_REALPATH''@/1/g' \
| -e 's/@''GNULIB_RPMATCH''@/0/g' \
| -e 's/@''GNULIB_SECURE_GETENV''@/1/g' \
| -e 's/@''GNULIB_SETENV''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_STRTOD''@/1/g' \
| -e 's/@''GNULIB_STRTOLL''@/0/g' \
| -e 's/@''GNULIB_STRTOULL''@/0/g' \
| -e 's/@''GNULIB_SYSTEM_POSIX''@/0/g' \
| -e 's/@''GNULIB_UNLOCKPT''@/0/g' \
| -e 's/@''GNULIB_UNSETENV''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_WCTOMB''@/IN_M4_GNULIB_TESTS/g' \
| < ../../m4-1.4.18/lib/stdlib.in.h | \
| sed -e 's|@''HAVE__EXIT''@|1|g' \
| -e 's|@''HAVE_ATOLL''@|1|g' \
| -e 's|@''HAVE_CANONICALIZE_FILE_NAME''@|1|g' \
| -e 's|@''HAVE_DECL_GETLOADAVG''@|1|g' \
| -e 's|@''HAVE_GETSUBOPT''@|1|g' \
| -e 's|@''HAVE_GRANTPT''@|1|g' \
| -e 's|@''HAVE_MKDTEMP''@|1|g' \
| -e 's|@''HAVE_MKOSTEMP''@|1|g' \
| -e 's|@''HAVE_MKOSTEMPS''@|1|g' \
| -e 's|@''HAVE_MKSTEMP''@|1|g' \
| -e 's|@''HAVE_MKSTEMPS''@|1|g' \
| -e 's|@''HAVE_POSIX_OPENPT''@|1|g' \
| -e 's|@''HAVE_PTSNAME''@|1|g' \
| -e 's|@''HAVE_PTSNAME_R''@|1|g' \
| -e 's|@''HAVE_QSORT_R''@|1|g' \
| -e 's|@''HAVE_RANDOM''@|1|g' \
| -e 's|@''HAVE_RANDOM_H''@|1|g' \
| -e 's|@''HAVE_RANDOM_R''@|1|g' \
| -e 's|@''HAVE_REALPATH''@|1|g' \
| -e 's|@''HAVE_RPMATCH''@|1|g' \
| -e 's|@''HAVE_SECURE_GETENV''@|1|g' \
| -e 's|@''HAVE_DECL_SETENV''@|1|g' \
| -e 's|@''HAVE_STRTOD''@|1|g' \
| -e 's|@''HAVE_STRTOLL''@|1|g' \
| -e 's|@''HAVE_STRTOULL''@|1|g' \
| -e 's|@''HAVE_STRUCT_RANDOM_DATA''@|1|g' \
| -e 's|@''HAVE_SYS_LOADAVG_H''@|0|g' \
| -e 's|@''HAVE_UNLOCKPT''@|1|g' \
| -e 's|@''HAVE_DECL_UNSETENV''@|1|g' \
| -e 's|@''REPLACE_CALLOC''@|0|g' \
| -e 's|@''REPLACE_CANONICALIZE_FILE_NAME''@|0|g' \
| -e 's|@''REPLACE_MALLOC''@|0|g' \
| -e 's|@''REPLACE_MBTOWC''@|0|g' \
| -e 's|@''REPLACE_MKSTEMP''@|0|g' \
| -e 's|@''REPLACE_PTSNAME''@|0|g' \
| -e 's|@''REPLACE_PTSNAME_R''@|0|g' \
| -e 's|@''REPLACE_PUTENV''@|0|g' \
| -e 's|@''REPLACE_QSORT_R''@|0|g' \
| -e 's|@''REPLACE_RANDOM_R''@|0|g' \
| -e 's|@''REPLACE_REALLOC''@|0|g' \
| -e 's|@''REPLACE_REALPATH''@|0|g' \
| -e 's|@''REPLACE_SETENV''@|0|g' \
| -e 's|@''REPLACE_STRTOD''@|0|g' \
| -e 's|@''REPLACE_UNSETENV''@|0|g' \
| -e 's|@''REPLACE_WCTOMB''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _Noreturn/r ../../m4-1.4.18/build-aux/snippet/_Noreturn.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h'; \
| } > stdlib.h-t && \
| mv stdlib.h-t stdlib.h
| rm -f string.h-t string.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */' && \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_STRING_H''@|<string.h>|g' \
| -e 's/@''GNULIB_FFSL''@/0/g' \
| -e 's/@''GNULIB_FFSLL''@/0/g' \
| -e 's/@''GNULIB_MBSLEN''@/0/g' \
| -e 's/@''GNULIB_MBSNLEN''@/0/g' \
| -e 's/@''GNULIB_MBSCHR''@/0/g' \
| -e 's/@''GNULIB_MBSRCHR''@/0/g' \
| -e 's/@''GNULIB_MBSSTR''@/0/g' \
| -e 's/@''GNULIB_MBSCASECMP''@/0/g' \
| -e 's/@''GNULIB_MBSNCASECMP''@/0/g' \
| -e 's/@''GNULIB_MBSPCASECMP''@/0/g' \
| -e 's/@''GNULIB_MBSCASESTR''@/0/g' \
| -e 's/@''GNULIB_MBSCSPN''@/0/g' \
| -e 's/@''GNULIB_MBSPBRK''@/0/g' \
| -e 's/@''GNULIB_MBSSPN''@/0/g' \
| -e 's/@''GNULIB_MBSSEP''@/0/g' \
| -e 's/@''GNULIB_MBSTOK_R''@/0/g' \
| -e 's/@''GNULIB_MEMCHR''@/1/g' \
| -e 's/@''GNULIB_MEMMEM''@/0/g' \
| -e 's/@''GNULIB_MEMPCPY''@/0/g' \
| -e 's/@''GNULIB_MEMRCHR''@/0/g' \
| -e 's/@''GNULIB_RAWMEMCHR''@/1/g' \
| -e 's/@''GNULIB_STPCPY''@/0/g' \
| -e 's/@''GNULIB_STPNCPY''@/0/g' \
| -e 's/@''GNULIB_STRCHRNUL''@/1/g' \
| -e 's/@''GNULIB_STRDUP''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_STRNCAT''@/0/g' \
| -e 's/@''GNULIB_STRNDUP''@/1/g' \
| -e 's/@''GNULIB_STRNLEN''@/1/g' \
| -e 's/@''GNULIB_STRPBRK''@/0/g' \
| -e 's/@''GNULIB_STRSEP''@/0/g' \
| -e 's/@''GNULIB_STRSTR''@/1/g' \
| -e 's/@''GNULIB_STRCASESTR''@/0/g' \
| -e 's/@''GNULIB_STRTOK_R''@/0/g' \
| -e 's/@''GNULIB_STRERROR''@/1/g' \
| -e 's/@''GNULIB_STRERROR_R''@/0/g' \
| -e 's/@''GNULIB_STRSIGNAL''@/1/g' \
| -e 's/@''GNULIB_STRVERSCMP''@/0/g' \
| < ../../m4-1.4.18/lib/string.in.h | \
| sed -e 's|@''HAVE_FFSL''@|1|g' \
| -e 's|@''HAVE_FFSLL''@|1|g' \
| -e 's|@''HAVE_MBSLEN''@|0|g' \
| -e 's|@''HAVE_MEMCHR''@|1|g' \
| -e 's|@''HAVE_DECL_MEMMEM''@|1|g' \
| -e 's|@''HAVE_MEMPCPY''@|1|g' \
| -e 's|@''HAVE_DECL_MEMRCHR''@|1|g' \
| -e 's|@''HAVE_RAWMEMCHR''@|1|g' \
| -e 's|@''HAVE_STPCPY''@|1|g' \
| -e 's|@''HAVE_STPNCPY''@|1|g' \
| -e 's|@''HAVE_STRCHRNUL''@|1|g' \
| -e 's|@''HAVE_DECL_STRDUP''@|1|g' \
| -e 's|@''HAVE_DECL_STRNDUP''@|1|g' \
| -e 's|@''HAVE_DECL_STRNLEN''@|1|g' \
| -e 's|@''HAVE_STRPBRK''@|1|g' \
| -e 's|@''HAVE_STRSEP''@|1|g' \
| -e 's|@''HAVE_STRCASESTR''@|1|g' \
| -e 's|@''HAVE_DECL_STRTOK_R''@|1|g' \
| -e 's|@''HAVE_DECL_STRERROR_R''@|1|g' \
| -e 's|@''HAVE_DECL_STRSIGNAL''@|1|g' \
| -e 's|@''HAVE_STRVERSCMP''@|1|g' \
| -e 's|@''REPLACE_STPNCPY''@|0|g' \
| -e 's|@''REPLACE_MEMCHR''@|0|g' \
| -e 's|@''REPLACE_MEMMEM''@|0|g' \
| -e 's|@''REPLACE_STRCASESTR''@|0|g' \
| -e 's|@''REPLACE_STRCHRNUL''@|0|g' \
| -e 's|@''REPLACE_STRDUP''@|0|g' \
| -e 's|@''REPLACE_STRSTR''@|0|g' \
| -e 's|@''REPLACE_STRERROR''@|0|g' \
| -e 's|@''REPLACE_STRERROR_R''@|0|g' \
| -e 's|@''REPLACE_STRNCAT''@|0|g' \
| -e 's|@''REPLACE_STRNDUP''@|0|g' \
| -e 's|@''REPLACE_STRNLEN''@|0|g' \
| -e 's|@''REPLACE_STRSIGNAL''@|0|g' \
| -e 's|@''REPLACE_STRTOK_R''@|0|g' \
| -e 's|@''UNDEFINE_STRTOK_R''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h'; \
| < ../../m4-1.4.18/lib/string.in.h; \
| } > string.h-t && \
| mv string.h-t string.h
| /home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/hosttools/mkdir -p sys
| /home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/hosttools/mkdir -p sys
| rm -f sys/stat.h-t sys/stat.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_SYS_STAT_H''@|<sys/stat.h>|g' \
| -e 's|@''WINDOWS_64_BIT_ST_SIZE''@|0|g' \
| -e 's/@''GNULIB_FCHMODAT''@/0/g' \
| -e 's/@''GNULIB_FSTAT''@/1/g' \
| -e 's/@''GNULIB_FSTATAT''@/0/g' \
| -e 's/@''GNULIB_FUTIMENS''@/0/g' \
| -e 's/@''GNULIB_LCHMOD''@/0/g' \
| -e 's/@''GNULIB_LSTAT''@/1/g' \
| -e 's/@''GNULIB_MKDIRAT''@/0/g' \
| -e 's/@''GNULIB_MKFIFO''@/0/g' \
| -e 's/@''GNULIB_MKFIFOAT''@/0/g' \
| -e 's/@''GNULIB_MKNOD''@/0/g' \
| -e 's/@''GNULIB_MKNODAT''@/0/g' \
| -e 's/@''GNULIB_STAT''@/1/g' \
| -e 's/@''GNULIB_UTIMENSAT''@/0/g' \
| -e 's|@''HAVE_FCHMODAT''@|1|g' \
| -e 's|@''HAVE_FSTATAT''@|1|g' \
| -e 's|@''HAVE_FUTIMENS''@|1|g' \
| -e 's|@''HAVE_LCHMOD''@|1|g' \
| -e 's|@''HAVE_LSTAT''@|1|g' \
| -e 's|@''HAVE_MKDIRAT''@|1|g' \
| -e 's|@''HAVE_MKFIFO''@|1|g' \
| -e 's|@''HAVE_MKFIFOAT''@|1|g' \
| -e 's|@''HAVE_MKNOD''@|1|g' \
| -e 's|@''HAVE_MKNODAT''@|1|g' \
| -e 's|@''HAVE_UTIMENSAT''@|1|g' \
| -e 's|@''REPLACE_FSTAT''@|0|g' \
| -e 's|@''REPLACE_FSTATAT''@|0|g' \
| -e 's|@''REPLACE_FUTIMENS''@|0|g' \
| -e 's|@''REPLACE_LSTAT''@|0|g' \
| -e 's|@''REPLACE_MKDIR''@|0|g' \
| -e 's|@''REPLACE_MKFIFO''@|0|g' \
| -e 's|@''REPLACE_MKNOD''@|0|g' \
| -e 's|@''REPLACE_STAT''@|0|g' \
| -e 's|@''REPLACE_UTIMENSAT''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/sys_stat.in.h; \
| } > sys/stat.h-t && \
| mv sys/stat.h-t sys/stat.h
| rm -f sys/time.h-t sys/time.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's/@''HAVE_SYS_TIME_H''@/1/g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_SYS_TIME_H''@|<sys/time.h>|g' \
| -e 's/@''GNULIB_GETTIMEOFDAY''@/1/g' \
| -e 's|@''HAVE_WINSOCK2_H''@|0|g' \
| -e 's/@''HAVE_GETTIMEOFDAY''@/1/g' \
| -e 's/@''HAVE_STRUCT_TIMEVAL''@/1/g' \
| -e 's/@''REPLACE_GETTIMEOFDAY''@/0/g' \
| -e 's/@''REPLACE_STRUCT_TIMEVAL''@/0/g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/sys_time.in.h; \
| } > sys/time.h-t && \
| mv sys/time.h-t sys/time.h
| /home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/hosttools/mkdir -p sys
| rm -f sys/wait.h-t sys/wait.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_SYS_WAIT_H''@|<sys/wait.h>|g' \
| -e 's/@''GNULIB_WAITPID''@/1/g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/sys_wait.in.h; \
| } > sys/wait.h-t && \
| mv sys/wait.h-t sys/wait.h
| rm -f time.h-t time.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */' && \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_TIME_H''@|<time.h>|g' \
| -e 's/@''GNULIB_GETTIMEOFDAY''@/1/g' \
| -e 's/@''GNULIB_MKTIME''@/0/g' \
| -e 's/@''GNULIB_NANOSLEEP''@/0/g' \
| -e 's/@''GNULIB_STRPTIME''@/0/g' \
| -e 's/@''GNULIB_TIMEGM''@/0/g' \
| -e 's/@''GNULIB_TIME_R''@/0/g' \
| -e 's/@''GNULIB_TIME_RZ''@/0/g' \
| -e 's|@''HAVE_DECL_LOCALTIME_R''@|1|g' \
| -e 's|@''HAVE_NANOSLEEP''@|1|g' \
| -e 's|@''HAVE_STRPTIME''@|1|g' \
| -e 's|@''HAVE_TIMEGM''@|1|g' \
| -e 's|@''HAVE_TIMEZONE_T''@|0|g' \
| -e 's|@''REPLACE_GMTIME''@|0|g' \
| -e 's|@''REPLACE_LOCALTIME''@|0|g' \
| -e 's|@''REPLACE_LOCALTIME_R''@|GNULIB_PORTCHECK|g' \
| -e 's|@''REPLACE_MKTIME''@|GNULIB_PORTCHECK|g' \
| -e 's|@''REPLACE_NANOSLEEP''@|GNULIB_PORTCHECK|g' \
| -e 's|@''REPLACE_TIMEGM''@|GNULIB_PORTCHECK|g' \
| -e 's|@''PTHREAD_H_DEFINES_STRUCT_TIMESPEC''@|0|g' \
| -e 's|@''SYS_TIME_H_DEFINES_STRUCT_TIMESPEC''@|0|g' \
| -e 's|@''TIME_H_DEFINES_STRUCT_TIMESPEC''@|1|g' \
| -e 's|@''UNISTD_H_DEFINES_STRUCT_TIMESPEC''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/time.in.h; \
| } > time.h-t && \
| mv time.h-t time.h
| rm -f unistd.h-t unistd.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''HAVE_UNISTD_H''@|1|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_UNISTD_H''@|<unistd.h>|g' \
| -e 's|@''WINDOWS_64_BIT_OFF_T''@|0|g' \
| -e 's/@''GNULIB_CHDIR''@/1/g' \
| -e 's/@''GNULIB_CHOWN''@/0/g' \
| -e 's/@''GNULIB_CLOSE''@/1/g' \
| -e 's/@''GNULIB_DUP''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_DUP2''@/1/g' \
| -e 's/@''GNULIB_DUP3''@/0/g' \
| -e 's/@''GNULIB_ENVIRON''@/1/g' \
| -e 's/@''GNULIB_EUIDACCESS''@/0/g' \
| -e 's/@''GNULIB_FACCESSAT''@/0/g' \
| -e 's/@''GNULIB_FCHDIR''@/0/g' \
| -e 's/@''GNULIB_FCHOWNAT''@/0/g' \
| -e 's/@''GNULIB_FDATASYNC''@/0/g' \
| -e 's/@''GNULIB_FSYNC''@/0/g' \
| -e 's/@''GNULIB_FTRUNCATE''@/0/g' \
| -e 's/@''GNULIB_GETCWD''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_GETDOMAINNAME''@/0/g' \
| -e 's/@''GNULIB_GETDTABLESIZE''@/1/g' \
| -e 's/@''GNULIB_GETGROUPS''@/0/g' \
| -e 's/@''GNULIB_GETHOSTNAME''@/0/g' \
| -e 's/@''GNULIB_GETLOGIN''@/0/g' \
| -e 's/@''GNULIB_GETLOGIN_R''@/0/g' \
| -e 's/@''GNULIB_GETPAGESIZE''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_GETUSERSHELL''@/0/g' \
| -e 's/@''GNULIB_GROUP_MEMBER''@/0/g' \
| -e 's/@''GNULIB_ISATTY''@/0/g' \
| -e 's/@''GNULIB_LCHOWN''@/0/g' \
| -e 's/@''GNULIB_LINK''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_LINKAT''@/0/g' \
| -e 's/@''GNULIB_LSEEK''@/1/g' \
| -e 's/@''GNULIB_PIPE''@/0/g' \
| -e 's/@''GNULIB_PIPE2''@/1/g' \
| -e 's/@''GNULIB_PREAD''@/0/g' \
| -e 's/@''GNULIB_PWRITE''@/0/g' \
| -e 's/@''GNULIB_READ''@/0/g' \
| -e 's/@''GNULIB_READLINK''@/1/g' \
| -e 's/@''GNULIB_READLINKAT''@/0/g' \
| -e 's/@''GNULIB_RMDIR''@/1/g' \
| -e 's/@''GNULIB_SETHOSTNAME''@/0/g' \
| -e 's/@''GNULIB_SLEEP''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_SYMLINK''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_SYMLINKAT''@/0/g' \
| -e 's/@''GNULIB_TTYNAME_R''@/0/g' \
| -e 's/@''GNULIB_UNISTD_H_GETOPT''@/0/g' \
| -e 's/@''GNULIB_UNISTD_H_NONBLOCKING''@/0/g' \
| -e 's/@''GNULIB_UNISTD_H_SIGPIPE''@/1/g' \
| -e 's/@''GNULIB_UNLINK''@/0/g' \
| -e 's/@''GNULIB_UNLINKAT''@/0/g' \
| -e 's/@''GNULIB_USLEEP''@/0/g' \
| -e 's/@''GNULIB_WRITE''@/IN_M4_GNULIB_TESTS/g' \
| < ../../m4-1.4.18/lib/unistd.in.h | \
| sed -e 's|@''HAVE_CHOWN''@|1|g' \
| -e 's|@''HAVE_DUP2''@|1|g' \
| -e 's|@''HAVE_DUP3''@|1|g' \
| -e 's|@''HAVE_EUIDACCESS''@|1|g' \
| -e 's|@''HAVE_FACCESSAT''@|1|g' \
| -e 's|@''HAVE_FCHDIR''@|1|g' \
| -e 's|@''HAVE_FCHOWNAT''@|1|g' \
| -e 's|@''HAVE_FDATASYNC''@|1|g' \
| -e 's|@''HAVE_FSYNC''@|1|g' \
| -e 's|@''HAVE_FTRUNCATE''@|1|g' \
| -e 's|@''HAVE_GETDTABLESIZE''@|1|g' \
| -e 's|@''HAVE_GETGROUPS''@|1|g' \
| -e 's|@''HAVE_GETHOSTNAME''@|1|g' \
| -e 's|@''HAVE_GETPAGESIZE''@|1|g' \
| -e 's|@''HAVE_GROUP_MEMBER''@|1|g' \
| -e 's|@''HAVE_LCHOWN''@|1|g' \
| -e 's|@''HAVE_LINK''@|1|g' \
| -e 's|@''HAVE_LINKAT''@|1|g' \
| -e 's|@''HAVE_PIPE''@|1|g' \
| -e 's|@''HAVE_PIPE2''@|1|g' \
| -e 's|@''HAVE_PREAD''@|1|g' \
| -e 's|@''HAVE_PWRITE''@|1|g' \
| -e 's|@''HAVE_READLINK''@|1|g' \
| -e 's|@''HAVE_READLINKAT''@|1|g' \
| -e 's|@''HAVE_SETHOSTNAME''@|1|g' \
| -e 's|@''HAVE_SLEEP''@|1|g' \
| -e 's|@''HAVE_SYMLINK''@|1|g' \
| -e 's|@''HAVE_SYMLINKAT''@|1|g' \
| -e 's|@''HAVE_UNLINKAT''@|1|g' \
| -e 's|@''HAVE_USLEEP''@|1|g' \
| -e 's|@''HAVE_DECL_ENVIRON''@|1|g' \
| -e 's|@''HAVE_DECL_FCHDIR''@|1|g' \
| -e 's|@''HAVE_DECL_FDATASYNC''@|1|g' \
| -e 's|@''HAVE_DECL_GETDOMAINNAME''@|1|g' \
| -e 's|@''HAVE_DECL_GETLOGIN''@|1|g' \
| -e 's|@''HAVE_DECL_GETLOGIN_R''@|1|g' \
| -e 's|@''HAVE_DECL_GETPAGESIZE''@|1|g' \
| -e 's|@''HAVE_DECL_GETUSERSHELL''@|1|g' \
| -e 's|@''HAVE_DECL_SETHOSTNAME''@|1|g' \
| -e 's|@''HAVE_DECL_TTYNAME_R''@|1|g' \
| -e 's|@''HAVE_OS_H''@|0|g' \
| -e 's|@''HAVE_SYS_PARAM_H''@|0|g' \
| | \
| sed -e 's|@''REPLACE_CHOWN''@|0|g' \
| -e 's|@''REPLACE_CLOSE''@|0|g' \
| -e 's|@''REPLACE_DUP''@|0|g' \
| -e 's|@''REPLACE_DUP2''@|0|g' \
| -e 's|@''REPLACE_FCHOWNAT''@|0|g' \
| -e 's|@''REPLACE_FTRUNCATE''@|0|g' \
| -e 's|@''REPLACE_GETCWD''@|0|g' \
| -e 's|@''REPLACE_GETDOMAINNAME''@|0|g' \
| -e 's|@''REPLACE_GETDTABLESIZE''@|0|g' \
| -e 's|@''REPLACE_GETLOGIN_R''@|0|g' \
| -e 's|@''REPLACE_GETGROUPS''@|0|g' \
| -e 's|@''REPLACE_GETPAGESIZE''@|0|g' \
| -e 's|@''REPLACE_ISATTY''@|0|g' \
| -e 's|@''REPLACE_LCHOWN''@|0|g' \
| -e 's|@''REPLACE_LINK''@|0|g' \
| -e 's|@''REPLACE_LINKAT''@|0|g' \
| -e 's|@''REPLACE_LSEEK''@|0|g' \
| -e 's|@''REPLACE_PREAD''@|0|g' \
| -e 's|@''REPLACE_PWRITE''@|0|g' \
| -e 's|@''REPLACE_READ''@|0|g' \
| -e 's|@''REPLACE_READLINK''@|0|g' \
| -e 's|@''REPLACE_READLINKAT''@|0|g' \
| -e 's|@''REPLACE_RMDIR''@|0|g' \
| -e 's|@''REPLACE_SLEEP''@|0|g' \
| -e 's|@''REPLACE_SYMLINK''@|0|g' \
| -e 's|@''REPLACE_SYMLINKAT''@|0|g' \
| -e 's|@''REPLACE_TTYNAME_R''@|0|g' \
| -e 's|@''REPLACE_UNLINK''@|0|g' \
| -e 's|@''REPLACE_UNLINKAT''@|0|g' \
| -e 's|@''REPLACE_USLEEP''@|0|g' \
| -e 's|@''REPLACE_WRITE''@|0|g' \
| -e 's|@''UNISTD_H_HAVE_WINSOCK2_H''@|0|g' \
| -e 's|@''UNISTD_H_HAVE_WINSOCK2_H_AND_USE_SOCKETS''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h'; \
| } > unistd.h-t && \
| mv unistd.h-t unistd.h
| rm -f wchar.h-t wchar.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''HAVE_FEATURES_H''@|1|g' \
| -e 's|@''NEXT_WCHAR_H''@|<wchar.h>|g' \
| -e 's|@''HAVE_WCHAR_H''@|1|g' \
| -e 's/@''GNULIB_OVERRIDES_WINT_T''@/0/g' \
| -e 's/@''GNULIB_BTOWC''@/1/g' \
| -e 's/@''GNULIB_WCTOB''@/IN_M4_GNULIB_TESTS/g' \
| -e 's/@''GNULIB_MBSINIT''@/1/g' \
| -e 's/@''GNULIB_MBRTOWC''@/1/g' \
| -e 's/@''GNULIB_MBRLEN''@/0/g' \
| -e 's/@''GNULIB_MBSRTOWCS''@/0/g' \
| -e 's/@''GNULIB_MBSNRTOWCS''@/0/g' \
| -e 's/@''GNULIB_WCRTOMB''@/1/g' \
| -e 's/@''GNULIB_WCSRTOMBS''@/0/g' \
| -e 's/@''GNULIB_WCSNRTOMBS''@/0/g' \
| -e 's/@''GNULIB_WCWIDTH''@/0/g' \
| -e 's/@''GNULIB_WMEMCHR''@/0/g' \
| -e 's/@''GNULIB_WMEMCMP''@/0/g' \
| -e 's/@''GNULIB_WMEMCPY''@/0/g' \
| -e 's/@''GNULIB_WMEMMOVE''@/0/g' \
| -e 's/@''GNULIB_WMEMSET''@/0/g' \
| -e 's/@''GNULIB_WCSLEN''@/0/g' \
| -e 's/@''GNULIB_WCSNLEN''@/0/g' \
| -e 's/@''GNULIB_WCSCPY''@/0/g' \
| -e 's/@''GNULIB_WCPCPY''@/0/g' \
| -e 's/@''GNULIB_WCSNCPY''@/0/g' \
| -e 's/@''GNULIB_WCPNCPY''@/0/g' \
| -e 's/@''GNULIB_WCSCAT''@/0/g' \
| -e 's/@''GNULIB_WCSNCAT''@/0/g' \
| -e 's/@''GNULIB_WCSCMP''@/0/g' \
| -e 's/@''GNULIB_WCSNCMP''@/0/g' \
| -e 's/@''GNULIB_WCSCASECMP''@/0/g' \
| -e 's/@''GNULIB_WCSNCASECMP''@/0/g' \
| -e 's/@''GNULIB_WCSCOLL''@/0/g' \
| -e 's/@''GNULIB_WCSXFRM''@/0/g' \
| -e 's/@''GNULIB_WCSDUP''@/0/g' \
| -e 's/@''GNULIB_WCSCHR''@/0/g' \
| -e 's/@''GNULIB_WCSRCHR''@/0/g' \
| -e 's/@''GNULIB_WCSCSPN''@/0/g' \
| -e 's/@''GNULIB_WCSSPN''@/0/g' \
| -e 's/@''GNULIB_WCSPBRK''@/0/g' \
| -e 's/@''GNULIB_WCSSTR''@/0/g' \
| -e 's/@''GNULIB_WCSTOK''@/0/g' \
| -e 's/@''GNULIB_WCSWIDTH''@/0/g' \
| < ../../m4-1.4.18/lib/wchar.in.h | \
| sed -e 's|@''HAVE_WINT_T''@|1|g' \
| -e 's|@''HAVE_BTOWC''@|1|g' \
| -e 's|@''HAVE_MBSINIT''@|1|g' \
| -e 's|@''HAVE_MBRTOWC''@|1|g' \
| -e 's|@''HAVE_MBRLEN''@|1|g' \
| -e 's|@''HAVE_MBSRTOWCS''@|1|g' \
| -e 's|@''HAVE_MBSNRTOWCS''@|1|g' \
| -e 's|@''HAVE_WCRTOMB''@|1|g' \
| -e 's|@''HAVE_WCSRTOMBS''@|1|g' \
| -e 's|@''HAVE_WCSNRTOMBS''@|1|g' \
| -e 's|@''HAVE_WMEMCHR''@|1|g' \
| -e 's|@''HAVE_WMEMCMP''@|1|g' \
| -e 's|@''HAVE_WMEMCPY''@|1|g' \
| -e 's|@''HAVE_WMEMMOVE''@|1|g' \
| -e 's|@''HAVE_WMEMSET''@|1|g' \
| -e 's|@''HAVE_WCSLEN''@|1|g' \
| -e 's|@''HAVE_WCSNLEN''@|1|g' \
| -e 's|@''HAVE_WCSCPY''@|1|g' \
| -e 's|@''HAVE_WCPCPY''@|1|g' \
| -e 's|@''HAVE_WCSNCPY''@|1|g' \
| -e 's|@''HAVE_WCPNCPY''@|1|g' \
| -e 's|@''HAVE_WCSCAT''@|1|g' \
| -e 's|@''HAVE_WCSNCAT''@|1|g' \
| -e 's|@''HAVE_WCSCMP''@|1|g' \
| -e 's|@''HAVE_WCSNCMP''@|1|g' \
| -e 's|@''HAVE_WCSCASECMP''@|1|g' \
| -e 's|@''HAVE_WCSNCASECMP''@|1|g' \
| -e 's|@''HAVE_WCSCOLL''@|1|g' \
| -e 's|@''HAVE_WCSXFRM''@|1|g' \
| -e 's|@''HAVE_WCSDUP''@|1|g' \
| -e 's|@''HAVE_WCSCHR''@|1|g' \
| -e 's|@''HAVE_WCSRCHR''@|1|g' \
| -e 's|@''HAVE_WCSCSPN''@|1|g' \
| -e 's|@''HAVE_WCSSPN''@|1|g' \
| -e 's|@''HAVE_WCSPBRK''@|1|g' \
| -e 's|@''HAVE_WCSSTR''@|1|g' \
| -e 's|@''HAVE_WCSTOK''@|1|g' \
| -e 's|@''HAVE_WCSWIDTH''@|1|g' \
| -e 's|@''HAVE_DECL_WCTOB''@|1|g' \
| -e 's|@''HAVE_DECL_WCWIDTH''@|1|g' \
| | \
| sed -e 's|@''REPLACE_MBSTATE_T''@|0|g' \
| -e 's|@''REPLACE_BTOWC''@|0|g' \
| -e 's|@''REPLACE_WCTOB''@|0|g' \
| -e 's|@''REPLACE_MBSINIT''@|0|g' \
| -e 's|@''REPLACE_MBRTOWC''@|1|g' \
| -e 's|@''REPLACE_MBRLEN''@|0|g' \
| -e 's|@''REPLACE_MBSRTOWCS''@|0|g' \
| -e 's|@''REPLACE_MBSNRTOWCS''@|0|g' \
| -e 's|@''REPLACE_WCRTOMB''@|0|g' \
| -e 's|@''REPLACE_WCSRTOMBS''@|0|g' \
| -e 's|@''REPLACE_WCSNRTOMBS''@|0|g' \
| -e 's|@''REPLACE_WCWIDTH''@|0|g' \
| -e 's|@''REPLACE_WCSWIDTH''@|0|g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_ARG_NONNULL/r arg-nonnull.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h'; \
| } > wchar.h-t && \
| mv wchar.h-t wchar.h
| rm -f wctype.h-t wctype.h && \
| { echo '/* DO NOT EDIT! GENERATED AUTOMATICALLY! */'; \
| sed -e 's|@''GUARD_PREFIX''@|GL_M4|g' \
| -e 's/@''HAVE_WCTYPE_H''@/1/g' \
| -e 's|@''INCLUDE_NEXT''@|include_next|g' \
| -e 's|@''PRAGMA_SYSTEM_HEADER''@|#pragma GCC system_header|g' \
| -e 's|@''PRAGMA_COLUMNS''@||g' \
| -e 's|@''NEXT_WCTYPE_H''@|<wctype.h>|g' \
| -e 's/@''GNULIB_OVERRIDES_WINT_T''@/0/g' \
| -e 's/@''GNULIB_ISWBLANK''@/0/g' \
| -e 's/@''GNULIB_WCTYPE''@/0/g' \
| -e 's/@''GNULIB_ISWCTYPE''@/0/g' \
| -e 's/@''GNULIB_WCTRANS''@/0/g' \
| -e 's/@''GNULIB_TOWCTRANS''@/0/g' \
| -e 's/@''HAVE_ISWBLANK''@/1/g' \
| -e 's/@''HAVE_ISWCNTRL''@/1/g' \
| -e 's/@''HAVE_WCTYPE_T''@/1/g' \
| -e 's/@''HAVE_WCTRANS_T''@/1/g' \
| -e 's/@''HAVE_WINT_T''@/1/g' \
| -e 's/@''REPLACE_ISWBLANK''@/0/g' \
| -e 's/@''REPLACE_ISWCNTRL''@/0/g' \
| -e 's/@''REPLACE_TOWLOWER''@/0/g' \
| -e '/definitions of _GL_FUNCDECL_RPL/r c++defs.h' \
| -e '/definition of _GL_WARN_ON_USE/r warn-on-use.h' \
| < ../../m4-1.4.18/lib/wctype.in.h; \
| } > wctype.h-t && \
| mv wctype.h-t wctype.h
| make all-am
| make[3]: Entering directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build/lib'
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o gl_avltree_oset.o ../../m4-1.4.18/lib/gl_avltree_oset.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o binary-io.o ../../m4-1.4.18/lib/binary-io.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o c-ctype.o ../../m4-1.4.18/lib/c-ctype.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o c-stack.o ../../m4-1.4.18/lib/c-stack.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o c-strcasecmp.o ../../m4-1.4.18/lib/c-strcasecmp.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o c-strncasecmp.o ../../m4-1.4.18/lib/c-strncasecmp.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o clean-temp.o ../../m4-1.4.18/lib/clean-temp.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o cloexec.o ../../m4-1.4.18/lib/cloexec.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o close-stream.o ../../m4-1.4.18/lib/close-stream.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o closein.o ../../m4-1.4.18/lib/closein.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o closeout.o ../../m4-1.4.18/lib/closeout.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o dirname.o ../../m4-1.4.18/lib/dirname.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o basename.o ../../m4-1.4.18/lib/basename.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o dirname-lgpl.o ../../m4-1.4.18/lib/dirname-lgpl.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o basename-lgpl.o ../../m4-1.4.18/lib/basename-lgpl.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o stripslash.o ../../m4-1.4.18/lib/stripslash.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o execute.o ../../m4-1.4.18/lib/execute.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o exitfail.o ../../m4-1.4.18/lib/exitfail.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o fatal-signal.o ../../m4-1.4.18/lib/fatal-signal.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o fd-hook.o ../../m4-1.4.18/lib/fd-hook.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o fd-safer-flag.o ../../m4-1.4.18/lib/fd-safer-flag.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o dup-safer-flag.o ../../m4-1.4.18/lib/dup-safer-flag.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o filenamecat.o ../../m4-1.4.18/lib/filenamecat.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o filenamecat-lgpl.o ../../m4-1.4.18/lib/filenamecat-lgpl.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o fopen-safer.o ../../m4-1.4.18/lib/fopen-safer.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o freading.o ../../m4-1.4.18/lib/freading.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o getprogname.o ../../m4-1.4.18/lib/getprogname.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o hard-locale.o ../../m4-1.4.18/lib/hard-locale.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o gl_linkedhash_list.o ../../m4-1.4.18/lib/gl_linkedhash_list.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o gl_list.o ../../m4-1.4.18/lib/gl_list.c
| gcc -I. -I../../m4-1.4.18/lib -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -isystem/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/recipe-sysroot-native/usr/include -O2 -pipe -c -o localcharset.o ../../m4-1.4.18/lib/localcharset.c
| Makefile:1915: recipe for target 'close-stream.o' failed
| make[3]: *** [close-stream.o] Segmentation fault (core dumped)
| make[3]: *** Waiting for unfinished jobs....
| make[3]: Leaving directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build/lib'
| Makefile:1674: recipe for target 'all' failed
| make[2]: *** [all] Error 2
| make[2]: Leaving directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build/lib'
| Makefile:1572: recipe for target 'all-recursive' failed
| make[1]: *** [all-recursive] Error 1
| make[1]: Leaving directory '/home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/build'
| Makefile:1528: recipe for target 'all' failed
| make: *** [all] Error 2
| ERROR: oe_runmake failed
| WARNING: /home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/temp/run.do_compile.29555:1 exit 1 from 'exit 1'
| ERROR: Function failed: do_compile (log file is located at /home/valeo-cic/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/m4-native/1.4.18-r0/temp/log.do_compile.29555)
ERROR: Task (/home/valeo-cic/imx-yocto-bsp/sources/poky/meta/recipes-devtools/m4/m4-native_1.4.18.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 100 tasks of which 0 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/valeo-cic/imx-yocto-bsp/sources/poky/meta/recipes-devtools/m4/m4-native_1.4.18.bb:do_compile
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
valeo-cic@bbr:~/imx-yocto-bsp/build-wayland$
Hi,
Seems the problem is with Mouse Laptop.
Built on ASUS Laptop build successfully.
Thank you for the support!
Bhanu,
Is fsl-image-qt5-validation-imx Distro will have AGL image also included in it ? or should we add AGL recipes separately for it in this Distro to build for imx8 ?
AGL component looks illusion with this Distro!
Thanks and Regards
Are you using AGL(Automotive grade Linux) onto I.MX8MQ evk. If you are using AGL then can you please provide the steps which you are performing?
Regards,
Radhika Somaiya.
Hi Radhika,
Is fsl-image-qt5-validation-imx Distro will have AGL image also included in it ? or should we add AGL recipes separately for it. in this Distro to build for imx8.
Thanks and Regards
Mani
HI Radhika Somiya,
The following is the procedure i followed.
Essentials:
$ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \
build-essential chrpath socat cpio python python3 python3-pip python3-pexpect \
xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \
xterm
$ sudo zypper install dblatex xmlto
Git 1.8.3.1 or greater
tar 1.27 or greater
Python 3.4.0 or greater
1.3.1. Downloading a Pre-Built buildtools Tarball
Locate and download the *.sh at http://downloads.yoctoproject.org/releases/yocto/yocto-2.7.1/buildtools/.
Execute the installation script. Here is an example:
$ sh ~/Downloads/x86_64-buildtools-nativesdk-standalone-2.7.1.sh
Execute the installation script. Here is an example:
$ sh ~/Downloads/x86_64-buildtools-nativesdk-standalone-2.7.1.sh
During execution, a prompt appears that allows you to choose the installation directory. For example, you could choose the following:
/home/your-username/buildtools
source /home/your_username/buildtools/environment-setup-x86-64-poky-linux
Essential Yocto Project host packages are:
$ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \
build-essential chrpath socat libsdl1.2-dev
$ mkdir ~/bin
$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repov
$ chmod a+x ~/bin/repo
$ PATH-${PATH}:~/bin
Yocto Project Setup
$ git config --global user.name "Your Name"
$ git config --global user.email "Your Email"
$ git config --list8
$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m
imx-4.14.98-2.0.0_ga.xml
$ repo sync
$ DISTRO=fsl-imx-xwayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-xwayland
$ bitbake fsl-image-qt5-validation-imx
Hey all,
I'm trying to install Linux on my i.mx8 Mini. I'm working on Ubuntu 2019.1 on VM with external SSD.
I follow the yocto guild and always get the native m4 error and then I see your comment on it. Whenever I try to follow the step 2. sudo zypper install dblatex xmlto. I'm getting this error.
Warning: No repositories defined. Operating only with the installed resolvables. Nothing can be installed.
and when I try to follow the step 4 by manually download the x86_64-buildtools-nativesdk-standalone-2.7.1.sh. It give me following error
/usr/bin/env: ‘/home/haider/Downloads/x86_64-buildtools-nativesdk-standalone-2.7.1.sh’: Permission denied
Do you have any comment on that.
Hi Experts,
There seems no fixed concrete steps to build AGL on imx8, kindly share if you do have. While chatting with techsupport team they suggested meta-nxp-agl - i.MX Yocto Project AGL Demo Layer , but this give so many issues when built. Nxp should provide proven steps for AGL build. which is not available i suppose, Please do share if you have one ?
Thanks
Mani
Hi Manivannan,
Could you please provide the information how you resolved the issue which i posted before ?
Thank You
Best Regards
HI Bhanu,
Please do share the AGL steps for imx8, were you able to build It successfully. ?
Regards
Mani
Hi Manivannan,
I am still struggling to build the XWayland image on i.MX 8QuadXPlus MEK.
Not succeeded.
Thank You!
Best Regards,
Bhanu
Bhanu.
I could build it, do a clean all and build again when struck otherwise I have some solutions compilation, look at it if its useful when you face same errors. Sorry if typed little hazy, but you can make it. First are the issues and then are the solutions sequentially, I faced these and could build it with the fix
Issues faced
Fetcher failure for http://www.aleksey.com/xmlsec/download/xmlsec1-1.2.24.tar.gz.tar.gz |
ERROR: Task (/home/user/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux-firmware/linux-firmware_git.bb:do_package_qa) failed with exit code '1' |
ERROR: Task (/home/user/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux-firmware/linux-firmware_git.bb:do_package_qa) failed with exit code '1' |
oe_runmake and Expansion error |
ERROR: Task /sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile) failed with exit code '1' |
ERROR: Task /sources/meta-openembedded/meta-oe/recipes-devtools/protobuf/protobuf_3.4.1.bb:do_fetch) failed with exit code '1' (On Wayland Distro) |
do_fetch, Timeout Errors, do_complie Errors, |
Corresponding solutions below
Goto File /sources/meta-security/recipes-security/xmlsec1/ xmlsec1-1.2.24.bb , Change the SRC_URI path to http://www.aleksey.com/xmlsec/download/old/${BP}.tar.qz |
To exclude perl support in build add the following lines to the linux-firmware_git.bbappend: do_install_prepend () { rm -rf ${S}/murata/.git } |
To include perl support in build add the following lines to the linux-firmware_git.bbappend: RDEPENDS_${PN} = "perl" |
Delete /tmp folder in the build directory close the terminal. start new Terminal and run sources setup-environment to continue with build steps |
After "repo sync", and run the build again. |
Delete SRC_URI = "git://github.com/google/protobuf.git;branch=3.4.x"+ Add SRC_URI = "git://github.com/google/protobuf.git" |
bitbake -c clean/cleanall "TARGET" |
Let me know, if it works !
Regards
Mani
The following is the Log file of Failure Located at /imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/temp/log.do_patch.28249
DEBUG: Searching for fix_path_xtra.patch in paths:
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf-2.69/fsl-imx-xwayland
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf/fsl-imx-xwayland
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/files/fsl-imx-xwayland
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf-2.69/
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf/
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/files/
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf-2.69/x86-64
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf/x86-64
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/files/x86-64
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf-2.69/
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf/
/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/files/
NOTE: Applying patch 'program_prefix.patch' (../sources/poky/meta/recipes-devtools/autoconf/autoconf/program_prefix.patch)
NOTE: Applying patch 'check-automake-cross-warning.patch' (../sources/poky/meta/recipes-devtools/autoconf/autoconf/check-automake-cross-warning.patch)
NOTE: Applying patch 'autoreconf-exclude.patch' (../sources/poky/meta/recipes-devtools/autoconf/autoconf/autoreconf-exclude.patch)
NOTE: Applying patch 'autoreconf-gnuconfigize.patch' (../sources/poky/meta/recipes-devtools/autoconf/autoconf/autoreconf-gnuconfigize.patch)
ERROR: Command Error: 'quilt --quiltrc /home/valeo/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/etc/quiltrc push' exited with 0 Output:
/home/valeo/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin/quilt: line 153: 29018 Segmentation fault (core dumped) bash $BASH_OPTS -c ". $QUILT_DIR/$command" "quilt ${command##*/}" "$@"
DEBUG: Python function patch_do_patch finished
DEBUG: Python function do_patch finished
ERROR: Function failed: patch_do_patch
We are able to build image successfully (Ubuntu version 16.4) for imx8mqevk by following the steps of attached Yocto User's guide version L4.14.98_2.0.0. Can you please try to fresh build?
For ERROR: m4-native-1.4.18-r0 do_compile: oe_runmake failed you can refer the given solutions from this link.
Regards,
Radhika Somaiya.
HI,
I tried the procedure got the following error.
Could you please help to resolve.
Your build environment has been configured with:
MACHINE=imx8qxpmek
SDKMACHINE=i686
DISTRO=fsl-imx-xwayland
EULA=
BSPDIR=
BUILD_DIR=.
meta-freescale directory found
valeo@valeo-MB-K686:~/imx-yocto-bsp/build-xwayland$ bitbake core-image-minimal
NOTE: Your conf/bblayers.conf has been automatically updated.
Parsing recipes: 100% |######################################################################################################################################################################| Time: 0:01:16
Parsing of 2562 .bb files complete (0 cached, 2562 parsed). 3483 targets, 221 skipped, 8 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8qxpmek"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "4.14-sumo"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-poky = "HEAD:c9bd4984f8f471ca2c43052714f4413ba99cf171"
meta-oe
meta-multimedia = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-freescale = "HEAD:27ca94f8a4336790ba117b4298566f6820e7e74c"
meta-freescale-3rdparty = "HEAD:82037216280a39957fb4272581637abec734ad50"
meta-freescale-distro = "HEAD:f7e2216e93aff14ac32728a13637a48df436b7f4"
meta-bsp
meta-sdk = "HEAD:8eeb420fad668b733ab95b460895e1c337c66b25"
meta-browser = "HEAD:75640e14e325479c076b6272b646be7a239c18aa"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-qt5 = "HEAD:d4e7f73d04e8448d326b6f89908701e304e37d65"
Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:01
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: autoconf-native-2.69-r11 do_patch: Command Error: 'quilt --quiltrc /home/valeo/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/etc/quiltrc push' exited with 0 Output:
/home/valeo/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin/quilt: line 153: 29018 Segmentation fault (core dumped) bash $BASH_OPTS -c ". $QUILT_DIR/$command" "quilt ${command##*/}" "$@"
ERROR: autoconf-native-2.69-r11 do_patch: Function failed: patch_do_patch
ERROR: Logfile of failure stored in: /home/valeo/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/temp/log.do_patch.28249
ERROR: Task (virtual:native:/home/valeo/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf_2.69.bb:do_patch) failed with exit code '1'
sumo - imx-4.14.98-2.0.0_ga
I follow the procedure as per the document i.MX_Yocto_Project_User's_Guide
Rev. L4.14.98-2.0.0_ga, 04/2019