ECSPI chip select and boot from SPI-Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ECSPI chip select and boot from SPI-Flash

1,232 次查看
宗標廖
Contributor V

Hello, Community

I came to a problem when I want to boot from SPI-FLash,

Please refer the attachment for details.

Best Regards,

ZongbiaoLiao

标签 (2)
0 项奖励
回复
3 回复数

1,024 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 宗標 廖

V20 gpio1.31 can be used by linux and mfg tools as ENET_MDC signal.

Also gpio1.31 has NVCC_ENET power domain,

while pad U6 - NVCC_GPIO, G21  -NVCC_EIM0.

Probably ADC has incompatible voltage levels used by these i.MX6 pads.

In general one can use a GPIO as chip select for SPI slave.

You can check if ADC is fully powered when i.MX6 begin to boot from SPI and

that ADC should no be powered before i.MX6.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,024 次查看
宗標廖
Contributor V

Hello,Igor

According to the schematics of imx6q-sabreai cpu board, NVCC_ENET,

NVCC_GPIO and NVCC_EIM0 have the same properties,so the power

behavior of U6 and V20 shoud be the same also, is it right?

In case 2(please refer the previous attachment), after I powed on the board,

V20 pin is always on 3.3V voltage,this shoud disable the SPI slave A,so SPI

slave A should have no influence to SPI-FLASH when boot up, is it right?

NVCC.PNG

0 项奖励
回复

1,024 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

I think you should concentrate your attention on "SPI-A" chip,

because it can interfere with i.MX6.

How it is powered ? Is it powered before i.MX6 ?

It should be powered after all i.MX6 power supplies become stable.

Regarding V20 - just for test, suggest to disconnect it from i.MX6 and

connect permanently to 3.3V (inactive) level.

~igor

0 项奖励
回复