Hi every body,
i know that che argument is everywhere is the forum , but i'm not able to do it. I really devasteted. I need to have a dual display, LVDS and HDMI with the same thing displayed.
I have a iMX& with kernel 3.0.35 and ubuntu 11.01
I configure uboot as:
video=mxcfb0:dev=ldb, LDB-VGA,if=RGB666 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24
the first diplay (lvds) works perfectly, but the second (hdmi) don't.
I cheched on /sys/class/graphis and on fb2 i have the hdmi. i cheched name file and modes. If i send a echo 1 > /sys/class/graphics/fb2/blank doesn't do anything on the hdmi display connected. If i do the same on fb0 (lbvds), it immediatelly switch off.
Can someone help me please?
Thanks
Haven't you mixed up the fb1 and fb2 interfaces? HDMI should operate as fb1 device. Please double check.
Have a great day,
Artur
thanks for the reply. I fixed the problem.
Now lvds and hdmi work separately. This means that if i configure to work with lvds, it works. if i configure to work with hdmi, it works too.
Now i would like to use dual mode, lvds + hdmi.
I onfigured uboot as:
video=mxcfb0:dev=ldb,${lvdsres1} video2=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24 ldb=dul0
on lvds is displayed correctly, but hdmi not. I send a echo 0 > /sys/class/graphics/fb2/blank and the display switch on and the pinguins are displayed with right resolution. What is not working is tha the image on lvds is not displayed on hdmi.
if i change ldb=dul1, the fb2 directory in /sys/class/graphics does not be.
Can you help me? I googled but with no success
thanks
Giorgio
hi fantin :
The problem solved?i have the same problem.