Does imx6 android support two camera run at the same time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does imx6 android support two camera run at the same time

2,261件の閲覧回数
lipeng1
Contributor I

dear all

I use the saberd imx6q,i want two camera run at the same time ,now the driver and hardware can support two camera run at same time ,but i don not  know if android can show two camera at the same

ラベル(2)
0 件の賞賛
返信
8 返答(返信)

1,551件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lipeng

please check below

android-imx6-kitkat/0237-ENGR00174526-Add-dual-camera-feature-into-mx6-ICS.patch at master · rabeeh/...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,551件の閲覧回数
lipeng1
Contributor I

dear igorpadykov

thanks for your reply

the patch you give me used for libcamera ,but the sabresd_6dq used the  libcamera2(IMX_CAMERA_HAL_V2),

Do you have patch for libcamera2 ? 

thanks

0 件の賞賛
返信

1,551件の閲覧回数
lipeng1
Contributor I

and the patch you give me only used for two camera swicth,not for  two camera run at the same time 

0 件の賞賛
返信

1,551件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lipeng

you can use usb camera as well.

~igor

0 件の賞賛
返信

1,551件の閲覧回数
lipeng1
Contributor I

do you mean use two usb camera same time?

0 件の賞賛
返信

1,551件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

any configuration is possible

0 件の賞賛
返信

1,551件の閲覧回数
lipeng1
Contributor I

now android4.2.2 can support two camera show sametime ?(imx6 sabresd_6dq

0 件の賞賛
返信

1,551件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信