Display settings to run X on an iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Display settings to run X on an iMX6

1,113件の閲覧回数
kristian_penno
Contributor I

I am running a stock debian armhf system using the kernel(3.10.17) provided from Torodex, our board vendor.

I'm trying to run X using a decent resolution (1280x1024) on the VGA connector.

My kernel line is"video=mxcfb0:dev=vga,1280x1024M@60

Is this correct?

X -configure doesn't find anything to work with.

Do I manually apply some settings for X?

Any help would be much appreciated.

KP

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

905件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please refer to Chapter 18 (X Windows Acceleration) of "i.MX 6 Linux Reference Manual".

Also, "Freescale_XServer_Video_Driver_User¡¯s_Guide.pdf" may be useful.

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_LINUX_DOCS&appType=license&location...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

905件の閲覧回数
kristian_penno
Contributor I

I'm unable to find either of those documents and I have no idea what the file you linked to is for.

Can you please provide links to the docs?

KP

0 件の賞賛
返信

905件の閲覧回数
yurirellosa
Contributor IV

fsl-yocto-3.10.17_1.0.0.gz is a compressed file, uncompress it and find the files inside

Best Regards

Yuri

0 件の賞賛
返信