I tried to start a Yocto project with:
$ mkdir ~/bin
$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
but I got the error:
bash: curl http://commondatastorage.googleapis.com/git-repo-downloads/repo : No such file or directory.
Could you please let me know why? I want to start a project targeting i.MXD Smart Devices Platform. Where can I get the right project for this particular kit?
Thanks,
John
已解决! 转到解答。
Hello John,
There is nothing wrong with your provided link.
I tried it at my side and its work fine here :smileyhappy:
Just keep in your mind that you download into your made "bin"(~/bin) directory not a root's "bin" directory.
I think you have not curl package install on your system, if it's not there then download it first.
find out the output logs for your same question.
mahi@DTP184:~/TESTT$ mkdir TESTT
mahi@DTP184:~/TESTT$ mkdir ~/TESTT/bin
mahi@DTP184:~/TESTT$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/TESTT/bin/repo
% Total % Received % Xferd Average Speed Time Time Time Current
Dload Upload Total Spent Left Speed
100 24081 100 24081 0 0 29877 0 --:--:-- --:--:-- --:--:-- 29914
mahi@DTP184:~/TESTT$ cd bin/
mahi@DTP184:~/TESTT/bin$ ls
repo
mahi@DTP184:~/TESTT/bin$
NOTE : I did all in TESTT directory.
hope this will help you.
Regards
JAYMIN DABHI
Please try the recent Freescale BSP ; instructions how to load and build L3.10.17_1.0.2 release :
http://cache.freescale.com/files/32bit/doc/support_info/IMX6YOCTOPATCHRN.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------