DDR stress test on IMX8QXP custom board and Evaluation board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR stress test on IMX8QXP custom board and Evaluation board

6,312件の閲覧回数
rameshasp
Contributor IV

Hello Team.

Currently we have Si B0 part processor IMX8QXP-CPU EVK board but In EVK we are able to do DDR stress test and we are getting log also. Why we are not able to do DDR stress test in our custom board having Si B0 IMX8QXP processor.

Attached logs from EVK and Custom board. Kindly check and provide the steps further. 

For Production we will use Si C0 revision processor part. Now we have to prove the working of this proto boards with Si B0. Please suggest to proceed further.

0 件の賞賛
返信
7 返答(返信)

6,298件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us your customer board's difference between IMX8QXP-CPU EVK board ? Have customer change DDR?

0 件の賞賛
返信

6,292件の閲覧回数
rameshasp
Contributor IV

In our custom board we are using same like as IMX8QXP_CPU design, Processor PIMX8QX6AVLFZAB is and LPDDR4 is part number is MT53E768M32D4DT-053AIT:E.

0 件の賞賛
返信

6,289件の閲覧回数
rameshasp
Contributor IV

Also i am getting below error after running DDR script.

DCD command finished
DDR frequency = 1200000000
MSI1 AHB Timeout
Error accessing DSC ID = 0x1A, offset = 0x00010000
Error accessing SS = A35

DDRScriptPNG.PNG

0 件の賞賛
返信

6,260件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

How about the DDR frequency = 1600000000? You can try to change the DDR frequency to see if it can work

0 件の賞賛
返信

6,252件の閲覧回数
rameshasp
Contributor IV

There is no option to change DDR frequency to 1600000000, we can change only 800MHZ and 1200MHz.

Please suggest how to change DDR frequency to 1600000000.

0 件の賞賛
返信

6,210件の閲覧回数
rameshasp
Contributor IV

can you please provide some more information:

While doing DDR calibration I am getting in EVK board like below log.

 

*************************************************************************

    MX8 DDR Stress Test Version: ER14

    Built on Mar 27 2020 12:28:23

*************************************************************************

 

--Set up the MMU and enable I and D cache--

  - This is the Cortex-A35 core

 - Check if I cache is enabled 

 - Enabling I cache since it was disabled 

 - Push base address of TTB to TTBR0_EL3 

 - Config TCR_EL3 

 - Config MAIR_EL3 

 - Enable MMU 

 - Data Cache has been enabled 

 - Check system memory register, only for debug 

 

  - VMCR Check:

  - ttbr0_el3: 0x13d000

  - tcr_el3: 0x2051c

  - mair_el3: 0x774400

  - sctlr_el3: 0xc01815

  - id_aa64mmfr0_el1: 0x101122

 

 - MMU and cache setup complete 

 

*************************************************************************

      ARM Clock(CA35): 1200MHz

      DDR Clock: 1860MHz

 

============================================

    DDR configuration

DDR type is LPDDR4

Data width: 32, bank num: 8

Row size: 16, col size: 10

Two chip selects are used 

Number of DDR controllers used on the SoC: 1

Density per chip select:  1536MB 

Density per controller is: 3072MB 

Total density detected on the board is: 3072MB 

 

Command Bus Training was executed 

 

 

********************************************

WARNING! DDR training errors were detected on DDRC 0!

DDR_PHY_PGSR0 = 0x8088c0ff

 Write Leveling Adjustment training error detected 

 VREF training error detected 

Recheck DDR initialization

********************************************

============================================

 

MX8QXP: Cortex-A35 is found

 

*************************************************************************

But in our custom board i am getting below log:

i.MX8QX_B0 is found

Download is complete

If you want to watch DDR script executing proces, please open SCU debug uart in other serial tool

Waiting for the target board boot...

 

can you please why i am not getting log as expected like EVK and what is the UART for Cortex-A35.

0 件の賞賛
返信

6,167件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

The aim of the DDR test tool is to find out the initial parameters of the LPDDR. The images built from the Yocto BSP is used for the EVK by default. So basically, you don't need to do the DDR test because you are using the same LPDDR4 as the EVK. You just need to modify the device tree file base on your board. Then the images build from Yocto should be able to boot on your board.

0 件の賞賛
返信