Booting imx8m mini from Demo image to SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting imx8m mini from Demo image to SD card

1,060 Views
Ruban1
Contributor II

Booting imx8m mini from Demo image to SD card

i have already download android-11.0.0_1.0.0_image_8mmevk

i have gone through all the pdf and tried to flash .

flash is getting successful but wen inserting in imx8m mini evk lpddr4 through minicom only booting is getting completed but while booting kernel it jumps out and reboots many time

So came to provide the commands to be used in Ubuntu 20.04 OS and 32 GB class 10 SD card

  In demo image there exist only 2 executable file

fastboot_imx_flashall.sh

uuu_imx_android_flash.sh

there is no README provided inside Demo image folder

 

0 Kudos
Reply
5 Replies

1,057 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ruban1

 

one can look at Android 11.0.0_1.0.0    Documentation​

in particular ANDROID QUICK START_GUIDE..

 

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Best regards
igor

0 Kudos
Reply

1,051 Views
Ruban1
Contributor II

I have already tried as per the Documents.

All the process build and flashing is Successful.When inserted SD card into IMX8M MINI EVK board .It displays 4 Penguin and get rebooted.

I checked with minicom

It does not move further to display Android or open into Android

 

0 Kudos
Reply

1,046 Views
igorpadykov
NXP Employee
NXP Employee

one can try with other SD cards, preferably brand new ones.

 

Best regards
igor

0 Kudos
Reply

1,039 Views
Ruban1
Contributor II

Sir, Can you kindly suggest which Brand of SD card is preferred Highly for booting Demo image or build image for IMX8M MINI with specification of the SD card along with Size .

Regards

Ruban

0 Kudos
Reply

1,041 Views
Ruban1
Contributor II

The SD card is a Brand new one . Company is ADATA (Premier microSDHC Card UHS-I class 10 32 GB)

Speed up to 100 MB/s

A1 Random R/1500 W/500 IOPS

0 Kudos
Reply