Custom iMX6Solo board flash emmc using sd card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom iMX6Solo board flash emmc using sd card

617件の閲覧回数
rameshasp
Contributor IV

Hi Sir,

i am trying to flash eMMC using sd card but i am able to flash image using sd card after changing boot mode for eMMC not getting console log or eMMC clk. and we are using processor imx6solo MCIMX6S6AVM10AD

below is the boot section of our design:

bootsection.PNG

SD CARD BOOT SELECTION
BOOT_CFG2_7BOOT_CFG2_6BOOT_CFG2_5BOOT_CFG2_4BOOT_CFG1_7BOOT_CFG1_6BOOT_CFG1_5BOOT_CFG1_4

eMMC BOOT SELECTION
BOOT_CFG2_7BOOT_CFG2_6BOOT_CFG2_5BOOT_CFG2_4BOOT_CFG1_7BOOT_CFG1_6BOOT_CFG1_5BOOT_CFG1_4

could you please help me on this.

Thanks & Regards,

Ramesha S P

0 件の賞賛
返信
2 返答(返信)

541件の閲覧回数
art
NXP Employee
NXP Employee

Did you correctly reset the processor after changing boot mode from SD card to eMMC? Did you correctly select the uSDHC port your eMMC chip is connected to (the state of the BT_CFG2_3 signal, that affects the uSDHC port selection, is not shown on your pictures)? Are all other BT_CFGx_y signals pulled down to 0 at the moment of reset?

Also, try not to use the eMMC 4.4 DDR mode during boot, i.e. pull the BT_CFG2_7 signal down to 0.

Best Regards,
Artur

0 件の賞賛
返信

542件の閲覧回数
rameshasp
Contributor IV
SD CARD BOOT SELECTION
BOOT_CFG2_7BOOT_CFG2_6BOOT_CFG2_5BOOT_CFG2_4BOOT_CFG1_7BOOT_CFG1_6BOOT_CFG1_5BOOT_CFG1_4
00000100

eMMC BOOT SELECTION
BOOT_CFG2_7BOOT_CFG2_6BOOT_CFG2_5BOOT_CFG2_4BOOT_CFG1_7BOOT_CFG1_6BOOT_CFG1_5BOOT_CFG1_4
11010110
0 件の賞賛
返信