Hello,
I design my own board with an imx28 CPU. I configured the board (resistors on LCD_D0 to LCD_05) to boot on SSP0 (SD card).
When I try to boot without SD card connected, I have the 0x8020a014 error code on the debug console. So it seems it want to boot on Sd card. So it's good.
But when I connect the SD card, I have absolutely nothing on the debug console.
I measured voltage and everything is good except VDD4P2. It equal to 0.8V !!!!!
This is the schematic :
Can you help me ?
已解决! 转到解答。
In order to close this topic, please find attached my patch for VDD5V Only and the patch for my DDR2 (Samsung K4T51163QQ-BCE7).
Finaly, these patchs are very simple.
To explain what my patches do :
In spl_power_init.c, I set DROPOUT_CTRL (in HW_POWER_DCDC4P2 register) to "DcDc Converter power source is DCDC_4P2 regardless of BATTERY voltage" instead of "DcDc converter selects either VDD4P2 or BATTERY, which ever is higher."
In spl_mem_init.c, I set CS_MAP (in HW_DRAM_CTL29 register) to 1 instead of 16 (?) and I set EIGHT_BANK_MODE (in HW_DRAM_CTL31 register) to "Memory devices have 4 banks" instead of "Memory devices have 8 banks".
In mx28evk.h, I set "define PHYS_SDRAM_1_SIZE" to 0x04000000 (64MB) instead of 0x40000000 (1GB).
Now, everything is fully stable. After 200 loops of 30MB test with memtester I have 0 error. All the supply from the IMX a solid and with a correct voltage.
Many thanks for all your help during these 3 months. This is the culmination :).
In order to close this topic, please find attached my patch for VDD5V Only and the patch for my DDR2 (Samsung K4T51163QQ-BCE7).
Finaly, these patchs are very simple.
To explain what my patches do :
In spl_power_init.c, I set DROPOUT_CTRL (in HW_POWER_DCDC4P2 register) to "DcDc Converter power source is DCDC_4P2 regardless of BATTERY voltage" instead of "DcDc converter selects either VDD4P2 or BATTERY, which ever is higher."
In spl_mem_init.c, I set CS_MAP (in HW_DRAM_CTL29 register) to 1 instead of 16 (?) and I set EIGHT_BANK_MODE (in HW_DRAM_CTL31 register) to "Memory devices have 4 banks" instead of "Memory devices have 8 banks".
In mx28evk.h, I set "define PHYS_SDRAM_1_SIZE" to 0x04000000 (64MB) instead of 0x40000000 (1GB).
Now, everything is fully stable. After 200 loops of 30MB test with memtester I have 0 error. All the supply from the IMX a solid and with a correct voltage.
Many thanks for all your help during these 3 months. This is the culmination :).
Hi Damien,
I'm going to keep my U-Boot patch mostly as-is for a few reasons:
- The patch disables battery voltage measurement when there is no battery
- The patch disables all code paths relating to booting from battery
- The power block configuration is based primarily on the Fressscale bootlets which I think should be retained unless we can come up with some pretty clear and convincing arguments as to why an alternative approach is better
I think there is scope for some refactoring of the power block setup code in U-Boot, but for now I think it best to leave it as close to the bootlet code sequence as practical
Just would like to mention that Graeme/Damien's patch for 5V only operation has been applied:
Regards,
Fabio Estevam
Hi Damien,
That's great news :-) Glad to know your board is stable now.
Just to make sure I understood:
1. You only need to apply VDD5V_Only_Uboot.patch.zip in spl_power_init.c. The previous VDD5V_Only_Uboot_2014.patch.zip that you posted on January, 6th is no longer needed. Is that correct?
2. About the second patch: you could let DDR settings inside spl_mem_init.c untouched and then rewrite CTL29 and CTL31 using mxs_adjust_memory_params(). Please check board/bluegiga/apx4devkit/spl_boot.c as a reference.
Regards,
Fabio Estevam
Hi Fabio,
1 . About the patch posted on January, 6th, you can simply delete it, and empty your recycle bin :smileyhappy:. It generate DDR errors (I searched a long time in spl_mem_init to find why my DDR was not stable, but it was not a DDR configuration mistake, but a power mistake caused by my patch).
2. Perfect, many thanks for this advice.
Hello,
I've finally managed to start U-Boot 2015.01-rc2 on my own board with VDD5V only.
I will now fix every little mistake then clean my code and post my patch.
But I still have two little problems.
1. U-Boot detects only 64Mib instead of 512Mib. This is my "include/configs/mx28_evk.h" file :
#define CONFIG_NR_DRAM_BANKS 4 /* 4 bank of DRAM */
#define PHYS_SDRAM_1 0x40000000 /* Base address */
#define PHYS_SDRAM_1_SIZE 0x20000000 /* 512 MB */
2. duart_tx don't work. When I have the message "Hit any key to stop autoboot:", I can press any key, U-boot launch autoboot.
I tried with a non-modified U-boot 2015.01-rc2 on mx28evk and the problem is also there. So I think is a problem on the U-boot code and not a problem due to my changes.
Was this problem already reported ?
Many thanks
Hi Damien,
Good progress.
Let's try to fix the duart issue first: I have just tested top of tree U-boot on my mx28evk and duart works fine here (U-Boot 2015.01-rc3-00069-gfc9b0b8).
Make sure your terminal has flow control disabled.
Thanks for your answer.
It's a bug on the U-Boot 2015.01-rc2.
With U-Boot 2015.01-rc3 it works :smileyhappy: !
There were no modification on SPL_POWER_INIT.c and SPL_MEM_INIT.c between rc2 and rc3 so all my modifications are still good.
This I my debug output :
HTLLC
Configured for 5v only power source.
Valid 5V detected
sz =08000000
LLC
U-Boot 2015.01-rc3 (Dec 12 2014 - 15:26:45)
CPU: Freescale i.MX28 rev1.2 at 454 MHz
BOOT: SSP SD/MMC #0, 3V3
SPI: ready
DRAM: 128 MiB
NAND: 0 MiB
MMC: MXS MMC: 0
MMC0: Command 8 timeout (status 0xe0284020)
MMC0: Command 55 timeout (status 0xe0384020)
MMC0: Command 1 timeout (status 0xe02c4020)
Card did not respond to voltage select!
MMC init failed
Using default environment
Video: MXSFB: 'videomode' variable not set!
In: serial
Out: serial
Err: serial
Net: FEC0 [PRIME], FEC1
Warning: FEC1 using MAC address from net device
Hit any key to stop autoboot: 0
=>
Now, the boot fails during mxs_mem_get_size() function. Especially on this line : sz = get_ram_size((long *)PHYS_SDRAM_1, PHYS_SDRAM_1_SIZE);
If I force sz to be 512Mib (so replace the previous line by sz=0x20000000), U-boot stops here :
HTLLC
Configured for 5v only power source.
Valid 5V detected
sz = 20000000
LLC
U-Boot 2015.01-rc3 (Dec 12 2014 - 15:36:08)
CPU: Freescale i.MX28 rev1.2 at 454 MHz
BOOT: SSP SD/MMC #0, 3V3
SPI: ready
DRAM:
But if I force sz to be 128Mib (so sz=0x08000000), It works but with only 128Mib (see debug output above)
EDIT :
The following lines are normal because I launch U-boot with mxsldr, so I don't have any sd card on my board :
MMC0: Command 8 timeout (status 0xe0284020)
MMC0: Command 55 timeout (status 0xe0384020)
MMC0: Command 1 timeout (status 0xe02c4020)
Card did not respond to voltage select!
MMC init failed
Hi Damien,
The sz = get_ram_size((long *)PHYS_SDRAM_1, PHYS_SDRAM_1_SIZE); assumes that there is only one bank of RAM.
I suppose you use EMI_CE0 and EMI_CE1 for the DDR chip selects on your board, right? Then you should use CONFIG_NR_DRAM_BANKS 2.
You should also change the size calculation as follows:
sz1 = get_ram_size((long *)PHYS_SDRAM_1, PHYS_SDRAM_1_SIZE);
sz2 = get_ram_size((long *)PHYS_SDRAM_2, PHYS_SDRAM_2_SIZE);
sz = sz1 + sz2;
and then in your board config file you need to pass PHYS_SDRAM_2 and PHYS_SDRAM_2_SIZE definitions.
Also, you would need to adjust CS_MAP field to 3 in the HW_DRAM_CTL29 register to make use of the 2 Chip Selects.
In board/freescale/mx28evk/iomux.c we have:
#define CS_MAP 0xf as we use a single chip select.
you should change it to 3 for your board.
Damien,
Maybe the two changes below should be enough:
1. Change CS_MAP to 3
2. In the board config file use:
/* Memory configuration */
#define CONFIG_NR_DRAM_BANKS 1 /* 1 bank of DRAM */
#define PHYS_SDRAM_1 0x40000000 /* Base address */
#define PHYS_SDRAM_1_SIZE 0x40000000 /* Max 1 GB RAM */
#define CONFIG_SYS_SDRAM_BASE PHYS_SDRAM_1
I think this would allow U-boot to detect the correct memory size.
If that does not work, then we should consider changing sz calculation as mentioned in my previous post.
Thanks for your help.
I use a Samsung K4T51163QQ-BCE7.
This is the addressing configuration :
Configuration : 32Mb x16
# of Bank : 4
Bank Address : BA0,BA1
Auto precharge : A10/AP
Row Address : A0 ~ A12
Column Address : A0 ~ A9
I only use 1 chip select, EMI_CE0 (my DDR has only one pin CS). But the Bank is selected with EMI_BA0 and EMI_BA1.
So, I suppose I don't need to change anything to CS_MAP, isn't it ?
Many thanks
Hi Damien,
The DDR you use is 512Mbits, which correspond to 64MBytes and you should use
CONFIG_NR_DRAM_BANKS | 1 |
as only one chip select is used.
Yes, you don't need to change CS_MAP.
Regards,
Fabio Estevam
Is the problem can only come from the DDR initialisation in the spl_mem_init ?
Because I retry a lot of time, I followed the excel tools scrupulously to set all the HW_DRAM_CTL register but I still have this error.
Many thanks
Are you able to boot the kernel on your board if you use bootlets instead? Does it boot without issues in this case?
I am not sure if the problem is bad DDR init or U-boot porting? Are the power supplies stable?
Maybe I found something.
The DDR2 our supplier provided us were not the DDR2-800 but DDR2-667 version ! So this DDR can not run at 200MHz. Do you know how to speed down the DDR clock to 166 MHz ?
Thanks
Ok, I have set 166 MHz in the excel tool and in spl_mem_init i set divider (for HW_CLKCTRL_FRA0_EMI) to 26 (for 166 MHz).
But it still don't work.
I look at the scoope and the power supply is really solid. 1V8 is 1.81V and 4V2 is 4.24V.
On the imx28evk, everything works fine
Hi Damien,
I made some changes to the patches you made for the memory and now I'm able to start Linux on your custom board :-)
Image is build using Yocto Dizzy. Only quick test I did now are a couple of reboots to check if the board starts up into Linux.
I will included a memory tester program in the image so we are able to do a complete test of the memory range and test stability of this memory configuration.
I will mail you the different patches and memory configurator file.