Hello,
I have implemented SWUpdate and I can successfully upgrade my kernel and OS. Now I am trying to create two new U-Boot environment variables.
CONFIG_KERNEL_TO_RUN and CONFIG_SWUPDATE_BOOTCMD. The idea is CONFIG_KERNEL_TO_RUN can have the values 0 or 1. If the value is 1 run the SWUpdate kernel to receive a new update, or run the default image kernel.
To add these new variables I am attempting to patch the mx6ul_14x14_evk.h file in build-fb/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/u-boot-imx/2021.04-r0. My patch is properly applied but when I run my device and enter the bootloader, running printenv my new setting is not present.
Note I have only attempted to add CONFIG_SWUPDATE_BOOTCMD at this point. Here is my patch file.
--- a/include/configs/mx6ul_14x14_evk.h 2023-02-23 15:43:58.407930365 -0600
+++ b/include/configs/mx6ul_14x14_evk.h 2023-02-23 15:41:52.594126013 -0600
@@ -120,6 +120,7 @@
"boot_fdt=try\0" \
"ip_dyn=yes\0" \
"splashimage=0x8c000000\0" \
+ "swupdate_bootcmd="__stringify(CONFIG_SWUPDATE_BOOTCMD)"\0" \
"mmcdev="__stringify(CONFIG_SYS_MMC_ENV_DEV)"\0" \
"mmcpart=" __stringify(CONFIG_SYS_MMC_IMG_LOAD_PART) "\0" \
"mmcroot=" CONFIG_MMCROOT " rootwait rw\0" \
@@ -218,6 +219,17 @@
"fi; " \
"fi; " \
"else run netboot; fi"
+
+#define CONFIG_SWUPDATE_BOOTCMD \
+ "setenv bootargs console=ttymxc0,115200 root=/dev/ram0 rootfstype=ext4 rw ;" \
+ "load mmc 1:3 0x83000000 /swupdate-image-imx6ull14x14evk.ext4.gz.u-boot;" \
+ "load mmc 1 0x82a00000 imx6ull-14x14-evk.dtb;" \
+ "load mmc 1 0x80800000 zImage;" \
+ "load mmc 1 0x83000000 300000 100000;" \
+ "setenv root /dev/ram0;" \
+ "setenv rootfstype ext4;" \
+ "setenv fw_env_config /etc/fw_env.config;" \
+ "bootz 0x80800000 0x83000000 0x82a00000;"
#endif
/* Miscellaneous configurable options */
Is there something I am missing? I figured if I told uboot about this new setting it would just appear.
已解决! 转到解答。
Dumb mistake I was patching the wrong header file. I was patching mx6ul_14x14_evk.h but needed to patch mx6ullevk.h.
I found this by looking into the file tmp/work/imx6ull14x14evk-poky-linux-gnueabi/u-boot-imx/2021.04-r0/build/mx6ull_14x14_evk_emmc_config/include/config.h which contains
/* Automatically generated - do not edit */
#define CONFIG_IMX_CONFIG board/freescale/mx6ullevk/imximage.cfg
#define CONFIG_BOARDDIR board/freescale/mx6ullevk
#include <config_uncmd_spl.h>
#include <configs/mx6ullevk.h>
#include <asm/config.h>
#include <linux/kconfig.h>
#include <config_fallbacks.h>
To test SWUpdate I was manually running the commands
setenv swupdate_bootcmd "setenv bootargs console=ttymxc0,115200 root=/dev/ram0 rootfstype=ext4 rw ; load mmc 1:3 0x83000000 /swupdate-image-imx6ull14x14evk.ext4.gz.u-boot;load mmc 1 0x82a00000 imx6ull-14x14-evk.dtb;load mmc 1 0x80800000 zImage;load mmc 1 0x83000000 300000 100000;setenv root /dev/ram0;setenv rootfstype ext4;setenv fw_env_config /etc/fw_env.config;bootz 0x80800000 0x83000000 0x82a00000"
savenev
run swupdate_bootcmd
I am now trying to automate this process.
Dumb mistake I was patching the wrong header file. I was patching mx6ul_14x14_evk.h but needed to patch mx6ullevk.h.
I found this by looking into the file tmp/work/imx6ull14x14evk-poky-linux-gnueabi/u-boot-imx/2021.04-r0/build/mx6ull_14x14_evk_emmc_config/include/config.h which contains
/* Automatically generated - do not edit */
#define CONFIG_IMX_CONFIG board/freescale/mx6ullevk/imximage.cfg
#define CONFIG_BOARDDIR board/freescale/mx6ullevk
#include <config_uncmd_spl.h>
#include <configs/mx6ullevk.h>
#include <asm/config.h>
#include <linux/kconfig.h>
#include <config_fallbacks.h>