Chromium on IMX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,981件の閲覧回数
Giacomo_
Contributor II

Hello community,
I am trying to compile the chromium-ozone-wayland based on Yocto hardknott (imx-5.10.35-2.0.0.xml) on IMX8MQEVK board, but the compilation fails with the error:

| Package dri was not found in the pkg-config search path.
| Perhaps you should add the directory containing `dri.pc'
| to the PKG_CONFIG_PATH environment variable
| No package 'dri' found
|
| See //content/gpu/BUILD.gn:141:18: which caused the file to be included.
| configs += [ "//build/config/linux/dri" ]
| ^-------------------------
| WARNING: exit code 1 from a shell command.

In my previous version (Yocto Warrior) I was able to fix it by adding this dependency:

DEPENDS += " mesa "

but this trick no longer works, has anyone successfully compiled chromium?
I know... There is no support for Chromium, I am just asking.

 

 

ラベル(2)
タグ(1)
0 件の賞賛
1 解決策
5,942件の閲覧回数
Jeroen_H
Contributor III

Just to let you know, I'm trying to buildby using this patch right now:

https://github.com/OSSystems/meta-browser/issues/528

Seach for "0013-Only-DRI-for-x11.txt" and adapt to your code version.

But, it takes a while to build Chromium, I'll post my finding later.

Hopefully DRI isn't needed on iMX8 and Wayland.

Cheers,

Jeroen.

元の投稿で解決策を見る

11 返答(返信)
5,934件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport
0 件の賞賛
5,905件の閲覧回数
Jeroen_H
Contributor III

Hi!

Thanks for pointing us out to the document. I've already gone through these steps.

Unfortunately, adding mesa to the depends, and building seperately still produced errors during do_configure().

Kind regards,

Jeroen.

0 件の賞賛
5,923件の閲覧回数
Giacomo_
Contributor II

Backporting? Yes, I can evaluate this too, thanks.

0 件の賞賛
5,962件の閲覧回数
Giacomo_
Contributor II

here you are my bbappend:

chromium-ozone-wayland_83.0.4103.116.bbappend

it contains only one line:

DEPENDS += " mesa "

0 件の賞賛
5,954件の閲覧回数
Jeroen_H
Contributor III

Okay, thanks, I'll have a look

0 件の賞賛
5,943件の閲覧回数
Jeroen_H
Contributor III

Just to let you know, I'm trying to buildby using this patch right now:

https://github.com/OSSystems/meta-browser/issues/528

Seach for "0013-Only-DRI-for-x11.txt" and adapt to your code version.

But, it takes a while to build Chromium, I'll post my finding later.

Hopefully DRI isn't needed on iMX8 and Wayland.

Cheers,

Jeroen.

5,924件の閲覧回数
Giacomo_
Contributor II

Yes please, let me know the outcome.

0 件の賞賛
5,906件の閲覧回数
Jeroen_H
Contributor III

Hi,

Building succeeded, I have chromium (83.0.4103.116) running now on iMX8M Mini, weston-wayland, and using the GPU of the iMX.

I'm using Zeus btw.

Performance looks good.

Still doing some testing, but I think you can take it from here

Jeroen.

0 件の賞賛
5,377件の閲覧回数
r_trivedi123
Contributor IV

Hi Jeroen,
Can you share,

Which BSP you used ?
How did you build (for wayland running on GPU ) ? , basically build step doc or pointers.
Any performance statistics or issues you found ?

Appreciate your guidance.

--
Thanks
Rutvij

0 件の賞賛
5,870件の閲覧回数
Giacomo_
Contributor II

Kudos to Jeroen (not the button only).

This is the way to go.

Thank you for helping!

0 件の賞賛
5,967件の閲覧回数
Jeroen_H
Contributor III

Hi,

I have the same issue (iMX8M Mini, using Zeus 5.4.47) , no solution found yet.
Can you tell me the exact version of Yocto Warrior (or actually the version of Chromium) you've been using previously?

Just wanted to have a look at the differences....

0 件の賞賛