The "i.MX Linux User's Guide" is referenced in several documents including the "Freescale Yocto Project User's Guide". However, I am unable to locate this document anywhere. Can someone direct me to the document?
Here's the reference pulled from the Freescale Yocto Project User's Guide.
Appendix B References
For details on boot switches, see Section "How to Boot the i.MX Boards" in the
i.MX Linux User's Guide
For how to download images using U-boot, see Section "Downloading Images Using U-Boot" in the
i.MX Linux User's Guide
For how to set up an SD/MMC card, see Section "Preparing an SD/MMC Card to Boot" in the
i.MX Linux User's Guide
Hi Brust
Linux User Guide is included in Doc Bundle for each BSP (also please find it attached)
Board Support Packages (27)
L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------