Can't get glTexDirectMapVIV to work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't get glTexDirectMapVIV to work

1,767 次查看
mod42
Contributor III

I try to get video from a CSI-2 interface of a custom iMX8QXP board to be displayed using OpenGLES (will need some transformations on the video image). For performance reasons we would like to use glTexDirectMapVIV to directly use the buffers from v4l2 as an OpenGLES texture. But unfortunatly I am not able to get this to work. I stripped our test program as much as possible so no v4l2 involved. Just egl/gles:

 

#include <stdbool.h>
#include <stdlib.h>
#include <unistd.h>

#include <GLES/gl.h>
#include <GLES/glext.h>

#include <vdk.h>

int main(int argc, char *argv[])
{
    int xRes = 1920;
    int yRes = 720;
    int optNumFrames = 600;
    bool optVivMap = false;

    int c;
    while(-1 != (c = getopt(argc, argv, "n:m")))
    {
        if('n' == c)
        {
            optNumFrames = strtoul(optarg, 0, 0);
        }
        else if('m' == c)
        {
            optVivMap = true;
        }
    }

    vdkEGL egl = {};

    EGLint configAttribs[] =
    {
        EGL_SAMPLES,      0,
        EGL_RED_SIZE,     8,
        EGL_GREEN_SIZE,   8,
        EGL_BLUE_SIZE,    8,
        EGL_ALPHA_SIZE,   EGL_DONT_CARE,
        EGL_DEPTH_SIZE,   16,
        EGL_SURFACE_TYPE, EGL_WINDOW_BIT,
        EGL_NONE,
    };

    EGLint attribListContext[] =
    {
        // Needs to be set for es2.0 as default client version is es1.1.
        EGL_CONTEXT_CLIENT_VERSION, 1,
        EGL_NONE
    };

    vdkInitialize();
    vdkSetupEGL(0, 0, xRes, yRes, configAttribs, NULL, attribListContext, &egl);
    vdkShowWindow(egl.window);

    glClearColor(0.2f, 0.0f, 0.0f, 0.0f);
    glViewport(0, 0, xRes, yRes);
    glMatrixMode(GL_PROJECTION);
    glOrthof(-10.0f, 10.0f, -10.0f , 10.0f, -1.0f, 1.0f);

    glEnable(GL_TEXTURE_2D);

    unsigned int texture;
    glGenTextures(1, &texture);

    glBindTexture(GL_TEXTURE_2D, texture);
    glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_WRAP_S, GL_CLAMP_TO_EDGE);
    glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_WRAP_T, GL_CLAMP_TO_EDGE);
    glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_MIN_FILTER, GL_LINEAR);
    glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_MAG_FILTER, GL_LINEAR);

    //Alloc texture data and write some data into it
    int texXRes = 64;
    int texYRes = 64;
    void * videoData = malloc(texXRes*texYRes*4);

    //Get some data to the texture
    uint8_t * p0 = (uint8_t *)videoData + 0 * texXRes * texYRes;
    uint8_t * p1 = (uint8_t *)videoData + 1 * texXRes * texYRes;
    uint8_t * p2 = (uint8_t *)videoData + 2 * texXRes * texYRes;
    uint8_t * p3 = (uint8_t *)videoData + 3 * texXRes * texYRes;
    for(size_t k = 0; k < texXRes * texYRes; k += 4)
    {
        *p0++ = rand();  *p0++ = rand(); *p0++ = rand(); *p0++ = rand();
        *p1++ = 0xFF;    *p1++ = 0x00;   *p1++ = 0x00;   *p1++ = 0x00;
        *p2++ = 0x00;    *p2++ = 0xFF;   *p2++ = 0x00;   *p2++ = 0x00;
        *p3++ = 0x00;    *p3++ = 0x00;   *p3++ = 0xFF;   *p3++ = 0x00;
    }

    if(optVivMap)
    {
        PFNGLTEXDIRECTMAPVIVPROC glTexDirectMapVIV = (PFNGLTEXDIRECTMAPVIVPROC)eglGetProcAddress("glTexDirectMapVIV");
        PFNGLTEXDIRECTINVALIDATEVIVPROC glTexDirectInvalidateVIV = (PFNGLTEXDIRECTINVALIDATEVIVPROC)eglGetProcAddress("glTexDirectInvalidateVIV");

        GLuint pAddr = ~0U;
        glTexDirectMapVIV(GL_TEXTURE_2D, texXRes, texYRes, GL_BGRA_EXT, &videoData, &pAddr);
        glTexDirectInvalidateVIV(GL_TEXTURE_2D);
    }
    else
    {
        glTexImage2D(GL_TEXTURE_2D, 0, GL_BGRA_EXT, texXRes, texYRes, 0, GL_BGRA_EXT, GL_UNSIGNED_BYTE, videoData);
    }

    glMatrixMode(GL_MODELVIEW);
    glLoadIdentity();

    glEnableClientState(GL_VERTEX_ARRAY);
    glEnableClientState(GL_TEXTURE_COORD_ARRAY);

    for(int i = 0; i < optNumFrames; i++)
    {
        glClear(GL_COLOR_BUFFER_BIT);

        float vertices[] = {
                -8.0f,  -8.0f, 0.0f,    //lower left
                    8.0f,  -8.0f, 0.0f,    //lower right
                -8.0f,   8.0f, 0.0f,    //upper left
                    8.0f,   8.0f, 0.0f,    //upper right

        };
        float texCoords[] = {
            0.0f,   1.0f,    //lower left
            1.0f,   1.0f,    //lower right
            0.0f,   0.0f,    //upper left
            1.0f,   0.0f,    //upper right
        };
        glVertexPointer(3, GL_FLOAT, 0, vertices);
        glTexCoordPointer(2, GL_FLOAT, 0, texCoords);

        uint8_t indices[] = { 0, 1, 2, 1, 3, 2 };
        glDrawElements(GL_TRIANGLES, 6, GL_UNSIGNED_BYTE, indices);

        glFinish();
        eglSwapBuffers(egl.eglDisplay, egl.eglSurface);
    }

    return EXIT_SUCCESS;
}

 

 If started without option -m (optVivMap == false) I can see the prepared texture. When the application is started with option -m I only see a white rectangle instead of the expected texture. Everything is based on rel_imx_5.4.70_2.3.0. 

I would be thankful for any hint.

0 项奖励
回复
7 回复数

1,762 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello mod42,

From quickly test, L4.14.98 BSP has no this issue, but L5.4.70 BSP has it. 

Some difference for the two kernel:

L5.4.70's GPU driver will create a DRM device "/dev/dri/card0" and DPU display driver will be "/dev/dri/card1".

But in L4.14.98 kernel, there is only one drm device "/dev/dri/card0" for DPU display. 

I had tried to change "/etc/xdg/weston/weston.ini", set "drm-device=card1". But the issue is still there.

 

Regards

 

0 项奖励
回复

1,745 次查看
mod42
Contributor III

So, your suggestion is to downgrade to L4.14.98 and stay there or will this be fixed in a future revision?

0 项奖励
回复

1,741 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

This will be fixed for next revision.

 

0 项奖励
回复

1,264 次查看
mod42
Contributor III

This is still not fixed in 5.15.52 with Vivante binaries imx-gpu-viv-6.4.3.p4.4-aarch64.bin. Any updates on this?

0 项奖励
回复

1,707 次查看
mod42
Contributor III

Is this supposed to be fixed in the 5.10.35_2.0.0 release? I rebuild all our stuff based on this revision and can't get it to work. The behavior is the same as in the 5.4.70 release.

0 项奖励
回复

1,514 次查看
marcus-castlepeakinc
Contributor III

I've built this on my imx8mp with 5.10.72-2.2.0  and the white texture with glTexDirectMapVIV still  occurs.  When is this going to be fixed?

0 项奖励
回复

1,519 次查看
marcus-castlepeakinc
Contributor III

Hello.

I tried to build your posted example and can't find vdk.h anywhere in /usr/include.  I'm using 5.10.72-2.2.0 BSP image.  Anyone have ideas?

0 项奖励
回复