Hi
I purchased i.MX8M mini EVK
The EVK I purchased has 2GB of LPDDR4 designed.
(There are also EVKs designed with DDR4)
Can I change to DDR3?
Can I design with 512MB or 1GB?
The product I am designing now does not have much work on the video side.
It is about checking the video seamlessly by connecting HD-class CAM with USB.
Please review
Thank you
Hi Danny,
Please refer to IMX8MMHDG: i.MX 8M Mini Hardware Developer’s Guide for DDR3L.
Regards,
Mrudang
Hi Mrudang
I will refer to IMX8MMHDG: i.MX 8M Mini Hardware Developer’s Guide
But I have a question
Where is the circuit diagram for reference (SCH-35104, SCH-31399)?
This is not in IMX8MMHDG: i.MX 8M Mini Hardware Developer’s Guide, what document?
Is the document I know different from the document you are telling me?
Please let me know
Thank you
Hi Danny,
The schematic is based on DDR4 and LPDDR4. but they have also mentioned DDR3 as well. It means this reference schematic is also applicable for DDR3 signal interface as well.
Section 3.4 of IMX8MMHDG: i.MX 8M Mini Hardware Developer’s Guide has provided pin signal assignment for all 3 DRAM.
Mrudang
Hi Mrudang
I referred to the document composed of DDR4 (SPF-35104) and prepared a circuit diagram for review. (The circuit diagram was attached)
Have you seen the circuit diagram I attached?
If you have seen it, please give me a comment on it
According to the document (IMX8MMHDG: i.MX 8M Mini Hardware Developer's Guide), when using DDR3L, it seems to use four DDR3L.
However, the circuit diagram using DDR4 uses two DDR4.
If there is a circuit diagram composed of DDR3L, please attach it.
Thanks
Hi Danny,
Please resend me the updated schematic.
If they have used 4 DRAM for their application. If we need to use 2 DRAM based on data lines and memory density we need to connect the DQ signals and address signals.
Mrudang.
Hi Mrudang
Among the above ripples, there is a circuit diagram I attached
I want you to give me a comment on it
1. Only two DDR3Ls are used? Should I use 4?
2. Please inform the wrong part of the attached circuit diagram.
3. Please attach a reference circuit diagram written in DDR3L.
4. Is there a circuit diagram written in i.MX8MM and DDR3L?
Thank you
HI Danny,
Now DRAM looks good. I believe Parity, Ten and ACT_n pins are not there in DDR3L. Those are for DDR4.
Is there anything else that could be a big problem besides the data line?
Ans: Data Mask, Data strobe has to be matched with Data lines. Earlier schematic it was not matching.
I think the wiring of DDR4 and DDR3L is similar, so I can do artwork by referring to the DDR4 schematic and PCB file.
Ans: Yes.
Mrudang