Hi ,
I want to do can communication on two imx6 ( MCIMX6DLAICPU2 ) boards which has can interfaces along with baseboard ( MCIMXABASEV1 ). The driver is already enabled , so I would like to know the procedure further.
If possible can you provide some sample application for experimenting purpose.
Thanks and Regards,
Abhirup Mitra
Hi Artur ,
Thanks for your response !
As you mentioned above , I reffered the reference manual and tried :
$ip link set can0 up type can bitrate 125000
I was able to see logs by dmesg command and the interface was ready. But when I tried with cansend and candump command I was unable to get the can frames.
Also I noticed as I typed the following in command prompt:
$ip -details -statistics link show can0
It showed the can state as BUS OFF which was previously ERROR-ACTIVE.
I tried to restart the interface and again send cansend message but still it persist to give same output.
I used this cansend command:
$ cansend 123#112233445566
I also tried connecting two IMX boards , CAN_HI to CAN_HI and CAN_LOW to CAN_LOW taking reference from schematics and tried communicating with cansend and candump on the boards respectively , but still I was unable to see any can communication.
Please let me know how can I solve the problem?
Thanks and Regards,
Abhirup Mitra
Hi Abhirup Mithra,
I am also trying for getting CAN protocol up on the same boards (MCIMX6DLAICPU2 & MCIMXABASEV1). And I have also gone through i.MX_Linux_Reference_Manual.pdf regarding the configuration settings while doing menuconfig.
Unfortunately, I am not succeeding on this.
Following image show the details of the debug messages:
For the command:
1) ifconfig -a
2) ip link set can0 up type can bitrate 125000
As you can see, for ifconfig -a, the HWaddr detail for CAN0 are value 0.
Queries:
1) Is it possible for you to share with me the binaries generated in your system? (the .sdcard image)
2) What could be reason that HWaddr detail for me is 0?
3) What results you are getting for ifconfig -a command?
Thanks in advance!
Best Regards,
Indrajit
Please follow the Chapter 37 of the attached document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------