Can I do not supply power for PCIE-HDMI-SATA-USB if not use them?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I do not supply power for PCIE-HDMI-SATA-USB if not use them?

828 Views
翔李
Contributor IV

HI,

If I don't use PCIE,SATA,HDMI,USB OF IMX6Q-IMX6 DUAL-SOLO etc,is it necessary to supply the power of their VCC-IN PIN? Can I NC these following PINS?
SATA_VP_VPH,,,HDMI_VP_VPH,,,PCIE_VP_VPH_VPTX,,,USB_VBUS.

What is more,If I don't use USB,Can I do not stuff 24MHZ CRYSTAL?

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

0 Kudos
Reply
2 Replies

697 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,

  For PCIE,SATA & HDMI, if you don't use them, not necessary to supply them, so you can make corresponding resistors NC.

  But for USB, power is required, because USB OTG port will be used to download images into Flash/SD/eMMC on board.

   In addition, 24MHz crystal is working clock for CPU, so it must be used.

Best regards,

Weidong

0 Kudos
Reply

697 Views
翔李
Contributor IV

THANKS.

I find a description about PCIE on AN4397  SATA VP VPH to be ground if not in use,so si it to be ground or NC? what about PCIE-HDMI?pastedImage_1.png

0 Kudos
Reply