Booting with SD card and eMMC at i.MX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting with SD card and eMMC at i.MX6Q

1,815 次查看
yklee1
Contributor II

Dear Team,

I have a questions about booting sequence of i.MX6Q.

Can I let i.MX6Q boot up with the image of SD card even if it has eMMC also having a bootable image sets?

What I mean, usually system(i.MX6Q) will boot up with the images inside eMMC.

But by some reason if I plug in SD card having proper bootable images, i.MX6Q should boot up with this images inside the plugged SD card.

Could you please let me know it is possible or not?

If yes, could you please give some hit?

Best Regards,

YK Lee

标签 (1)
0 项奖励
回复
4 回复数

1,328 次查看
jan_spurek
NXP Employee
NXP Employee

Hi,

the boot device is selected by fuses in BOOT_CFG1.

For eMMC: BOOT_CFG1[7:5] = 011

For SD card:  BOOT_CFG1[7:5] = 010

If you are using the SabreSD board, you can change the configuration via SW6 switch:
eMMC: 11100110 (from 1-8 bit)

SD: 01000010 (from 1-8 bit) - SD3 slot or 10000010 (from 1-8 bit) - SD2 slot

You can find detailed information in RM page 335.

0 项奖励
回复

1,328 次查看
yklee1
Contributor II

Hi,

Thanks a lot for your detail explenation.

I reviewed the document you mentioned.

But frankly I cannot find the answer for my question yet.

I would like to know boot device order is configured at Boot Rom or not like below,

     Checking whether eMMC has bootable image sets -> If yes, boot from eMMC.  If not, checking external SD card -> If yes, booting, if not checking SPI flash memory -> ...

Frankly I could not find the clear answer at RM.

If you know it, could you please let me know whether it is possible or not?

Best Regards,

0 项奖励
回复

1,328 次查看
igorpadykov
NXP Employee
NXP Employee

Hi YK

this is not possible with i.MX6Q, however for i.MX6SDL,SL there is

Manufacture Mode, described in sect.8.11 SD/MMC Manufacture Mode

i.MX6SDL Reference Manual (rev.2  5/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

When internal boot and recover boot (if enabled) failed, boot will go to SD/MMC

manufacture mode before serial download mode. In manufacture mode, one bit bus width

is used despite of the fuse setting.

In manufacture mode, SD or MMC card will be scanned on uSDHC1 and uSDHC2. If

card is detected and valid boot image is found in card, then boot image will be loaded

then executed.

Best regards

igor

0 项奖励
回复

1,328 次查看
jan_spurek
NXP Employee
NXP Employee

The initial boot device is selected by fuses. After power up, the system will attempt to boot from it. In order to proceed, there must be at least U-Boot on this device (for you it is the eMMC). As far as I know, if there is no U-boot on the initial boot device, nothing will happen and the system will not boot. After U-Boot gets loaded, you can choose from which device the linux image will be loaded by modifying environment variables.

You can write your own set of commands, which will do the procedure you described.

0 项奖励
回复