Boardbring up - IMX6solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boardbring up - IMX6solo

ソリューションへジャンプ
4,142件の閲覧回数
robinsingh
Contributor III

Hi All ,

I am trying to bring up a custom board based on IMX6SOLO. currently i am  using a Development kit based on (IMX6SX) ---sabresd and android is running  on it. can somebody give me some  pointer for starting or required/possible change in u-boot/kernel ?

I am planning to start with Sdcard boot and then move to eMMC.  here are my questions:

1) Is there any porting guide from freescale for new board ?

2) what are the change, I have to do in u-boot for DRAM (Hynix - H5TC4G63CFR-PBA ) ? pointer to the source file for imx6solo  ?

3) Do I have to change anything in Mgftool for downloading the new u-boot/kernel/android images ?

4) any other suggest  ?

thanks in advance.

Robin

ラベル(4)
0 件の賞賛
返信
1 解決策
3,577件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi robin

1. attached is Porting Guide document

2. for new board it is necessary to run ddr test, find new ddr settings

and update appropriate  *.cfg file, like uboot/..mx6sabresd/mx6dl_4x_mt41j128.cfg

i.MX6/7 DDR Stress Test Tool V2.20

3. the same modifications are needed for mfg tool firmware, steps for rebuilding

one can find in attached Yocto Guide sect.6.2 Manufacturing Tool, MFGTool

4. https://community.freescale.com/docs/DOC-100203

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,578件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi robin

1. attached is Porting Guide document

2. for new board it is necessary to run ddr test, find new ddr settings

and update appropriate  *.cfg file, like uboot/..mx6sabresd/mx6dl_4x_mt41j128.cfg

i.MX6/7 DDR Stress Test Tool V2.20

3. the same modifications are needed for mfg tool firmware, steps for rebuilding

one can find in attached Yocto Guide sect.6.2 Manufacturing Tool, MFGTool

4. https://community.freescale.com/docs/DOC-100203

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,577件の閲覧回数
robinsingh
Contributor III

Hi Igor,

Thank you for your reply.

I am trying to run the Stress test tool but i did not find any script for my CPU  imx6solo . can you please guide me how to generate this script file e.g any xls sheeti.Mx6DQSDL DDR3 Script Aid  like you have for other processor.

please take a look at the attached XLS sheet is it correct ? or i need to use any other xls sheet for reference ?

Thanks

Robin

0 件の賞賛
返信
3,577件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Robin

yes this is correct file.

Best regards

igor

0 件の賞賛
返信
3,574件の閲覧回数
robinsingh
Contributor III

Hi Igor,

I am getting this error in stress tool :

ERROR: DCD addr is out of valid range.

ERROR: DCD addr is out of valid range.

ERROR: DCD addr is out of valid range.

can you please take a look on our setting in attached xls sheet ? we are using H5TC4G63CFR-PBA DDR3(256x16) . here are the spec for this device.

pastedImage_0.png

please give us your feedback based on xlsx setting, am i missing anything ?

Regards

Robin

0 件の賞賛
返信
3,574件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Robin

please create new thread for this problem..

Best regards

igor

0 件の賞賛
返信