Board reset - i.MX 6DualLite SABRE Smart Device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Board reset - i.MX 6DualLite SABRE Smart Device

跳至解决方案
1,530 次查看
nilesha
Contributor I

We have i.MX 6DualLite SABRE Smart Device.


BSP: fsl-bsp-relase rocko

https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/README?h=rocko-4.9.88-2.0.0...

Board reset when running GPU test.

root@imx6dlsabresd:/unit_tests/GPU# ./gpu.sh
 
---- Running < gpu.sh > test ----
/unit_tests/GPU /unit_tests/GPU
 
U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1bf9f (Mar 20 2020 - 11:27:09
+0530)
 
CPU:   Freescale i.MX6DL rev1.1 996 MHz (running at 792 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 39C
Reset cause: POR
Model: Freescale i.MX6 DualLite SABRE Smart Device Board
Board: MX6-SabreSD
DRAM:  1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x11
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

标签 (3)
0 项奖励
回复
1 解答
1,402 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Nilesh

I tested on my side with MX6Q and sabre board and no reset was found even with qt webengine, I´m using 4.14.78 BSP.

Regards

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,402 次查看
nilesha
Contributor I

Thanks for your valuable input.

This is power supply issue and after changing power supply then no more device reset.

0 项奖励
回复
1,402 次查看
nilesha
Contributor I

Thanks for reply

I have tested using  warrior-4.19.35-1.1.0 

README\imx - meta-fsl-bsp-release - i.MX Yocto Project Release Layer 

But same result. 

Board reset when running GPU test.

Same result occurs when running qt webengine.

0 项奖励
回复
1,403 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Nilesh

I tested on my side with MX6Q and sabre board and no reset was found even with qt webengine, I´m using 4.14.78 BSP.

Regards

0 项奖励
回复
1,402 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Niless,

The error is present in that particular BSP, please change you BSP to the new one L4.19.35 or L4.14.78.

Regards

0 项奖励
回复