BT1120 16bit csi0 Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BT1120 16bit csi0 Driver

1,183 次查看
jorgesoria
Contributor II

I'm trying to develop a v4l2 driver for getting data from the csi0 bus in BT1120 format.(I'm using sabrelite for testing)

I'm trying to use the sii9135 patch but the kernel version that supports it directly is very old (3.0.15 from Boundary devices).

Have you ported the patch to a newer kernel version?

Which version are you using?

I'm a little lost with this task, I hope I'm not asking any dumb question.

 

I share a previous discussion with Allan Mattew so everyone can access to this useful information:

 

Allan Matthew  hace 1 semana

Hi Jorge-
The BT1120 patch is definitely a bit tricky.  I did end up using that sii9135 patch (for mxc_v4l2_capture) and used it as a reference for my adv7610.c driver file.  Although 3.0.15 is pretty old, there aren't too many differences to 3.10.17, but you'll definitely want to go through and check everything.  Lastly, I think I mention in a couple of my posts about what settings I had to use to get the BT1120 working, I think everything I needed is noted there.

Best of luck!
-Allan

 

Jorge Soria  hace 1 semana

Thank you Allan, i'll go though your posts and try to port the patch to 3.10.17.

I've no previous experience in kernel or driver development so this is an adventure for me

 

Your help is much appreciated!

Jorge

 

Jorge Soria  hace 7 días

Hello Allan, I've been making the modifications to the kernel following the patch.

You are right, 3.0.15 and 3.10.17 aren't so different. There is one file that doesn't exist en 3.10.17 which is "board-mx6q_sabrelite.c".

Do you know where is that funcionality in modern kernels? Is it in the Device Tree or in an equivalent source file I haven't found?

Do you remember any extra modifications that I must do in the Device tree?

 

Thank you very much for your hints, they are very useful and I'm learning a lot!.

Jorge

 

Allan Matthew  hace 7 días

Yes, you need to use the device tree for the newer kernel.  You'll find it in arch/arm/boot/dts/.  I had to add my decoder chip to an i2c bus and specify the pin connection format for the IPU1/CSI0 in the devicetree file.

 

Glad you're learning!  Btw please post this stuff publicly in the future so it can help others.  Thanks!

-Allan

 

Is it possible to modify this driver so it doesn't use any i2c communication at all? My device will be always sending data in the same format (always the same resolution, and supposedly always on).

Thanks.

Original Attachment has been moved to: dummy_camera_sii9135.patch.zip

标签 (2)
0 项奖励
回复
1 回复

713 次查看
jorgesoria
Contributor II

We managed to modify the driver to meet our requeriments and port it to 3.10.17 kernel some time ago.

It is configured as a platform device in Device Tree and it behaves as a dummy framegrabber, so no i2c communication needed.

I attach a patch hoping it could help someone with a similar issue.

Special thanks to Allan Mattew and S.j. Wang for the original patch.

0 项奖励
回复