BLE audio sink on iMX6/7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLE audio sink on iMX6/7

1,139件の閲覧回数
xifan
Contributor II

Dear NXP Team,

I want to stream audio from android phone to iMX6/7 via BLE(bluetooth low energy), what are the necessary steps to realize it if the actual imx bsp release is used ?

Due to the document

https://community.nxp.com/docs/DOC-103385 

sbc and pulseaudio packages should be installed, but not clear:

1. how to install the packages, via receipe in yocto or directly copy them (after compiling) into the rootfs?

2. After successfuly installation of such packages, do I need to write a user application to handle ble audio streaming request from android phone and the reaction from pulseaudio? 

3. Do you have any guide/tutorial to give an overview of the necessary steps to run ble audio streaming on iMX?

Thanks

0 件の賞賛
返信
1 返信

977件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xi

one can check presentation

Industry Leading Wi-Fi® + Bluetooth®/Bluetooth BLE Connectivity Solutions for All i.MX Products 

for software check yocto and linux documentation

Freescale Yocto Project main page 

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信