Dear Sirs,
We have developed electronic equipment for the agricultural sector. Now we are finalizing the development of a HMI device, similar to a tablet. But, more robust and for agricultural applications.
As processor, we are using a Toradex SOM, line Colibri iMX6. I need in this project an output for a Speaker. I do not need high sound quality. I just need a volume that is enough to be heard inside operating cabins. I need a speaker to play only alerts / warnings
I need to developed one hardware using the module's headphone output (or another audio output). After that, I needed one amplifier to play a Speaker.
Is it possible to indicate some PN for this application?
Kindly
Complementing the information. The Colibri Headphone_L analog output comes from the SGTL5000 CODEC, probably from the LINEOUT_L output.
Sirs,
Complementing the information. The output form Colibri 'Headphone_L' analog output comes from the SGTL5000 CODEC, probably from the LINEOUT_L output.