Hello,
I want to ask i.MX8QXP and i.MX8QP i.MX8QM,does they can support 8M@30fps camera input?
Solved! Go to Solution.
The theoretical maximum is 6G bit, which can be calculated according to the color depth of your own pixel.
If each pixel has a color depth of 16 bits, then 16 * 30 * 8M=3.84G bits should be able to use.
But if the color depth is 32 bits then it can not work.
The theoretical maximum is 6G bit, which can be calculated according to the color depth of your own pixel.
If each pixel has a color depth of 16 bits, then 16 * 30 * 8M=3.84G bits should be able to use.
But if the color depth is 32 bits then it can not work.