Android9.0 IMx6q-sabresd board booting error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android9.0 IMx6q-sabresd board booting error

1,648件の閲覧回数
ThanarajS
Contributor III

Hi All,

As I followed NXP user guide document to prepare the setup for Android 9.0 using IMX6Q-SABRESD board.

I downloaded source, compiled and created the images.

Using SD-Card, I tried to flash and bring up the board. I getting below errors.,

Please help me to resolve the issues on fstab mounting.

LOG:

U-Boot 2018.03-dirty (Aug 21 2019 - 15:08:12 +0530)

CPU: Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 36C
Reset cause: WDOG
Model: Ricoh i.MX6 MultiLink-Panel 8.0 Board
Board: MultiLink-Panel 9.0
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
flash target is MMC:0
Net:
Error: ethernet@02188000 address not set.
No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
RNG already instantiated 0x40000003
RNG already instantiated 0x40000003
verify OK, boot 'boot'
kernel @ 14008000 (10182072)
ramdisk @ 15000000 (1835263)
fdt @ 14f00000 (57786)
## Booting Android Image at 0x14007800 ...
Kernel load addr 0x14008000 size 9944 KiB
## Flattened Device Tree blob at 14f00000
Booting using the fdt blob at 0x14f00000
XIP Kernel Image ... OK
Using Device Tree in place at 14f00000, end 14f111b9
No PMIC found 2!

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.14.98-dirty (root@administartor) (gcc version 4.9.x 20150123 (prerelease) (GCC)) #4 SMP 9
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt: Machine model: Ricoh i.MX6 MultiLink-Panel 8.0 Board
Memory policy: Data cache writealloc
cma: Reserved 320 MiB at 0x32000000
random: get_random_bytes called from start_kernel+0xac/0x450 with crng_init=0
percpu: Embedded 18 pages/cpu @f64e7000 s41292 r8192 d24244 u73728
Built 1 zonelists, mobility grouping on. Total pages: 522290
Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,fbpix=RGB32,bpp=32 video=mxcd
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1726228K/2097152K available (13312K kernel code, 1057K rwdata, 4064K rodata, 1024K init, 504K bs)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf8000000 - 0xff800000 ( 120 MB)
lowmem : 0xc0000000 - 0xf7800000 ( 888 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0e00000 (14304 kB)
.init : 0xc1300000 - 0xc1400000 (1024 kB)
.data : 0xc1400000 - 0xc1508550 (1058 kB)
.bss : 0xc150a000 - 0xc1588348 ( 505 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
ftrace: allocating 41814 entries in 123 pages
Preemptible hierarchical RCU implementation.
Tasks RCU enabled.
NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
L2C-310 errata 752271 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76470001
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux: Initializing.
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: Spectre v2: using BPIALL workaround
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10100000 - 0x10100060
Hierarchical SRCU implementation.
smp: Bringing up secondary CPUs ...
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU1: Spectre v2: using BPIALL workaround
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU2: Spectre v2: using BPIALL workaround
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
CPU3: Spectre v2: using BPIALL workaround
smp: Brought up 1 node, 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
CPU3: update max cpu_capacity 1024
devtmpfs: initialized
CPU2: update max cpu_capacity 1024
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 1024 (order: 4, 65536 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.5
vdd1p1: supplied by regulator-dummy
vdd3p0: supplied by regulator-dummy
vdd2p5: supplied by regulator-dummy
vddarm: supplied by regulator-dummy
vddpu: supplied by regulator-dummy
vddsoc: supplied by regulator-dummy
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
imx rpmsg driver is registered.
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usb_phy_generic 2000000.aips-bus:usbphy_nop1: 2000000.aips-bus:usbphy_nop1 supply vcc not found, using dr
usb_phy_generic 2000000.aips-bus:usbphy_nop2: 2000000.aips-bus:usbphy_nop2 supply vcc not found, using dr
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA, using PIO instead.
i2c i2c-1: of_i2c: modalias failure on /soc/aips-bus@02100000/i2c@021a4000/pfuze100@08
i2c i2c-1: Failed to create I2C device for /soc/aips-bus@02100000/i2c@021a4000/pfuze100@08
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA, using PIO instead.
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA, using PIO instead.
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource mxc_timer1
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 1796K
hw perfevents: no interrupt-affinity property for /soc/pmu, guessing.
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
Bus freq driver module loaded
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(0.710:1): state=initialized audit_enabled=0 res=1
workingset: timestamp_bits=14 max_order=19 bucket_order=5
Registering sdcardfs 0.1
jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
fuse init (API version 7.26)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
pwm-backlight backlight: backlight supply power not found, using dummy regulator
mxc_mipi_dsi 21e0000.mipi: invalid reset gpio: -2
mxc_mipi_dsi 21e0000.mipi: failed to reset: -2
mxc_mipi_dsi: probe of 21e0000.mipi failed with error -2
ldb 2000000.aips-bus:ldb: crtc not specified or invalid
ldb: probe of 2000000.aips-bus:ldb failed with error -22
mxc_sdc_fb fb@0: NO mxc display driver found!
mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!
mxc_sdc_fb fb@2: Can't get fb option for mxcfb2!
mxc_sdc_fb fb@3: Can't get fb option for mxcfb3!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: Falling back to user helper
mxs-dma 110000.dma-apbh: initialized
imx-pgc-pd imx-pgc-power-domain.0: Linked as a consumer to 20dc000.gpc
imx-pgc-pd imx-pgc-power-domain.1: Linked as a consumer to 20dc000.gpc
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 27, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 77, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized vivante 1.0.0 20120216 for platform:Vivante GCCore on minor 0
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
zram: Added device: zram0
ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
ahci-imx 2200000.sata: failed to reset phy: -110
ahci-imx: probe of 2200000.sata failed with error -110
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_KEY_COL1 already requested by 20e0000.iomuxc; cannot claim foi
imx6q-pinctrl 20e0000.iomuxc: pin-128 (2008000.ecspi) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 128 (MX6Q_PAD_KEY_COL1) from group ecspi1grp on devc
spi_imx 2008000.ecspi: Error applying setting, reverse things back
spi_imx: probe of 2008000.ecspi failed with error -22
libphy: Fixed MDIO Bus: probed
tun: Universal TUN/TAP device driver, 1.6
CAN device driver interface
fec 2188000.ethernet: 2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: d2:28:3b:f1:b9:70
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
PPP generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
usbcore: registered new interface driver kaweth
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
usbmisc_imx 2184800.usbmisc: 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
imx_usb 2184000.usb: 2184000.usb supply vbus not found, using dummy regulator
imx_usb 2184200.usb: 2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 4.14.98-dirty ehci_hcd
usb usb1: SerialNumber: ci_hdrc.1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usbcore: registered new interface driver xpad
usbcore: registered new interface driver usb_acecad
usbcore: registered new interface driver aiptek
usbcore: registered new interface driver gtco
usbcore: registered new interface driver hanwang
usbcore: registered new interface driver kbtab
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_NANDF_ALE already requested by 20e0000.iomuxc; cannot claim f4
imx6q-pinctrl 20e0000.iomuxc: pin-182 (1-0004) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 182 (MX6Q_PAD_NANDF_ALE) from group egalax_i2c2_intgc
egalax_ts 1-0004: Error applying setting, reverse things back
egalax_ts: probe of 1-0004 failed with error -22
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_NANDF_CLE already requested by 20e0000.iomuxc; cannot claim f4
imx6q-pinctrl 20e0000.iomuxc: pin-181 (2-0004) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 181 (MX6Q_PAD_NANDF_CLE) from group egalax_i2c3_intgc
egalax_ts 2-0004: Error applying setting, reverse things back
egalax_ts: probe of 2-0004 failed with error -22
input: max11801_ts as /devices/soc0/soc/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_CSI0_DAT12 already requested by 21f0000.serial; cannot claim c
imx6q-pinctrl 20e0000.iomuxc: pin-162 (0-003c) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 162 (MX6Q_PAD_CSI0_DAT12) from group ipu1grp-2 on dc
ov564x 0-003c: Error applying setting, reverse things back
ov564x: probe of 0-003c failed with error -22
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_CSI0_DAT12 already requested by 21f0000.serial; cannot claim c
imx6q-pinctrl 20e0000.iomuxc: pin-162 (0-003c) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 162 (MX6Q_PAD_CSI0_DAT12) from group ipu1grp-2 on dc
ov5642 0-003c: Error applying setting, reverse things back
ov5642: probe of 0-003c failed with error -22
ov5640_power_on: cannot get io voltage error
ov5640_power_on: cannot get core voltage error
ov5640_power_on: cannot get analog voltage error
ov5640_read_reg:write reg error:reg=300a
camera ov5640_mipi is not found
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
max11801_ts 1-0048: FIFO_RD_AUX_MSB read failed (-6)
max11801_ts 1-0048: FIFO_RD_AUX_MSB read failed (-6)
max11801_ts 1-0048: FIFO_RD_AUX_MSB read failed (-6)
max11801_ts 1-0048: FIFO_RD_AUX_MSB read failed (-6)
__power_supply_register: Expected proper parent device for 'battery'
(NULL device *): hwmon_device_register() is deprecated. Please convert the driver to use hwmon_device_re.
__power_supply_register: Expected proper parent device for 'usb'
mag3110 2-000e: check mag3110 chip ID
mag3110 2-000e: read chip ID 0xfffffffa is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
mma8x5x 0-001c: read chip ID 0xfffffffa is not equal to 0x1a,0x2a,0x3a,0x4a,0x5a!
mma8x5x: probe of 0-001c failed with error -22
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
imx2-wdt 20c0000.wdog: timeout 60 sec (nowayout=0)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.37.0-ioctl (2017-09-20) initialised: dm-devel@redhat.com
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc1: new high speed SDHC card at address aaaa
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmcblk1: mmc1:aaaa SC16G 14.8 GiB
Primary GPT is invalid, using alternate GPT.
mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mxc_vpu 2040000.vpu_fsl: VPU initialized
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_KEY_ROW2 already requested by 20e0000.iomuxc; cannot claim fo0
imx6q-pinctrl 20e0000.iomuxc: pin-131 (soc:hdmi_cec@00120000) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 131 (MX6Q_PAD_KEY_ROW2) from group hdmicecgrp on dec
mxc_hdmi_cec soc:hdmi_cec@00120000: Error applying setting, reverse things back
mxc_hdmi_cec: probe of soc:hdmi_cec@00120000 failed with error -22
Galcore version 6.2.4.190076
mmc3: new DDR MMC card at address 0001
mmcblk3: mmc3:0001 HAG4a2 7.34 GiB
mmcblk3boot0: mmc3:0001 HAG4a2 partition 1 8.00 MiB
mmcblk3boot1: mmc3:0001 HAG4a2 partition 2 8.00 MiB
mmcblk3rpmb: mmc3:0001 HAG4a2 partition 3 4.00 MiB
mmcblk3: p1 p2 p3 < p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 >
[drm] Initialized vivante 1.0.0 20170808 for 130000.gpu on minor 1
leds-gpio: probe of leds failed with error -16
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ashmem: initialized
usbcore: registered new interface driver snd-usb-audio
fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW
fsl-hdmi-dai soc:hdmi_audio@00120000: failed to probe. Load HDMI-video first.
fsl-hdmi-dai: probe of soc:hdmi_audio@00120000 failed with error -12
NET: Registered protocol family 26
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
ctnetlink v0.93: registering with nfnetlink.
xt_time: kernel timezone is -0000
IPv4 over IPsec tunneling driver
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: arp_tables: (C) 2002 David S. Miller
Initializing XFRM netlink socket
NET: Registered protocol family 10
Segment Routing with IPv6
mip6: Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20170425 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20170425)
can: broadcast manager protocol (rev 20170425 t)
can: netlink gateway (rev 20170425) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
lib80211: common routines for IEEE802.11 drivers
registered taskstats version 1
random: fast init done
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_EIM_D29 already requested by 20e0000.iomuxc; cannot claim fors
imx6q-pinctrl 20e0000.iomuxc: pin-50 (gpio-keys) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 50 (MX6Q_PAD_EIM_D29) from group gpio_keysgrp on dec
gpio-keys gpio-keys: Error applying setting, reverse things back
gpio-keys: probe of gpio-keys failed with error -22
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:31 UTC (31)
usb_otg_vbus: disabling
usb_h1_vbus: disabling
mipi_dsi_pwr_on: disabling
ALSA device list:
No soundcards found.
Freeing unused kernel memory: 1024K
init: init first stage started!
init: Using Android DT directory /proc/device-tree/firmware/android/
init: First stage mount skipped (missing/incompatible fstab in device tree)
init: Skipped setting INIT_AVB_VERSION (not in recovery mode)
init: Loading SELinux policy
selinux: SELinux: Could not open /sepolicy: No such file or directory

init: Failed to load monolithic SELinux policy: No such file or directory
init: Unable to load SELinux policy
init: Reboot start, reason: reboot, rebootTarget: bootloader
init: Reboot ending, jumping to kernel
imx-sdma 20ec000.sdma: external firmware not found, using ROM firmware
ci_hdrc ci_hdrc.1: remove, state 4
usb usb1: USB disconnect, device number 1
ci_hdrc ci_hdrc.1: USB bus 1 deregistered
reboot: Restarting system with command 'bootloader'

Thanks!

Thanaraj.

Regards,
Thanaraj Subramani
ラベル(3)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

1,120件の閲覧回数
shivanipatel
Senior Contributor II

Hi, Thanaraj Subramani

Have you tried to flash the prebuilt images of Android 9.0 for i.MX6q SABRESD from this link?

Are you facing the issue with prebuilt images as well?

Regards,

Shivani

0 件の賞賛
返信

1,120件の閲覧回数
ThanarajS
Contributor III

Yes I have tried. its not at all booting, throwing "Please reset the board error".

FYI, I am using Sd card for flashing and booting image not emmc.

Note: Given link is not working to download the image.

Please provide me information to compile AOSP 9.0 for SD CARD boot.

Thanks

Regards,
Thanaraj Subramani
0 件の賞賛
返信

1,120件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you downloading the demo images with UUU or with the fsl-sdcard-partition.sh script?

Best regards,

Diego.

0 件の賞賛
返信

1,120件の閲覧回数
ThanarajS
Contributor III

Hi Diego,

I am using fsl-sdcard-partition.sh script to flash the image into sdcard.

Also please provide if you have any specific command to compile AOSP 9.0 for SD Card Device (not emmc)

Thanks

Regards,
Thanaraj Subramani
0 件の賞賛
返信

1,120件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

On the newer Android versions, there is no need to make the SD the target build.

However, you can make it with the below commands.

  1. Fist, remove /out/target/product/<your product>/root directory and boot*.img.
  2. Finally, build the boot.img and recovery.img as follows:

         make bootimage BUILD_TARGET_DEVICE=sd

Hope this could help you.

Best regards,

Diego.

0 件の賞賛
返信