Hi All,
The new Android R13.4.1.02 release is now available on the http://www.freescale.com/site.
· Files available
Name | Description | Files | |
1 | Android 13.4.1.02 patch release supports to run i.MX 6Solo emulation on i.MX 6DualLite SABRE-SD platform. Patch based on Android 13.4.1 BSP. Includes source code, demo image and MFG tool |
· Target HW boards
o i. MX6DL Sabre SDP board
· Known issues
o For known issues and limitations please consult the release notes
Hii,
I am trying to run imx6 sabre sd dual-lite board in solo mode. I applied the u-boot patches in bootable/bootloader/u-boot of android r13.4.1 release. But it's not booting. The log we are getting is as follow:
U-Boot 2009.08-00635-g5a8341b (Feb 08 2013 - 14:37:50)
CPU: Freescale i.MX6 family TO1.1 at 792 MHz
Temperature: can't get valid data!
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 198000000Hz
emi_slow clock: 22000000Hz
ddr clock : 396000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6DL/Solo-SABRESD: unknown-board Board: 0x61011 [POR ]
Boot Device: SD
I2C: ready
DRAM: 512 MB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
Hi,
Can you enter this question as a new question on the community? That will help us to track the solution because this publication was not entered as a question.
Regards