Hello!
Everybody know that Google open Android 4.0 sources, does anybody try to port it on IMX53 QSB? I am using know 2.3 BSP from adeneo. I have build 4.0 and get system.img file , but I use make PRODUCT-generic-user not imx53_loco like in adeneo. I dont touch 2.6.35 kernel from 2.3. Could anybody give some advices what to change in sources to get it working? init, init.rc?
and have you double checked all packages you need to have installed on you machine?
I only created one linaro sdcard, and the error I saw was caused by missing package
Does anyone knows what do i need to fix this error ? I'm running on Ubuntu 11.10 x86
I see...
Device Mount point Size
/dev/fd0 none 0MB
/dev/sda none 102400MB
/dev/sda1 / 101888MB
/dev/sda2 none 509MB
/dev/sda5 none 509MB
/dev/sdb none 3768MB
/dev/sr0 none 0MB
Are you 100% sure, on selecting [/dev/sdb] (y/n)? y
Checking that no-one is using this disk right now ...
OK
Warning: bad partition start (earliest 794625)
end of partition 4 has impossible value for cylinders: 1023 (should be in 0-1019)
If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
Traceback (most recent call last):
File "./linaro-image-tools/linaro-android-media-create", line 138, in <module>
args.should_create_partitions, args.should_align_boot_part)
File "/home/android/ICS/linaro-image-tools/linaro_image_tools/media_create/partitions.py", line 66, in setup_android_partitions
get_android_partitions_for_media (media, board_config)
File "/home/android/ICS/linaro-image-tools/linaro_image_tools/media_create/partitions.py", line 372, in get_android_partitions_for_media
media.path, 1 + board_config.mmc_part_offset)
File "/home/android/ICS/linaro-image-tools/linaro_image_tools/media_create/partitions.py", line 432, in _get_device_file_for_partition_number
device_path = _get_udisks_device_path(dev_file)
File "/home/android/ICS/linaro-image-tools/linaro_image_tools/media_create/partitions.py", line 447, in _get_udisks_device_path
return udisks.get_dbus_method('FindDeviceByDeviceFile')(device)
File "/usr/lib/python2.7/dist-packages/dbus/proxies.py", line 68, in __call__
return self._proxy_method(*args, **keywords)
File "/usr/lib/python2.7/dist-packages/dbus/proxies.py", line 143, in __call__
**keywords)
File "/usr/lib/python2.7/dist-packages/dbus/connection.py", line 630, in call_blocking
message, timeout)
dbus.exceptions.DBusException: org.freedesktop.UDisks.Error.Failed: No such device
Hi,
Any link to download the ICS source code for I.MX53 QSB ?? I searched in the linaro release but could not find one!! :smileysad:
I took the pre-built image. And after a reboot it got to homescreen.
Next step for me is to take source code.
I just donwloaded and it isn't up and running.
android cannot boot completely. Did you get to homescreen?
Hi, today I found Linaro's build ICS and flash it. I get not stable working ICS, but I see workscpaces, and launch Settings app. It works very buggy. Kernel is 3.1, Android 4.0.1, you could find compiled system on their site linaro.org
Hi. I´m looking forward to start working on ICS port for QSB, but I had not time yet =(
Do you know which is the kernel ICS needs? I don´t think it will be 2.6.35
I will follow this thread, so we can keep the discussion....