About unused NVCC18_IO in i.MX6SL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About unused NVCC18_IO in i.MX6SL.

ソリューションへジャンプ
612件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or madam,

[Q1]

If one doesn't use the 1.8V voltage in i.MX6SL system, is it necessary to input 1.8 V to NVCC18_IO? (Or, is it ok the NC?)

[Q2]

Refer to (P.73) 7.2.4 Power-up sequence in low voltage system design in i.MX6SL HardwareDevelopmentGuide Rev1.

If one use the 3.15V(NVCC33_IO) for all logic IO, is it possible to ignore the Sect 7.2.4?

Best Regards

Keita

ラベル(1)
0 件の賞賛
返信
1 解決策
537件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

1.
  NVCC18_IO must be provided.

2.

It is possible to ignore the Sect 7.2.4, assuming NVCC18_IO is applied.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
538件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

1.
  NVCC18_IO must be provided.

2.

It is possible to ignore the Sect 7.2.4, assuming NVCC18_IO is applied.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信