About the use of i. MX8MPlus USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the use of i. MX8MPlus USB

705件の閲覧回数
pengluo
Contributor III

The number of USB ports of imx8M plus is not enough. Can I divide a USB 3.0 port difference into a USB 2.0 and a USB 3.0 port difference for use? If so, can one be the host, the other the device, or the otg?
Do you have any good suggestions?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

693件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @pengluo,

I hope you are doing well.

If I understood correctly, you are looking to divide one USB port into two ports. However, that doesn't seem to be feasible.

If more USB ports are desired, one can use the USB Hub chipset. 

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信

685件の閲覧回数
pengluo
Contributor III

I see. Thank you for your advice

0 件の賞賛
返信