About the use of i. MX8MPlus USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the use of i. MX8MPlus USB

245 Views
pengluo
Contributor III

The number of USB ports of imx8M plus is not enough. Can I divide a USB 3.0 port difference into a USB 2.0 and a USB 3.0 port difference for use? If so, can one be the host, the other the device, or the otg?
Do you have any good suggestions?

Labels (1)
0 Kudos
2 Replies

233 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @pengluo,

I hope you are doing well.

If I understood correctly, you are looking to divide one USB port into two ports. However, that doesn't seem to be feasible.

If more USB ports are desired, one can use the USB Hub chipset. 

Thanks & Regards,
Ritesh M Patel

0 Kudos

225 Views
pengluo
Contributor III

I see. Thank you for your advice

0 Kudos