Hi NXP:
I'm now porting audio. I used external aux port is aux3 from Schematic, but I don't know which internal port is used.
How do I ensure which internal aux port is used?
Thanks.
Hello,
Are you using one of our boards? If yes, Which one?
Best Regards,
Diego.
Hi:
Yes, I use imx6q.
Thanks
Yes. I'm using the SABRESD board
Hello
Like you said, according to the schematic, the external aux port is connected to aud3 port. But following the schematic that audio port is connected to the CSI0_DAT (4 - 7) of the i.MX6Q - DISP CSI. Confirming with the i.MX pins tool the CSI0_DAT (4 - 7) is muxed with the AUD3_TXC, AUD3_TXD, AUD3_TXFS, AUD3_RXD respectively.
I hope this can solve your question.
Best Regards,
Diego.
Hello
Are you using the SABRESD board?
Best Regards,
Diego.
Hi Vaverka:
we use imx6qdl.
Thanks.
Hi Kainan,
Could you please specify which NXP IC are you using? It will help us to find the correct space for your question.
Best regards,
Tomas