Dear All,
I have a question about DDR setting register.
My customer would like to use DDR3_x64.
Refer to 44.12.46 MMDC PHY Read DQS Gating Control Register 0 (MMDCx_MPDGCTRL0) in MCIMX6DQRM(Rev.2).
There is below description.
======
For Channel 0: DDR3_x16, DDR3_x32, DDR3_x64
For Channel 1: DDR3_x64
======
Next, refer to "DG_HC_DEL1" bits.
-----------
Read DQS gating half cycles delay for Byte1 (channel 0 register) and Byte5 in 64-bit mode (channel 1 register)
-----------
Last, refer to "DG_CMP_CYC" and "DG_DIS" bit ,etc.
There isn't the description of channel 0 and channel 1.
[Question]
How should one set channel 0 and channel 1 to MMDCx_MPDGCTRL0?
I couldn't understand well...
Best Regards,
Keita
解決済! 解決策の投稿を見る。
Hi Keita,
>DG_HC_DEL1 and DG_HC_DEL0 bits were set for Channel 0 & 1 PHY?
Yes.
>Refer to Figure 2. DDR3 64-Bit Calibration Registers in AN4476(Rev.2).
>I have understood that MMDCx_MPDGCTRL0 register is "Calibration control" which is in Figure.2.
I think Figure 2 just shows generic structure, not registers.
Best regards
igor
Hi Keita
DQS Gating is used only for DDR3 memory, only channel 0 is used.
I.MX6Q has two “logic controllers” – one controller for each “channel”
or AXI port - this is not relevant for DDR3, only for LPDDR2.
Channel 1 ‘logic controller’ only employed when configuring MMDC for
dual-channel LPDDR2 usage and not used for DDR3.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your reply.
Sorry, I couldn't understand well.
Let me clarify these registers again.
My customer will use DDR3 with x64 bits width.
Refer to 44.12.46 MMDC PHY Read DQS Gating Control Register 0 (MMDCx_MPDGCTRL0) in MCIMX6DQRM(Rev.2).
Are these below description typo??
1. Supported Mode Of Operations:
======
For Channel 0: DDR3_x16, DDR3_x32, DDR3_x64
For Channel 1: DDR3_x64
======
2. DG_HC_DEL1 and DG_HC_DEL0 bits
======
Read DQS gating half cycles delay for Byte1 (channel 0 register) and Byte4 in 64-bit mode (Channel 1 register)
======
Best Regards,
Keita
Hi Keita,
sorry, I couldn't understand well:
where so you think typo - what word exactly?
Best regards
igor
Hi Igor,
You answered; DQS Gating is used only for DDR3 memory, only channel 0 is used.
So I consider that below description looks typo.
1. Supported Mode Of Operations:
======
For Channel 0: DDR3_x16, DDR3_x32, DDR3_x64
For Channel 1: DDR3_x64
======
2. DG_HC_DEL1 and DG_HC_DEL0 bits
======
Read DQS gating half cycles delay for Byte1 (channel 0 register) and Byte4 in 64-bit mode (Channel 1 register)
======
Best Regards,
Keita
Hi Keita,
thanks for clarifcation.
This is not accurate wording, since there are
two logic terms (please look at image above):
1. Channel1 logic controller
2. Channel1 PHY
meaning in text was for "Channel1 PHY" - configuration
characteristics for data bytes [4-7]
Best regards
igor
Hi Igor,
Thank you for your reply.
i.e. DG_HC_DEL1 and DG_HC_DEL0 bits were set for Channel 0 & 1 PHY?
Refer to Figure 2. DDR3 64-Bit Calibration Registers in AN4476(Rev.2).
I have understood that MMDCx_MPDGCTRL0 register is "Calibration control" which is in Figure.2.
Best Regards,
Keita
Hi Keita,
>DG_HC_DEL1 and DG_HC_DEL0 bits were set for Channel 0 & 1 PHY?
Yes.
>Refer to Figure 2. DDR3 64-Bit Calibration Registers in AN4476(Rev.2).
>I have understood that MMDCx_MPDGCTRL0 register is "Calibration control" which is in Figure.2.
I think Figure 2 just shows generic structure, not registers.
Best regards
igor