Dear All,
I'd like to know the preview performance in i.MX6DQ.
In the case of input 1080p@60fps video data from MIPI-CSI2, is it possible to use the preview function?
<Q1>
[Data] : 1920(W) * 1080(H) * 60(fps) * 1.35(Blanking) * 24(bit) = 3,844 Mbit/s = 480 MByte/s
[MIPI-CSI2] : 800Mbps/lane for four data lanes configuration = 400 MBytes/s
--> [Data] > [MIPI-CSI2]
From the above results, I consider i.MX6DQ (MIPI-CSI2 I/F) cannot support 1080p@60fps.
Is my understanding correct?
<Q2>
[Data] : 1920(W) * 1080(H) * 60(fps) * 1.35(Blanking) * 16(bit) = 2,563 Mbit/s = 320 MByte/s
--> [Data] < [MIPI-CSI2]
In this case, is it possible to use the preview function?
I worried about CPU load, data transfer internal IPU, and CSI performance(CSI2IPU gasket: MIPI to CSI),etc.
Please give me advice.
Best Regards,
Keita
Hi Keita
1. yes understanding is correct
2. yes it is possible
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------