About IMX6DQ RM of 17.6.2 Hardware ECC Accelerator Status Register 0 described.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About IMX6DQ RM of 17.6.2 Hardware ECC Accelerator Status Register 0 described.

跳至解决方案
789 次查看
takashitakahash
Contributor III

Hi, community.

want to check for a description of IMX6DQ RM.

IMX6DQ RM  of 17.6.2  Hardware ECC Accelerator Status Register 0, bit # 15 8 STATUS_BLK0 are described below.

0x01 ERROR1 One error found on the block.

0x02 ERROR2 One  errors found on the block.

0x03 ERROR3 One errors found on the block.

0x04 ERROR4 One errors found on the block.

But  described on The number of errors reported will be in the range of 0 to the ECC correction level for block 0 .and the stated, so

Below is correct?

0x02 ERROR2 2 errors found on the block.

0x03 ERROR3 — 3 errors found on the block.

0x04 ERROR4 4 errors found on the block.

标签 (3)
0 项奖励
回复
1 解答
716 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

your understanding is correct and this is described in

sect. 17.4.2.2 Using the Decoder IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
717 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

your understanding is correct and this is described in

sect. 17.4.2.2 Using the Decoder IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复