About IMX6DQ RM of 17.6.2 Hardware ECC Accelerator Status Register 0 described.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About IMX6DQ RM of 17.6.2 Hardware ECC Accelerator Status Register 0 described.

Jump to solution
751 Views
takashitakahash
Contributor III

Hi, community.

want to check for a description of IMX6DQ RM.

IMX6DQ RM  of 17.6.2  Hardware ECC Accelerator Status Register 0, bit # 15 8 STATUS_BLK0 are described below.

0x01 ERROR1 One error found on the block.

0x02 ERROR2 One  errors found on the block.

0x03 ERROR3 One errors found on the block.

0x04 ERROR4 One errors found on the block.

But  described on The number of errors reported will be in the range of 0 to the ECC correction level for block 0 .and the stated, so

Below is correct?

0x02 ERROR2 2 errors found on the block.

0x03 ERROR3 — 3 errors found on the block.

0x04 ERROR4 4 errors found on the block.

Labels (3)
0 Kudos
Reply
1 Solution
678 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

your understanding is correct and this is described in

sect. 17.4.2.2 Using the Decoder IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
679 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

your understanding is correct and this is described in

sect. 17.4.2.2 Using the Decoder IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply