Dear Sir or Madam,
External Pull down resistor was connected "AUD_TXFS" pad (H21) in i.MX6SL.
The default pad's state is Input Keeper, but the pad's state was seen as "High" before uboot processing.
Is it possible to keep the pad's state "Low" from power-on to Kernel operation?
Best Regards,
Keita
已解决! 转到解答。
Hi,
Perhaps the problem is concerned with general power up issue,
when during short period of stabilization states of pins are not defined,
and - moreover - some GPIOs may be actively driven.
Regards,
Yuri.
Hello. Yuri,
> is it possible to look at the schematic (via request) ?
Yes, possible.
But, I'd like to send it by secure transfer.
Could you tell me your e-mail address?
Best Regards,
Keita
Hello,
You may try 1K Ohm pull down resistor, but - first - please check
if the high level on the aud_txfs pin is not produced by an external circuit.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
Hello. Thank you for your reply.
We put the 1K Ohm pull down register, but the result wasn't solved. (The voltage level decrease a little.)
Do you have other idea?
(Or, does it set "AUD_TXFS" to High in iROM?)
Best Regards,
Keita
Hi,
Perhaps the problem is concerned with general power up issue,
when during short period of stabilization states of pins are not defined,
and - moreover - some GPIOs may be actively driven.
Regards,
Yuri.