AR6103 MAC address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AR6103 MAC address

Jump to solution
1,548 Views
Elangovan
Contributor I

Hi,

I am using AR6103 in our i.MX258 platform through SDIO.

With the default MAC address the device is working fine.

Here I am getting same mac address for all the boards.

Guide me to resolve this issue.

With Regards,

Elangovan C

Labels (2)
0 Kudos
Reply
1 Solution
1,212 Views
jimmychan
NXP TechSupport
NXP TechSupport

In the BSP reference manual, Chapter 16,17 are talking about Ethernet & FEC. You may also take the u-boot source code for reference because u-boot also can set the MAC for the board.

View solution in original post

0 Kudos
Reply
2 Replies
1,212 Views
YixingKong
Senior Contributor IV

Elangovan, please click Correct Answer/Helpful Answer if your question is resolved

Thanks,

Yixing

0 Kudos
Reply
1,213 Views
jimmychan
NXP TechSupport
NXP TechSupport

In the BSP reference manual, Chapter 16,17 are talking about Ethernet & FEC. You may also take the u-boot source code for reference because u-boot also can set the MAC for the board.

0 Kudos
Reply