AR6103 MAC address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,551件の閲覧回数
Elangovan
Contributor I

Hi,

I am using AR6103 in our i.MX258 platform through SDIO.

With the default MAC address the device is working fine.

Here I am getting same mac address for all the boards.

Guide me to resolve this issue.

With Regards,

Elangovan C

ラベル(2)
0 件の賞賛
返信
1 解決策
1,215件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

In the BSP reference manual, Chapter 16,17 are talking about Ethernet & FEC. You may also take the u-boot source code for reference because u-boot also can set the MAC for the board.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,215件の閲覧回数
YixingKong
Senior Contributor IV

Elangovan, please click Correct Answer/Helpful Answer if your question is resolved

Thanks,

Yixing

0 件の賞賛
返信
1,216件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

In the BSP reference manual, Chapter 16,17 are talking about Ethernet & FEC. You may also take the u-boot source code for reference because u-boot also can set the MAC for the board.

0 件の賞賛
返信