ADB devices not recognising for imx8m mini evk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADB devices not recognising for imx8m mini evk board

2,569 Views
Ruban1
Contributor II

command adb devices

its not recogising the imx8m mini evk board 

0 Kudos
Reply
7 Replies

2,553 Views
Ruben_Charles_avt
Contributor III

Hi @Ruban1,

Would you please share the log of the error?

From your description, you may want to first check if you enabled the USB developer option within your Android BSP.

This document might be helpful:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Using-ADB-with-your-Sabre-Board/ta-p/111...

Cheers

 

0 Kudos
Reply

2,554 Views
Ruben_Charles_avt
Contributor III

Hi @Ruban1 

Would you please share the log of the error?

From your description, you may want to first check if you enabled the USB developer option within your Android BSP.

This document might be helpful:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Using-ADB-with-your-Sabre-Board/ta-p/111...

Cheers

 

0 Kudos
Reply

2,544 Views
Ruban1
Contributor II
  • Go to Settings.
  • Click on "about tablet"
  • Scroll down to the last row (Build Number) and tap that row 7 times.
  • Return to the previous screen and click on "developer options
  • Confirm that "usb debugging" is checked.

the in command window i typed

adb devices

it doesnot show anything.. its empty. As if its not connected to host PC

 

0 Kudos
Reply

2,514 Views
Ruben_Charles_avt
Contributor III

Hi @Ruban1 ,

 

Please make sure that you are executing adb devices within the same folder as adb.exe. Just tested this on an i.MX 8M Nano EVK with success; you should see something similar:

 

C:\Android\platform-tools_r31.0.2-windows\platform-tools>adb devices
* daemon not running; starting now at tcp:5037
* daemon started successfully
List of devices attached
1e0b3a0a5c85f0d5        device

 

I am using the Android SDK Platform Tools, btw.

Hope this helps!

Tags (1)
0 Kudos
Reply

2,497 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!

 

2,507 Views
Ruban1
Contributor II

i am using ubuntu 20.04 .. cant u provide me details regarding ubuntu 20.04. not windows  

0 Kudos
Reply

2,491 Views
Ruben_Charles_avt
Contributor III

Just tested this on my Ubuntu 20.04 laptop. Hope it helps.

1. Install adb

 

ruben@ruben-HP-ZBook-15-G3:~$ sudo apt install adb

 

2. Connect your i.MX EVK using an USB cable, make sure to not use the debug UART.

3. Start adb

 

ruben@ruben-HP-ZBook-15-G3:~/Pictures$ sudo adb start-server
[sudo] password for ruben: 
* daemon not running; starting now at tcp:5037
* daemon started successfully

 

4. Make sure to have your EVK listed

 

ruben@ruben-HP-ZBook-15-G3:~/Pictures$ adb devices -l
List of devices attached
1e0b3a0a5c85f0d5       device usb:1-4 product:evk_8mn model:EVK_8MN device:evk_8mn transport_id:1

 

4. In my case, I transferred a picture from my laptop to the EVK, just to test:

 

ruben@ruben-HP-ZBook-15-G3:~/Pictures$ adb push apalis.jpg /storage/emulated/0/DCIM
apalis.jpg: 1 file pushed. 12.0 MB/s (133704 bytes in 0.011s)

 

5. Finish. Open your gallery at Android and you should see the the file.

 

ruben@ruben-HP-ZBook-15-G3:~/Pictures$ adb kill-server

 

6. Optional. It may possible that you need to enable adb as root user

 

ruben@ruben-HP-ZBook-15-G3:~/Pictures$ adb root

 

 

0 Kudos
Reply