8250 dw serial port driver in i.MX8 Nano

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8250 dw serial port driver in i.MX8 Nano

237 Views
jeslinpauljoseph
Contributor II

We are using i.MX nano based custom board in our device.

We want to use the 8250dw driver for one of the serial port.

1. Is it possible to modify /tweek the 8250 Driver and load the same in the i.MX?

2. If so can you guide what are all the changes need to be done?

0 Kudos
Reply
1 Reply

214 Views
Chavira
NXP TechSupport
NXP TechSupport

HI @jeslinpauljoseph!

Thank you for contacting NXP Support!


Do you want to use the driver 8250dw for UART ports of the iMX?


If my understandig is correct it is not possible because the UART ports of the iMX only works with our drivers.


Best Regards!

Chavira

0 Kudos
Reply