Dear NXP team,
want to know support of 1024 x 720 resolution with imx8mplus soc. We have a requiremebt with this non standard resolution hope the dedicated controllers are capable of rescaling to these resolution from the other resolutions received from the cameras to the available display
thanks
AMR
Thanks @joanxie @for the quick response
for poc we are planning to use https://www.variscite.com/wp-content/uploads/2017/12/VLCD-CAP-GLD-LVDS.pdf but for production it will change
for GKTW70SDAE4SE, this is 800x480 LCD panel, you can refer to the link as below:
"https://variwiki.com/index.php?title=DART-MX8M-PLUS_Display"
for imx8mp lvds support, the lvds is sourced from limited PLL as below
static const struct imx_pll14xx_rate_table imx_pll1443x_tbl[] = { PLL_1443X_RATE(1039500000U, 173, 2, 1, 16384), PLL_1443X_RATE(650000000U, 325, 3, 2, 0), PLL_1443X_RATE(594000000U, 198, 2, 2, 0), PLL_1443X_RATE(519750000U, 173, 2, 2, 16384), PLL_1443X_RATE(393216000U, 262, 2, 3, 9437), PLL_1443X_RATE(361267200U, 361, 3, 3, 17511), };
so couldn't support any pixel clock lvds, you can check if your display meets this or not, if yes, current bsp can support this
So I understand that if display has the capability bsp already has the support
Thanks once again for the quickest response