0ohm registor at DRAM_SDCLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

0ohm registor at DRAM_SDCLK

2,367件の閲覧回数
T_I
Contributor I

Hi

 

We design our custom board based on MCIMX53-START-R & MCIMX53SMD. DRAM_SDCLK has a series  terminator (0ohm). What meaning does this have?  If not necessary, I want to remove the resistor for space of the board.

regurds,

53-ddr.jpg

0 件の賞賛
返信
3 返答(返信)

2,200件の閲覧回数
T_I
Contributor I

Hi

Thanks for the reply.

I understand their meaning. 

0 件の賞賛
返信

2,200件の閲覧回数
NicolasIzquierd
Contributor III

Hi...

Totally agree with Yuri, those are access points and possibly resistor to compensate the signals due the pcb fabrication,so,  I do not recommend to remove them.

0 件の賞賛
返信

2,200件の閲覧回数
Yuri
NXP Employee
NXP Employee

First - the resistors may serve as test points for probe to analyze waveforms.
Next - if real (SDCLK) signal on the board appears to be not very "good" - it will be possible
to improve situation by locating more suitable termination resistors.
So, it may be recommended to use them at least for prototype design. 

0 件の賞賛
返信