请教,在i.MX28 EVK board上mfgtool更新wince fw问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

请教,在i.MX28 EVK board上mfgtool更新wince fw问题

1,018 Views
garylijs
Contributor II

在i.MX28 EVK board上,用mfg tool(mfgtool版本是1.6.2.048)更新eboot_ivt.sb到SDMMC显示操作完成,开机按space进入eboot menu,发现menu里的设置还是之前旧的,所以现在有个疑问:新eboot是否真写到SDMMC。

另外,从串口吐出的debug信息上,只看到更新eboot成功,没有看到更新nk.nb0和file,实际我在UCL.xml里除了配置files/eboot_ivt.sb,还配置了files/nk.nb0和files/sandy.mp3,应该这些都要更新才对。

下面是我的UCL.xml的配置:

<UCL>

  <CFG>

    <STATE name="Recovery" dev="IMX28"/>

    <STATE name="Updater"   dev="Updater" /> 

    <DEV name="IMX28" vid="15A2" pid="004F"/>

    <DEV name="Updater" vid="066F" pid="37FF" />

  </CFG>

    <LIST name="NAND" desc="Choose NAND as media">

        <CMD type="boot" body="Recovery" file="uce_ivt.sb">Booting Update Client Engine.</CMD>

        <CMD type="find" body="Updater" timeout="180"/>

        <CMD type="push" body="MediaType:NAND">Send media type.</CMD>       

  <!--<CMD type="push" body="QueryStoreStatus:DSK1:,Timeout:10">Query store status.</CMD>-->

  <CMD type="push" body="QueryStoreName:NAND FLASH Storage,Timeout:10">Send store name.</CMD>

        <CMD type="push" body="wfw">Notity device to prepare receiving a firmware.</CMD>

  <CMD type="push" body="fwtype:EB_SB">Specify firmware type.</CMD>

        <CMD type="push" body="send" file="files/eboot_ivt.sb">Sending a firmware file.</CMD>

        <CMD type="push" body="save">write the firmware to NAND flash.</CMD>

        <CMD type="push" body="wfw">Notity device to prepare receiving a firmware.</CMD>

  <CMD type="push" body="fwtype:NK_NB">Specify firmware type.</CMD>

  <CMD type="push" body="send" file="files/nk.nb0">Sending a firmware file.</CMD>

  <CMD type="push" body="save">write the firmware to NAND media.</CMD>

  <CMD type="push" body="QueryFolderStatus:NANDFlash,Timeout:10">Query store folder status.</CMD>

  <CMD type="push" body="wfl">Notity device to prepare receiving a file.</CMD>

  <CMD type="push" body="filename:NANDFlash\\sandy.mp3">Sending file name.</CMD>

  <CMD type="push" body="send" file="files/sandy.mp3">Sending a file.</CMD>

  <CMD type="push" body="save">Finish sending data.</CMD>

        <CMD type="push" body="Done">Whole update work is finished.</CMD>

  </LIST>

    <LIST name="SD/MMC" desc="Choose SD/MMC as media">

  <CMD type="boot" body="Recovery" file="uce_ivt.sb">Booting Update Client Engine.</CMD>

        <CMD type="find" body="Updater" timeout="180"/>

        <CMD type="push" body="MediaType:SDMMC">Send media type.</CMD>

        <!--<CMD type="push" body="QueryStoreStatus:DSK1:,Timeout:10">Query store status.</CMD>-->

  <CMD type="push" body="QueryStoreName:SD Memory Card,Timeout:10">Query store name.</CMD>

  <CMD type="push" body="Partitions:EBOOT:64MB,NK:32MB,File">Starting partitions.</CMD>

  <CMD type="push" body="wfw">Notity device to prepare receiving a firmware.</CMD>

  <CMD type="push" body="fwtype:EB_SB">Specify firmware type.</CMD>

        <CMD type="push" body="send" file="files/eboot_ivt.sb">Sending a firmware file.</CMD>

  <CMD type="push" body="save">write the firmware to SD/MMC media.</CMD>

  <CMD type="push" body="wfw">Notity device to prepare receiving a firmware.</CMD>

  <CMD type="push" body="fwtype:NK_NB">Specify firmware type.</CMD>

  <CMD type="push" body="send" file="files/nk.nb0">Sending a firmware file.</CMD>

  <CMD type="push" body="save">write the firmware to SD/MMC media.</CMD>

  <CMD type="push" body="QueryFolderStatus:SDMemory,Timeout:10">Query store folder status.</CMD>

  <CMD type="push" body="wfl">Notity device to prepare receiving a file.</CMD>

  <CMD type="push" body="filename:SDMemory\\sandy.mp3">Sending file name.</CMD>

  <CMD type="push" body="send" file="files/sandy.mp3">Sending a file.</CMD>

  <CMD type="push" body="save">Finish sending data.</CMD>

        <CMD type="push" body="Done">Whole update work is finished.</CMD>

    </LIST>

</UCL>

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

770 Views
garylijs
Contributor II

下面是从串口吐出的debug 信息,从debug信息中可以看到NAND不支持(目前EVK上没有NAND),只支持SD/MMC,但只看到更新ebbot,其他nk.nb0,file没有看到更新信息。

pArgs->ip4address........ 0

pDevice->Name............  s

pDevice->ifcType......... 0

pDevice->id.............. 0x80080000

pDevice->resource........ 0

pDevice->type............ 2

pDevice->pDriver......... 0x8048902C

WARN: OALKitlInit: KITL Disabled

reset GPMI module

enable bch module

ERROR: F:\WINCE600_2\PLATFORM\COMMON\SRC\SOC\COMMON_FSL_V2\NAND\FMDCOMMON\BIG_SECTOR_INTERLEAVE\.\fmd.cpp line 208: No NAND type matched!

BOT_InternalInit with Drivers\Active\06

UFN_ATTACH with key = Drivers\Active\06

UFN_CONFIGURED: BOT_OpenInterface again

UTP command:Media type: SDMMC.

UTP command:QueryStoreName.

UTP command:Check if disk is ready.

Please be patient to wait...

Send storage Friendly name: SD Memory Card.

Send time out: 10.

Find Store Device Name is DSK1:

Find Store Friendly Name is SD Memory Card

Info:Find Store by Friendly Name SD Memory Card

Get Store disk name:DSK1: by Friendly name SD Memory Card.

Opening disk DSK1: OK.

GetStoreList:szDisplayName is DSK1: SD Memory Card

Create g_pWriteBufferPool successfully!

DSK1: is ready.

UTP command:Partitions.

UTP command:Creating partitions.

Please be patient to wait...

There are 3 partitions.

EBOOT Partition 0:64MB done!

NK Partition 1:32MB done!

File Partition 2:0MB done!

WriteMBR: Write MBR to SDHC Finished!

Sleep 100 ms.

Sleep 200 ms.

Sleep 300 ms.

Sleep 400 ms.

Sleep 500 ms.

Sleep 600 ms.

Reopen disk DSK1: after SD/MMC virtual plugin.

ReCreate g_pWriteBufferPool successfully!

UTP command:Write image.

UTP command:Firmware type.

UTP command:Image type: EBOOT SB.

UTP command:Send.

UTP command:Send data.

Minimun image buffer size is : 0x10000.

Whole data length to be sent: 0x559b0.

INFO: Totally 685 sectors needs to be written.

Recievin

0 Kudos
Reply