如何制作Android系统的update升级包?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

如何制作Android系统的update升级包?

176 Views
oyyp86462
Contributor I

现在的车载板是I.MX6DL 2+16G  系统是Android4.4.3  怎么制作Android系统的update升级包,将Android系统4.4.3升级到7.1?

0 Kudos
Reply
3 Replies

137 Views
oyyp86462
Contributor I

你好,

会不会影响现有已经匹配好的屏参等信息?有没有更详细的升级教程?

0 Kudos
Reply

123 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

there is no tutorial from NXP, and I think yes it affect all the resources since android 8 has too much changes between version.

Regards

0 Kudos
Reply

145 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can note create an upgrade application since android 4 is out of support even android 7 too.

regards

0 Kudos
Reply