关于Android5.1移植wm8960若干问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于Android5.1移植wm8960若干问题

3,665 Views
void_
Contributor I

大家好,我用的是sabresd-6dl平台,在移植wm8960出现了下列问题,希望得到大家的帮助,先谢过了

imx6qdl-sabresd.dtsi配置如下:

     sound {
        compatible = "fsl,imx-audio-wm8960";
        model = "wm8960-audio";
        cpu-dai = <&ssi2>;
        audio-codec = <&codec>;
        codec-master;
        gpr = <&gpr>;
        audio-routing =
            "Headset Jack", "HP_L",
            "Headset Jack", "HP_R",
            "LINPUT1", "Main MIC",
            "LINPUT3", "Main MIC",
            "RINPUT1", "Main MIC",
            "RINPUT3", "Main MIC",
            "Main MIC", "MICB";
        mux-int-port = <2>;
        mux-ext-port = <3>;
        status = "okay";
    }; 

   codec: wm8960@1a {                                                                                                                                                

        compatible = "wlf,wm8960";

        reg = <0x1a>;

        clocks = <&clks 201>;

        clock-names = "mclk";

        clock-frequency = <12000000>;

        wlf,shared-lrclk;

    };

&ssi2 {

        fsl,mode = "i2s-slave";

        status = "okay";

};

其他没做文件没做任何修改,开机打印信息如下:

root@sabresd_6dq:/ # dmesg | grep wm

<5>    lowmem  : 0xc0000000 - 0xef000000   ( 752 MB)

<6>wm8962-supply: no parameters

<4>pwm-backlight.25 supply power not found, using dummy regulator

<6>imx-wm8960 sound.21: wm8960-hifi <-> 202c000.ssi mapping ok

<6>wm8962-supply: disabling

<6>  #0: wm8960-audio

而且一直打印下列错误

ASoC: HiFi startup failed: -16

ASoC: HiFi startup failed: -16

ASoC: HiFi startup failed: -16

ASoC: HiFi startup failed: -16

ASoC: HiFi startup failed: -16

ASoC: HiFi startup failed: -16

Labels (3)
0 Kudos
Reply
3 Replies

1,932 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,

     按照出错的LOG,应该来自imx-wm8960.C文件中,参数初始化时就没有通过。那么问题可能出在CPU端I2S有关的代码中。所以请检查一下:

(1)AUD3复用部分代码是不是对的。

(2)这里的cpu_dai好像不对:

imx6qdl-sabresd.dtsi配置如下:

     sound {

... ...

        cpu-dai = <&ssi2>;  //请修改为 cpu-dai = <&ssi1>

... ...

(3)WM8960 MCLK的问题

从你的代码中,你采用的12MHz(我做过试验12MHZ是可以使用的),但是24MHz时钟也是可以的。这里要注意的是:采用不同的MCLK时,从MCLK输入,经过PLL,直至得到sysclk(bit_clock)是不一样的配置,所以要注意一下驱动中的配置方式。

Best Regards,

Weidong

0 Kudos
Reply

1,932 Views
void_
Contributor I

Hi,Weidong

       非常感谢你的回复,我追踪了下错误的出处,的确是来自imx-wm8960.c中的imx-hifi-startup函数

static int imx_hifi_startup(struct snd_pcm_substream *substream)
{
    struct snd_soc_pcm_runtime *rtd = substream->private_data;
    struct snd_soc_dai *codec_dai = rtd->codec_dai;
    struct snd_soc_dai *cpu_dai = rtd->cpu_dai;
    struct snd_soc_card *card = codec_dai->codec->card;
   struct imx_wm8960_data *data = snd_soc_card_get_drvdata(card);
    bool tx = substream->stream == SNDRV_PCM_STREAM_PLAYBACK;
    struct fsl_sai *sai = dev_get_drvdata(cpu_dai->dev);
    int ret = 0;

   data->is_stream_opened[tx] = true;
    if (data->is_stream_opened[tx] != sai->is_stream_opened[tx] ||
        data->is_stream_opened[!tx] != sai->is_stream_opened[!tx]) {
        data->is_stream_opened[tx] = false;
       return -EBUSY;
    }

     .......   

}

(1)AUD3复用部分代码

         pinctrl_audmux: audmuxgrp {
            fsl,pins = <
                MX6QDL_PAD_CSI0_DAT7__AUD3_RXD      0x130b0                                                                                                     
                MX6QDL_PAD_CSI0_DAT4__AUD3_TXC      0x130b0
                MX6QDL_PAD_CSI0_DAT5__AUD3_TXD      0x110b0
                MX6QDL_PAD_CSI0_DAT6__AUD3_TXFS     0x130b0
            >; 
        };  

(2)这里的cpu_dai设置cpu-dai = <&ssi1>

(3)WM8960 MCLK不指定12M

                MX6QDL_PAD_GPIO_0__CCM_CLKO1    0x130b0

经上面三个步骤确认修改,重新编译下载镜像,结果还是一样,在论坛我看到一个同样问题的帖子

https://community.nxp.com/message/642991#comment-642991

但也没人给出正确的回复,希望得到你的帮助,谢谢

0 Kudos
Reply

1,933 Views
xianyoju
Contributor II

问题解决了吗?我也遇到同样的问题!!

能把解决方法说一下吗?

0 Kudos
Reply